Join us at Greenbuild Nov 19-22, 2019 in Atlanta
Click here to register for your free floor pass today
Menu
Search
Menu

Router Compatibility List

Compatible Devices for OnQ and Nuvo

* = WiFi Alliance Certified


Hardware Make Model(s) Compatible/Tested Works out of the box Known Issues
Router/SwitchArrisTG862G-CT*
SBG-6580*
Nuvo Player Portfolio On-Q Digital Audio On-Q lyriQ Digital Streaming ModuleNoUnder the Advanced Options menu - the Multicast Enable option must be enabled.
Router/SwitchActiontec VerizonMI424WR*Nuvo Player Portfolio On-Q Digital Audio On-Q lyriQ Digital Streaming ModuleYes
Router/SwitchLegrandDA2154-V1
DA1054
Nuvo Player Portfolio On-Q Digital Audio On-Q lyriQ Digital Streaming Module IntuityYes
Router/SwitchD-LINKDIR-865L v1.03 and v1.06*
DIR-655 v3.00 and 3.02*
Nuvo Player Portfolio On-Q Digital Audio On-Q lyriQ Digital Streaming Module IntuityNoDIR865L - Firmware v1.03 - IPV4 Multicast Streaming is not enabled by default. This option will need to be checked. This issue is corrected in v1.06 firmware. DIR-655 - Firmware 3.00 - Firmware v1.03 - IPV4 Multicast Streaming is not enabled by default. This option will need to be checked. This issue is corrected in v1.06 firmware.
Router/SwitchTP-LINKArcher C7 V2* v.131217 and v.150304
TP-WR841N* v3.14.4 and 3.16.9
Nuvo Player Portfolio On-Q Digital Audio On-Q lyriQ Digital Streaming Module IntuityNoFor the Archer C7 v131217 IGMP Proxy will need to be disabled under the NetworkIPTV menu selection.
Router/SwitchBuffaloWZR-600DHP* v20180 and v245PZ
WCR-GN* v1.04 and v1.08
Nuvo Player Portfolio On-Q Digital Audio On-Q lyriQ Digital Streaming Module IntuityYesNone
Router/SwitchMotorolaNVG-589Nuvo Player Portfolio On-Q Digital Audio On-Q lyriQ Digital Streaming Module IntuityYes
Router/SwitchLuXulXBR-4400
XWR-1750
XWR-600
Nuvo Player Portfolio On-Q Digital Audio On-Q lyriQ Digital Streaming ModuleYesNone
Router/SwitchCisco/LinksysEA4500*
EA6500*
E2500*
WRT-54GL* v4.30.14 and v4.30.16
E1200* v2.0.04 and 2.0.07
Nuvo Player Portfolio On-Q Digital Audio On-Q lyriQ Digital Streaming Module Intuity WRT-54GL E1200YesNone
Router/SwitchNetgearNighthawk R7000 WNDRMACV2
WNDR3700v4*v1.0.1.42 and 1.0.2.78
WNDR4300v2* 1.0.0.26
WNR100v3*
ADSL Modem Model 7550
Nuvo Player Portfolio On-Q Digital Audio On-Q lyriQ Digital Streaming Module IntuityYesNone
Router/SwitchTechnicolorTC-8305*
C2000T Century Link*
Nuvo Player Portfolio On-Q Digital Audio On-Q lyriQ Digital Streaming Module Intuity C2000TYesNone
Router/SwitchASUSRT-N56U* v.3.0.0.43744561
RT-N53* v3.0.0.4.374311 and v3.0.0.4.376.3754
Nuvo Player Portfolio On-Q Digital Audio On-Q lyriQ Digital Streaming Module IntuityYesNone
Access PointsLegrandDA1101
DA1104
Nuvo Player Portfolio On-Q Digital Audio On-Q lyriQ Digital Streaming Module IntuityYes
Access PointsLuXulXAP-1550
XAP-1230
Nuvo Player Portfolio On-Q Digital Audio On-Q lyriQ Digital Streaming ModuleYesNone

Incompatible Devices


Hardware Make Model(s) Issue Remedy
Router/ SwitchActiontecGT724WGR
M1000
C1000A
W1000
PK5000
These model routers/modems do not fully support the passing of multicast packets via the wired and wireless networks.A Legrand or third party wireless access point is needed. We recommend the DA2154-V1.
Router/ SwitchAlcatel LucentI-240W-R
I-240W-Q
I-240W-T
These model routers/modems do not allow multicast packets to pass between the wired and wireless connections on the router/modem.A Legrand or third party wireless access point is needed. We recommend the DA2154-V1.
Router/SwitchTrendNetTEW-812-DRU v2.0.10.0These model routers/modems do not fully support the passing of multicast packets via the wired and wireless networks. The Intuity system does not commission properly when using this router device.A Legrand or third party wireless access point is needed. We recommend the DA2154-V1.
Router/ SwitchBelkinF7D4301
F7D4302
F7Dxxxx
These model routers/modems do not fully support the passing of multicast packets via the wired and wireless networks.A Legrand or third party wireless access point is needed. We recommend the DA2154-V1.
Router/ SwitchBelkinF9K1103This router does not support the passing of proper IGMP packets. Some functions of the On-Q system may not work properly.A Legrand or third party wireless access point is needed. We recommend the DA2154-V1.
Router/ SwitchCiscoAll DPC/EPC/DPQ models Except DPC3825 and DPC3939These model routers/modems do not fully support the passing of multicast packets to the SSDP destination port UDP Port 1900.A Legrand or third party wireless access point is needed. We recommend the DA2154-V1.
Router/ SwitchHuaweiHG532dThese model routers/modems do not fully support the passing of multicast packets to the SSDP destination port UDP Port 1900.A Legrand or third party wireless access point is needed. We recommend the DA2154-V1.
Router/ SwitchKPNInternetPlus ModemThis router blocks all UPnP traffic.An additional router will be necessary between this device and the On-Q or NuVo audio system.
Router/ SwitchLinksysWCG200-CComcast provided device. This device only supports 5 local IP addresses.There is no way to increase the local DHCP IP address pool.
Router/ SwitchNetgearCG814WGv1
CG814WGv2
Comcast provided device. This device only supports 4 local IP addresses.The local DHCP pool can be increased but only 4 local devices will have internet access.
Router/SwitchUbeeDDW3201BThis model routers/modems do not allow multicast packets to pass between the wired and wireless connections on the router/modem by default.Enable Multicast Enable in the router settings.
Router/SwitchUbeeDDW365This model routers/modems do not allow multicast packets to pass between the wired and wireless connections on the router/modem by default.Enable Multicast Enable in the router settings.
Router/ SwitchUS RoboticsUSR 8054These model routers/modems do not fully support the passing of multicast packets via the wired and wireless networks.Enable Multicast Streaming in the router settings.
NAS DrivesFantecAll ModelsNo support for Windows File Sharing SMB.None.
NAS DrivesHawkingHNAS1Defaults to static IP of 192.168.1.1. This creates an IP conflict with a large number of routers.Use the setup CD to assign an IP address outside of the DHCP scope.
NAS DrivesLevel OneFNS 1000Built-in DHCP server is enabled by default. Can create IP address conflicts. Also defaults to a static IP address.Disable DHCP server and give the NAS a static IP.
NAS DrivesNetgearSC101
SC101T
This device is an NDAS it requires the computer to be on and running software in order to access the files stored on it.None.