COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

Legrand Debuts Nuvo Series Two Landscape Speaker System at CEDIA that Delivers Premium Audio for Outdoor Entertaining

Designed to be Heard and Not Seen, Slim Satellite Speaker and In-ground Subwoofer Provide Perfect Low-Profile Solution for Extending Audio Systems Outdoors


SAN DIEGO, September 7, 2017 – Legrand, the global specialist in electrical and digital building infrastructures, announced an expansion of its outdoor speaker line with the introduction of the Nuvo Series Two Landscape Satellite Speakers and Subwoofer. The new low-profile speaker system, designed for inconspicuous placement, delivers impressive audio with extensive coverage outside of the home. These models extend the company’s outdoor speaker line offerings.

Featuring a 3½-inch poly woofer and a ½-inch UFLC tweeter in a trim, black teardrop enclosure, the satellite speaker delivers clear, robust audio to the deck, pool or backyard. The powerful subwoofer features an 8-inch driver housed in a cylindrical enclosure, designed to be buried in the ground to blend subtly into landscaping while providing standout bass response. The products are available as a kit (NV-2LSK-BK) including the buried sub and four satellite speakers, as well as an expansion pack of two satellite speakers (NV-2LS3-SAT2BK).

“The Legrand Nuvo Landscape speaker and subwoofer provide home tech pros with an ideal solution to offer their customers incredible listening experiences for any outdoor audio installation, or as an addition to an existing Nuvo whole-home audio system,” said Fritz Werder, Legrand VP and general manager, On-Q and Nuvo lines. “Each model features unobtrusive designs that will easily integrate into any outdoor or landscaped environment.”

Each of these landscape speakers are IP-67 and MIL-STD-810-compliant to provide years of reliable performance in harsh weather conditions. They both also carry a lifetime warranty.

Additional information on the Nuvo Series Two Landscape Satellite Speaker and Subwoofer is available here.

About Legrand and Legrand, North & Central America

Legrand is a global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth, including, in particular, connected devices stemming from Legrand’s global Eliot (Electricity and IoT) program. Legrand reported sales of $5.6 billion in 2016. Legrand has a strong presence in North and Central America, with a portfolio of well-known product lines that include C2G, Cablofil, Electrorack, Luxul, Middle Atlantic, Nuvo, OCL, On-Q, Ortronics, Pass & Seymour, Pinnacle, QMotion, Quiktron, Raritan, Solarfective, Vantage, Wattstopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating and DJSI (ISIN code FR0010307819) www.legrand.us

 

Media Contacts:

Feintuch Communications

Doug Wright / Richard Roher

212-808-4903 / 917-207-9604

legrand@feintuchpr.com