Legrand Launches Latest in Edge Computing Series: Two New Cabinets for Digital Buildings
New London, CT
January 24, 2018
Legrand North America®, a global leader in high-performance network infrastructure solutions, today introduced two new cabinets as part of its ongoing effort to enable digital buildings and edge computing: the vertical wall-mount cabinet and swing-out wall-mount cabinet.
“Ideally, every strategy deployed in a digital building will enable edge computing and the next wave of broader connectivity,” said Domenic Trapassi, product manager at Legrand. “These two new cabinet solutions from Legrand help enable edge computing in digital buildings by maximizing flexibility and versatility.”
Vertical Wall-Mount Cabinets
The new vertical wall cabinets offer a versatile, low-profile solution with comprehensive flexibility to fit system needs today and as technology evolves.
Legrand’s vertical wall cabinets are a cost-effective solution that offers flexibility, versatility and accessibility – ideal for digital building and IoT applications. Their unique design allows mounting of racks where needed. They also offer:
- A configurable platform that mounts equipment vertically to minimize the cabinet’s protrusion from the wall;
 - Component mounting flexibility to tailor the cabinet for the needs of the system, including modular options for mounting equipment of varied sizes and form factors;
 - Fixed and pivoting mounting rail options that include 12-24 threaded and cage nut mounting options;
 - Ability to mount small computing devices: Backpans available in various overall depths and heights; and
 - Two door options to enable the desired level of system security.
 
“In buildings that have Power-over-Ethernet lighting or other IoT applications, the right wall cabinet strategy can save critical facility space and help meet the increasing demand for edge computing, making it imperative for facility managers to pick exactly the right solution to deploy,” said Trapassi. “Whether in a new install or a retrofit, Legrand’s vertical wall cabinets offer flexibility and superior design, as well as seamless integration into the infrastructure without custom components.”
Swing-Out Wall-Mount Cabinets
Designed for greater durability and versatility, Legrand’s new swing-out wall-mount cabinets offer particular value within space-limited and retail settings. These new Legrand cabinets offer a flexible, low-profile solution that meets the broad requirements of evolving technology systems while readily managing the cabling loads typical in today’s modern building networks.
“We designed these latest swing-out wall-mount cabinets to be extremely rugged and to offer incredible space savings because our customers – especially those within the retail sector – require a network setup that’s highly adaptable to their equipment and space requirements,” said Trapassi. “These swing-out cabinets are compact and a proven way to optimize space because they can mount to a wall and replace a rack.”
For more information on Legrand’s wall cabinet solutions, please click HERE.
###
About Legrand, North America
Legrand is a global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth, including, in particular, connected devices stemming from Legrand’s global Eliot (Electricity and IoT) program. Legrand reported sales of $5.6 billion in 2016. Legrand has a strong presence in North and Central America, with a portfolio of well-known market brands and product lines that includes AFCO Systems, C2G, Cablofil, Chief, Da-Lite, Electrorack, Finelite, Luxul, Middle Atlantic Products, Nuvo, OCL, On-Q, Ortronics, Pass & Seymour, Pinnacle, QMotion, Quiktron, Raritan, Sanus, Solarfective, Vaddio, Vantage, Wattstopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating, and DJSI (ISIN code FR0010307819) www.legrand.us. 
Media contact:
Jay Staunton
Skibereen Consulting
jay@skibereen.com
781-790-6023