text.skipToContent text.skipToNavigation

Why Receptacle Devices are the Best Way to Beat Project Delays


The electrical contracting industry is fighting a severe capacity crunch. Approximately 77% of contracting firms report that their difficulty in hiring is specifically due to a lack of qualified candidates.* When less-skilled labor is on the job, the risk of error soars, resulting in costly rework and longer timelines — 66% of firms are now forced to lengthen project schedules due to these constraints.*

To combat these delays, electrical contractors are moving away from traditional, labor-intensive approaches. Instead, they are adopting smart strategies that reduce labor hours and minimize installation errors. This is where solutions like accelerated wiring systems, such as the Legrand PowerHold™ Receptacle Device, come into play. By cutting installation time from over a minute to 10 seconds or less, electrical contractors are able to pivot from fixing mistakes to making more profit.

Eliminates Rework


Contractors are not just relying on skill alone. They are starting to use reliable products to help improve quality. PowerHold changes the game through speed and standardization. By comparing the conservative traditional wiring time of 2 minutes (120 seconds) to PowerHold's installation time of 10 seconds, the system is 12 times faster.

Because the process is so fast, it makes it easier to install a receptacle for electricians of all skill levels. It becomes a standardized, shorter process. This translates into recovered labor costs and the increased capacity needed to take on more jobs.

Improves Safety

Contractors don't have to choose between speed and safety. PowerHold is designed to support worker safety, even with newer workers. The patented tooth design locks wires in with high retention force (more than 30 pounds) to virtually eliminate loose connections — the biggest cause of dangerous callbacks and delays.

zoomed image of color-coded levers

The system features color-coded levers (white for neutral, black for hot, green for ground) that align with uniform industry terms. It features an audible snap that eliminates guesswork and instantly confirms that the connection is correct. This lets contractors confidently assign newer workers to repetitive tasks, preventing costly mistakes that can stall the job.

Finally, because the device is designed to eliminate the need for multiple tools like screwdrivers and drills, it’s easier to master. Its ergonomic design helps eliminate drill slippage and repetitive screwdriver turns. It also features larger levers compared to competitive products, making it easier for contractors to operate even while wearing gloves.

Accelerates Projects in High-Volume Sectors

In big jobs like apartment buildings (MDU), hotels (hospitality) and retail spaces (light commercial), speed and consistency are everything. Since contractors install thousands of devices, saving even one second per unit can prevent major delays across the entire project.

The shallow design of the PowerHold device is a huge help. In dense buildings, junction boxes are often crammed with bulky wires. With traditional tools, crews can waste time struggling to force components into these tight spots. PowerHold has a reduced depth that makes managing thick wires, like 10 or 12 gauge, easier inside these confined spaces. It quickly cuts down the effort and time needed for each installation.

Because the basic wiring process is so easy, senior electricians don't have to constantly watch over simple tasks. They are free to focus on strategic work, which immediately increases contractors’ ability to pursue new, complex projects — work that 45% of firms are currently forced to turn down.*

PowerHold is also a great solution for prefabrication. The consistent 10-second installation time guarantees fast output in the factory, dramatically speeding up the overall project. Plus, the receptacle helps improve quality inside the factory, eliminating the risk of time-consuming, expensive rework.

Making the switch to modern, efficient tools, like PowerHold, is the key to winning more bids and completing every job faster to keep your bottom line strong.

*Skilled Labor Shortages in Construction - Travelers Insurance, accessed November 4, 2025,

https://www.travelers.com/resources/business-industries/construction/skilled-labor-shortages