Groundbreaking Outdoor Power
Discover how the Outdoor Ground Box brings safe, permanent
power to stadium events.
Legrand is established in nearly 90 countries
View all at Legrand.com
On game day, power isn’t just a utility—it’s part of the experience. From Friday night lights to sold-out concerts and championship games, stadiums rely on outdoor power to keep fans safe, performers energized and operations running smoothly.
But stadium environments are brutal on electrical infrastructure. Outdoor power systems face constant exposure to weather, heavy foot traffic, temporary event setups and growing electrical demands. When outdoor power fails, the impact is immediate—and impossible to hide.
Rain, snow, heat, ice, humidity and flooding are all part of life for stadiums. Outdoor electrical equipment—especially power installed at ground level—must survive conditions that indoor systems never encounter.
Water intrusion is one of the biggest risks, particularly for stadiums located in flood-prone or coastal regions. According to guidance from UL, electrical equipment used in wet locations must be specifically designed and tested to withstand prolonged exposure to moisture and water ingress.
Submerged under 53 inches of water during Hurricane Harvey, this high school football stadium’s Outdoor Ground Box was tested by real flood conditions—and kept working.
Stadiums today host far more than sports. Concerts, festivals, graduations, esports events and community gatherings all bring unique—and often temporary—power needs.
Without permanent outdoor power infrastructure, facilities are forced to rely on generators and extension cords, increasing setup time, labor costs and safety risks. The National Fire Protection Association emphasizes minimizing temporary wiring wherever possible to reduce trip hazards and electrical risk in public venues.
In spaces designed to hold thousands, electrical safety isn’t optional. It’s foundational.
Outdoor power in stadiums must meet strict requirements for grounding, tamper resistance, and protection in wet locations. These standards are outlined in the National Electrical Code, which forms the foundation for most local and state electrical regulations.
In stadium environments, these requirements aren’t theoretical. High foot traffic, exposure to weather, cleaning operations, and temporary event setups all increase the risk of electrical hazards. Improperly protected outlets or exposed cords don’t just risk noncompliance—they put fans, staff, and performers directly in harm’s way.
Industry guidance from the National Fire Protection Association reinforces the need to minimize temporary wiring in public venues, citing increased trip hazards and electrical risk—especially in high-traffic areas.
☑ Wet-Location Rated
Designed and tested for exposure to rain, irrigation, washdowns and flooding
☑ Tamper-Resistant Protection
Prevents unauthorized access in public, high-traffic areas
☑ Proper Grounding
Reduces shock risk and supports safe operation during live events
☑ Enclosed & Protected Connections
Limits water intrusion and accidental contact with energized components
☑ Flush or Low-Profile Installation
Reduces trip hazards and keeps walkways clear
☑ Tested to Recognized Standards
Evaluated to meet applicable requirements from the National Electrical Code and third-party certification bodies like UL
Modern stadiums are more connected than ever. Digital signage, high-speed Wi-Fi, real-time analytics, mobile concessions, security systems, and fan charging stations all increase demand for reliable outdoor power — and those systems aren’t free in terms of electrical load.
Connected infrastructure is becoming a major investment. The global smart stadium market — a broad category that includes everything from IoT devices to advanced connectivity solutions in sports venues — is projected to grow from an estimated ~$19.5 billion in 2024 to more than $41 billion by 2029 at a compound annual growth rate (CAGR) of around 16.4%.
Other forecasts paint an even larger picture, with the global smart stadium market expected to be worth nearly $75 billion by 2034, expanding at a CAGR of about 15.6% as connected technologies become central to fan engagement and stadium operations.
The trend toward connectivity is also reflected in how fans consume data in stadiums. Instead of just showing up with tickets, attendees increasingly use mobile apps for tickets, stats, concessions, social posting, and in-seat experiences — and carriers are seeing the data growth. According to recent reporting, mobile data usage at NFL stadiums increased roughly 37% per game compared with the previous season, with fans generating nearly 960 terabytes of data across events.
All of this means that older stadium electrical systems — originally designed for lighting, basic concessions, and simple broadcasting — are now being asked to support massive new loads for digital connectivity, charging, and analytics. Without planning for scalable outdoor power infrastructure, facility operators risk overloading circuits, creating hotspots of demand that legacy electrical systems weren’t built to handle.
Aesthetics matter—especially in venues designed around sightlines, branding, and atmosphere. Bulky enclosures, exposed cords, and temporary cabling don’t just look out of place; they interrupt the fan experience and distract from the event itself.
Flush-mounted outdoor power solutions install level with the surface, keeping power accessible without competing for attention. When infrastructure disappears into the environment, fans stay focused on the field, the stage, and the moment—not what’s underfoot.
Stadiums don’t have room for failure. Events are scheduled months in advance, tickets are sold and expectations are set long before the gates open. When the lights come on and the crowd arrives, power has one job: work.
Outdoor power must perform after severe weather, long periods of inactivity and repeated use—often under intense pressure. There’s no backup plan once the event begins, and no margin for disruption when thousands are watching.
In stadium environments, reliability isn’t proven in perfect conditions. It’s proven when everything has already been tested.
Outdoor power in stadiums doesn’t get a second chance. That’s why the Outdoor Ground Box performance is validated long before installation, through rigorous testing that simulates real-world exposure to water, weather and repeated use.
Stadiums are built for big moments—kickoffs, encores, championships and community gatherings that people remember long after the lights go out. Behind every one of those moments is power that has to perform without hesitation.
From extreme weather and temporary events to safety, aesthetics and reliability, outdoor power in stadium environments faces challenges few other facilities encounter. When power is thoughtfully designed into the venue—protected from the elements, compliant with code, ready for repeated use and invisible when it should be—it stops being a risk and starts being a strength.
Because in a stadium, there’s no rewind. No second chance. And no room for power that doesn’t hold up when the crowd is watching.
Discover how the Outdoor Ground Box brings safe, permanent
power to stadium events.
Turn outdoor spaces into vibrant places to celebrate life outside.