text.skipToContent text.skipToNavigation

Wattstopper® Fixture Integrated Outdoor Sensors to Support Philips Lighting SR Platform


San Jose, Calif., July 12, 2017 – Legrand, North & Central America announced today the development of new Wattstopper FDP-300 Series sensors.  The sensors, which will launch under Legrand’s Eliot program, will be the first in the market to add occupancy detection to a connected outdoor fixture. Specifically engineered for OEM use, these digital sensors will offer multi-level control based on motion and/or daylight contribution and designed to share information to and from peripheral devices, including wireless nodes and digital LED drivers such as Philips Xitanium SR drivers. Legrand is part of Philips Lighting SR (System Ready) Certified Program and the FDP-300 Series sensors will be the first products being developed as part of this partnership.

Outdoor lighting systems are experiencing a market shift from analog to digital sensors and network controlled solutions. This shift to connected lighting and intelligent controls are driven by emerging technologies such as LEDs and initiatives like the Internet of Things (IoT). These sensors enable connected intelligent lighting for outdoor spaces and ensure substantial energy and maintenance cost savings.

As part of an outdoor lighting solution, FDP-300 Series sensors will help facility engineers and city managers to easily monitor, control, commission, and diagnose outdoor lighting while maximizing safety and security. Ideal for street lighting applications, commercial site lighting, and parking lots in commercial and city spaces, the sensors will feature robust SR functionality.

Easily incorporated into manufacturing and design processes, the FDP-300 Series will come in multiple mounting options to fit with a variety of luminaires.

Features and benefits:

  • Maximum sequence of operations flexibility enables the FDP-300 Series to perform in a variety of applications.  
  • Ease of installation and setup with local or remote commissioning. These sensors can be easily and securely set up, configured, and customized locally or though the cloud.
  • IP66 and IK08 Rated to ensure the highest protection against water, dust, and other non-corrosive material as well as against external mechanical impacts – critical for street lighting products.
  • Code compliance with latest ASHRAE 90.1/ IECC and California Title 24 outdoor lighting control requirements.

 
Legrand Eliot Program

The Wattstopper FDP-300 Series digital fixture integrated outdoor sensors tie to the larger context of Legrand’s Eliot (Electricity + IoT) program. Eliot is a global Legrand IoT program that brings together Legrand's worldwide expertise to advance connectivity and intelligence in the built environment, mobilize Legrand’s capabilities around the world, and speed development of Legrand connected devices wherever the Internet of Things can enhance value for all users.

Products, systems, and services under Legrand’s Eliot program, including the FDP-300 Series sensors, adhere to three important principles:

  1. Products and solutions enhance value by simplifying usage and facilitating maintenance.
  2. They are intuitive and easy to install and operate, which is part of Legrand’s DNA.
  3. Consistent with Legrand values, Eliot products, systems, and services respect and preserve the confidentiality of user’s data.
These critical principles shape how Legrand is approaching innovation under the Eliot program.

For more information on Eliot, visit www.legrand.us/about-us/eliot.
 

###

 
About Wattstopper

Wattstopper, a product line of Legrand, offers the most comprehensive line of simple, scalable and flexible energy efficient lighting controls and solutions for commercial and residential applications. The Wattstopper range of products, programs, and services have been helping customers save energy, meet green initiatives and comply with energy codes for more than 30 years. www.legrand.us/wattstopper.

 
About Legrand and Legrand, North & Central America

Legrand is a global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial, and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth, including, in particular, connected devices stemming from Legrand’s global Eliot (Electricity and IoT) program. Legrand reported sales of $5.6 billion in 2016. Legrand has a strong presence in North and Central America, with a portfolio of well-known product lines that include C2G, Cablofil, Electrorack, Luxul, Middle Atlantic, Nuvo, OCL, On-Q, Ortronics, Pass & Seymour, Pinnacle, QMotion, Quiktron, Raritan, Solarfective, Vantage, Wattstopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating, and DJSI (ISIN code FR0010307819) www.legrand.us.
 
###


Media contact:
Mary Placido
,Legrand Building Control Systems
415-218-3627 mary.placido@legrand.us