text.skipToContent text.skipToNavigation
Filter Results Selecting a filter will reload the page.
Category
Brand
Brand

Choose from one of Legrand's brands.

Type
Type

Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application

Color
Color

The color of the product itself

Certifications
Product Certifications

Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
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
Refers to the specific types of connections a device uses to join electrical conductors and create an electrical circuit. When you select the first desired connector, a second filter will appear listing any connectors on the opposite end of your selected connector on a device.

Temperature Rating
Temperature Rating

The Designated / Rated / Maximum / Range Temperature at Which the Instrument May be Used in Continuous Operation without Loss of its Basic Properties and performance

Conductor Size
Conductor Size

The Physical Dimension of Current Carrying Member of the Cable

Number of Ports
Number of Ports

The Number of Application-Specific or Process-Specific Software Construct Serving as a Communication Endpoint / is Generally a Specific Place for Being Physically Connected to Some Other Device /A Number of Physical Access Point(S) Between a Conductor and

Rack Units
Rack Units Rack Units_030104

Unit Used to Describe the Height of Equipment Intended for Mounting

Number of Conductors
Number of Conductors

The Number of Materials/Strands/Pairs Which Contain Movable Electric Charges

Impedance
Impedance

A Material's Opposition to the Flow of Electric Current

Simplex/Duplex
Simplex/Duplex

A Communications Network can Provide one-Way / Multi-Way Communication Service

Wire Gauge
Wire Gauge

Measuring and Indicating a Quantity of Wire

Cable Length
Cable Length

The Longest Dimension of Insulated Conductors

Product Family
Product Family

Used to identify and differentiate offerings within a particular product line. Product families are typically treated as adjectives. It is not recommended to use the product line (ex: Wiremold®) and product family names (Evolution™) together. This will introduce a level of unnecessary confusion for the audience.

Conductor Material
Conductor Material

The Material of Current Carrying Member of the Cable

Operating Temperature
Operating Temperature

The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit

Product Width
Product Width

The overall width of the product.
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
Jacket Material
Jacket Material

The outer material used to insulate a cord or cable's wiring.

Insulation Thickness
Insulation Thickness

Describes the specific width of insulation material used by a device for electrical retention, signal conservation, general safety, etc.
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
Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.

Conductor Stranding
Conductor Stranding

Indicates the configuration of wires used for electrical conduction. Solid conductors provide greater current capacity and increased durability, while stranded conductors provide greater flexibility.
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
Product Depth
Product Depth

The overall depth of a product.

Capacitance
Capacitance

Describes the ability of two conductors to store electrical energy, which can impact a cable's signal propagation and delay.

Jacket Application
Jacket Application

Describes the specific application(s) a cable's jacket is designed to be used in, such as in-wall, plenum, or riser.

Country of Origin
Product Height
Product Height

The overall height of a product.

SHOW MORE SHOW LESS
Connectivity Footprint
Connectivity Footprint

Refers to the unique application or solution that products like connectivity adapters, jacks, or panels can fit within or are compatible with.
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
Typical Insertion Loss
Typical Insertion Loss

Refers to the most common amount of signal lost at a connection/mating point, measured in decibels (dB).

Product Length
Product Length

The overall length of a product.
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
Denotes the NEC (National Electric Code) standards the outer casing/jacket surrounding a cable or cord's internal wiring and insulation is rated to.

Shuttered Adapters
Shuttered Adapters

Refers to to the cap/door mechanism on a panel or insert that remains closed to help prevent contaminants from entering the ferrule end face, but can be opened to insert/install a connector.
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
22 Products available