text.skipToContent text.skipToNavigation

What Is a Pop‑Up Outlet? Key Considerations Before Installation

June 8, 2026

Pop‑up outlets have become a popular solution for adding power on kitchen islands, peninsulas, and workspaces where clean design matters. While they offer flexibility and a modern aesthetic, pop‑up countertop outlets come with specific functional, safety and code considerations that are important to understand before installation. 

This guide explains what a pop‑up outlet is, how it works, and what you should consider to determine whether it’s the right fit for your space. 

What Is a Pop‑Up Outlet?

A pop‑up outlet is a type of electrical receptacle installed directly into a countertop or work surface. When not in use, the outlet remains flush or nearly flush with the surface. When power access is needed, the unit is activated—typically by pressing or lifting—to raise the receptacles above the countertop. 

Most pop‑up countertop outlets include: 

  • One or more standard 120V receptacles 
  • A spring‑loaded or mechanical lift mechanism 
  • A housing that installs through a cutout in the countertop 

Code Requirements That Apply to Pop‑Up Outlets

Pop‑up outlets are subject to several National Electrical Code (NEC) rules, particularly when installed in kitchens. Importantly, not all pop‑up outlets are code‑compliant by default, so proper product selection matters. 

Key NEC considerations include:

GFCI Protection

Pop‑up outlets installed in kitchens generally require Ground‑Fault Circuit Interrupter (GFCI) protection due to proximity to water and countertop use. This protection may be built into the outlet or provided upstream at the circuit breaker or another receptacle. 

Tamper Resistance

Kitchen receptacles must typically be tamper‑resistant (TR) to prevent accidental contact—especially in homes with children.  

Accessibility and Usability

Code and safety standards also address how easily an outlet can be used: 

  • The outlet must be listed for countertop installation 
  • Controls should be operable without excessive force 
  • The unit must remain stable and safe when extended 

Because code interpretations can vary by jurisdiction, it’s critical to verify that the specific pop‑up outlet model is approved for countertop use in your location. 

Key Considerations Before Installing a Pop‑Up Outlet 

Before cutting into a countertop, evaluate both the physical constraints and how the outlet will be used day to day.

Countertop Thickness and Material

Pop‑up outlets require a minimum countertop thickness and under‑counter clearance to house the lift mechanism and wiring. Natural stone, quartz, solid surface, and butcher block may all have different installation requirements. Pop-up outlets can require cutting a hole in a countertop of more than 4 inches. 

Key questions to confirm: 

  • Does the outlet meet the minimum depth required by the manufacturer? 
  • Is the countertop material compatible with the installation method? 
  • Will drilling the cutout affect structural integrity or warranties? 

Under Counter Space

Pop-up outlets may require significant space underneathe the countertop, so it’s important to check any cabinetry or plumbing that could be potentially in the way.  

While there are varying sizes of pop-up outlets, they can be as large as 15 inches below the countertop.

Moisture and Spill Protection

Kitchens are spill‑prone environments, which makes sealed designs critical. Look for pop‑up outlets that: 

  • Include gasketed or sealed lids 
  • Are rated for countertop use in damp locations 
  • Prevent liquids from entering the electrical housing when closed 

Poorly sealed units can become safety hazards or fail prematurely.

Inspection and Approval

Not all pop‑up outlets are evaluated the same way. Before installation, confirm that the unit is: 

  • UL or ETL listed 
  • Specifically approved for countertop use (not just furniture or commercial applications) 
  • Accepted by local inspectors 

Choosing a listed and approved product helps avoid failed inspections and costly retrofits. 

Pop‑Up Outlet Pros and Cons

Like any electrical solution, pop‑up outlets offer advantages and tradeoffs. 

Pros 

  • Provides access to one or more outlets exactly when needed 
  • Remains flush with the countertop surface when not in use 
  • Helps maintain a clean, uncluttered kitchen design 
  • May include USB outlets for additional charging flexibility 

Cons 

  • Can be bulky and difficult to keep clean 
  • Outlet and installation costs can be higher than traditional options 
  • Users with mobility or dexterity limitations may find the mechanism challenging 
  • Lift mechanisms or springs can wear over time and malfunction 
  • Extended units may obstruct usable countertop workspace 
  • Requires sufficient under counter clearance, which may interfere with cabinetry, drawers, or plumbing 

Pop-Up Outlet vs. Surface Mount Outlet

Unlike a pop-up outlet, a surface mount outlet on a kitchen countertop offers a solution with a smaller footprint, fast installation and less hardware. Offering a sleek alternative that is easy to keep clean and maintain over long-term use, a surface mount outlet can be installed with or without a lid to easily blend in while always being accessible. 

Learn more about the Legrand surface mount Kitchen Countertop Outlet.