text.skipToContent text.skipToNavigation

Streamlining Data Center Infrastructure with Effective Cable Management

In the fast-paced world of data center management, you might deprioritize cable management. As technology evolves and new equipment is deployed in the cabinet, the importance of cable management cannot be overstated. If cables become untidy and cluttered, they can cause many problems, including poor airflow, underperforming equipment, and higher energy costs.

As more hardware is added, so is more cable. If technicians don’t organize the wiring with each addition or change, they may end up with a spaghetti-like mess that hinders equipment performance and airflow.

A well-organized cable infrastructure makes it easier to identify each cable for troubleshooting, moving and adding equipment, and retrofitting. Proper management involves routing cables neatly, placing copper and fiber in separate trunks, keeping cables away from power distribution unit (PDU) cords, and shortening the distance between connections to reduce the cost of materials.

Good cable management results in fewer troubleshooting tickets. When issues occur, it’s easier to address them. Knowing what each cable connects to which component accelerates troubleshooting. 

Separate Copper and Fiber Pathways


A fundamental aspect of proper cable management is the separation of copper from fiber. Copper and fiber have very different characteristics. Fiber is immune to electrical magnetic interference, while copper is susceptible to its effects. By separating these trunks, you can minimize the risk of interference while simplifying cable management. 

Copper is highly conductive, and as such, it is very useful for transferring heat to cooling systems. However, the insulation around the copper wire, typically made of plastic or cotton, can trap heat at the back of the cabinet. Organizing the cables to allow proper ventilation is essential to optimizing equipment performance.

Energy Efficiency and Costs


Efficient airflow management is critical to data center operations. Disorganized, untidy cables create clutter, which can interfere with airflow, leading to hot spots and increased cooling costs. This is especially true in modern data centers, where increased equipment density reduces the amount of usable space. In order to dissipate heat efficiently and prevent equipment damage, cable trays, racks, and other tools should be utilized to keep cables out of the way of airflow paths. 

Maintenance and scalability


A well-organized cable layout makes adding hardware and replacing or moving equipment easier. For example, it prevents technicians from wasting time tracking connections to ensure they don’t unplug the wrong cord. As such, proper cable management, including labeling, color-coding, and documentation, improves maintenance and makes it easier to scale. Modular and scalable cable management solutions, such as patch panels and modular trays, can also facilitate future expansion, as they allow reconfiguration without disruption. 

Staff Productivity and Safety


Tangled cables are a hazard in many respects, potentially hindering staff productivity and safety. Besides forcing technicians to spend longer on maintenance, disorganized cables compromise safety by creating hazards, making it easier to disconnect a device by accident, and potentially causing injuries. 

Furthermore, if cables aren’t properly ventilated or are allowed to touch PDU power cords, they increase the risk of overheating, which can damage equipment and even start fires if properly rated cables aren’t used. By maintaining organized cabling, data center managers can reduce the risk of overheating and human error, ensuring more reliable operations.

For more information, view the Cabinet Accessories Catalog to ensure safe and effective cable organization and management.