text.skipToContent text.skipToNavigation

Legrand Nuvo P30 Touch Screen Ccontroller Offers Intuitive In-Wall System Operation


​​​​​​​AMSTERDAM., February 7, 2017 – Legrand, the global specialist in electrical and digital building infrastructures, announced the availability of its Nuvo P30 touch screen system controller, a fully functioning seven-inch Android tablet housed in a custom enclosure that runs the existing Player Portfolio app. It gives users the choice between handheld control via the apps for android & iOS or in-wall use to suit all music listening experiences.

In addition to being the access point for system control, the touch screen (NV-P30-BK) will run popular streaming services and apps, including Spotify, Pandora and more. You can also access and play music stored on networked devices in the home through the Player Portfolio system.

“The Nuvo P30 touch screen and Player Portfolio app offer intuitive easy in-wall control of the whole home audio system. If you’re simply adjusting the source and volume for a relaxing night at home, or playing DJ for a gathering of friends and family, it’s right there,” said Walt Zerbe, Legrand’s product manager for audio. “The in-wall control option is especially convenient for muting or lowering volume quickly when there's a knock at the door, or allowing immediate access to preset source favorites without searching for a phone or tablet.”

The 7-inch touch panel has a high contrast 1024 x 600 IPS capacitive screen and a sleek design that blends easily into any room’s décor. The included mounting plate makes installation simple. Its connection to the Player Portfolio system is made via a single RJ45 802.11af PoE connection.

The Nuvo P30 touch screen will be available in March for MSRP $349.

For more information on Legrand’s Nuvo P30 touch screen, please click here.

Join the conversation on Legrand Nuvo’s Twitter, Facebook and LinkedIn pages.

 

About Legrand

Legrand is a global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth, including, in particular, connected devices stemming from Legrand’s global Eliot (Electricity and IoT) program. Legrand reported sales of $5.3 billion in 2015. Legrand has a strong presence in North and Central America, with a portfolio of well-known product lines that include C2G, Cablofil, Electrorack, Luxul, Middle Atlantic, Nuvo, On-Q, Ortronics, Pass & Seymour, Pinnacle, QMotion, Quiktron, Raritan, Solarfective, Vantage, Wattstopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating and DJSI (ISIN code FR0010307819) www.legrand.us. 

 

#  #  #

 

Media Contacts:

Feintuch Communications
Doug Wright / Richard Roher                         
212-808-4903 / 212-808-4902
legrand@feintuchpr.com