COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

LEGRAND UNVEILS THE NUVO P600, WORLD’S FIRST DIN RAIL STREAMING PLAYER THAT SUPPORTS POPULAR STREAMING SERVICES

Full-Featured Audio Player Supports Spotify, Pandora, Among Others


AMSTERDAM, February 6, 2018—Legrand, the global specialist in electrical and digital building infrastructures, introduces the Nuvo P600 Player, the world’s first DIN rail streaming player that supports popular music streaming services, including Spotify, Pandora, Napster and Deezer.

Compatible with the DIN rail mounting system heavily adopted throughout Europe and the rest of the EMEA, the new player is compatible with all other in-room and rack-mounted models in Legrand’s expanding ecosystem of Nuvo Player Portfolio streaming players. The Nuvo Player Portfolio system supports as many as 16 players and 16 simultaneous, independent streams.

The P600 Player also gives any room instant access to endless music options from networked collections or a variety of Internet radio and streaming services, all controlled with the intuitive Nuvo Player Portfolio app. For efficiency and quality, the P600 features a built-in Class D digital amplifier and supplies up to 40 watts of power to a single zone.

Designed for DIN rail mounting, the P600 can be conveniently installed alongside compatible devices from Legrand and other manufacturers on the rail. Power to the P600 is provided through Legrand’s new P601 power supply, and one P601 can be used to power four P600 players.

“The Nuvo P600 Player adds ease of installation and flexibility for international installers to specify, sell, and expand Nuvo Player Portfolio systems in homes and light commercial settings,” said Fritz Werder, Legrand’s VP/general manager of the Nuvo and On-Q product lines. “We are very excited to debut this innovative and flexible model at ISE 2018, where we know our dealers and distributors are looking for a DIN solution.”

The P600, like all players in the Nuvo Player Portfolio system, is compatible with Nuvo in-wall keypads, the Nuvo Player app for iOS and Android devices, the P500 Sound Bar and Subwoofer, and the P400 Tabletop Speaker, among others, so users can easily create a complete multi-room audio solution. It can also be integrated into third-party control platforms including Vantage, Bticino, Control4, Crestron, KNX, URC, RTI and more, as well as with the Domotz PRO remote network management platform for an improved dealer experience in troubleshooting and support scenarios.

For more information on the Nuvo P600, please click here.

About Legrand and Legrand, North and Central America

Legrand is a global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial, and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth, including, in particular, connected devices stemming from Legrand’s global Eliot (Electricity and IoT) program. Legrand reported sales of $5.6 billion in 2016. Legrand has a strong presence in North and Central America, with a portfolio of well-known market brands and product lines that includes AFCO Systems, C2G, Cablofil, Chief, Da-Lite, Electrorack, Finelite, Luxul, Middle Atlantic Products, Milestone AV, Nuvo, OCL, On-Q, Ortronics, Pass & Seymour, Pinnacle, Projecta, QMotion, Quiktron, Raritan, Sanus, Server Technology, Solarfective, Vaddio, Vantage, Wattstopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating, and DJSI (ISIN code FR0010307819) www.legrand.us.