text.skipToContent text.skipToNavigation

New Legrand 42” Plastic Enclosure Easily Integrates Wireless Devices Into Structured Wiring Installations


MIDDLETOWN, PA., August 29, 2017 – Legrand, the global specialist in electrical and digital building infrastructures, introduced its 42” Plastic Enclosure (ENP4250), which is transparent to radio frequencies to enable placement of wireless devices into traditional structured wiring installations without interference or reduction of signal coverage.

Made with a sturdy, durable ABS plastic, the enclosure features a universal mounting grid that maximizes its compatibility with third-party products without requiring additional brackets. The unique design also allows it to be utilized for surface- or recess-mounted applications. Extra venting along the door for heat dissipation and staggered mounting tabs allow multiple enclosures to mount in adjacent stud bays.

“Following on the success of our 30” inch plastic enclosure, this 42” model offers the accessibility and convenience that will make it a staple for installers tasked with outfitting homes with larger and more complex systems that combine wired and wireless devices,” said Fritz Werder, Legrand’s VP/general manager for the On-Q and Nuvo lines. “Its intelligent, innovative design is also compatible with a wide array of Legrand and third-party products, another key benefit that makes life a little easier for installers.” 

The 42” plastic enclosure features an extended cover that adds 1.2” of depth for cable headroom and third-party device flexibility. The metal hinge on the cover attaches to either the right or left side of the enclosure in seconds without the need for tools or a second set of hands. The enclosure can be locked using included screws.

The tapered design allows enclosures and covers to stack for efficient transportation and warehousing. Available bulk packs of enclosures and doors offer added convenience and value for larger jobs.

The 42” enclosure (ENP4250) is currently available for MSRP $149.00.

For more information on this product, please click here.

About Legrand and Legrand, North & Central America

Legrand is a global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth, including, in particular, connected devices stemming from Legrand’s global Eliot (Electricity and IoT) program. Legrand reported sales of $5.6 billion in 2016. Legrand has a strong presence in North and Central America, with a portfolio of well-known product lines that include C2G, Cablofil, Electrorack, Luxul, Middle Atlantic, Nuvo, OCL, On-Q, Ortronics, Pass & Seymour, Pinnacle, QMotion, Quiktron, Raritan, Solarfective, Vantage, Wattstopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating and DJSI (ISIN code FR0010307819) www.legrand.us

# # #


​​​​​​​Media Contacts:

Feintuch Communications

Doug Wright / Richard Roher

212-808-4903 / 917-207-9604

legrand@feintuchpr.com