text.skipToContent text.skipToNavigation
Filter Results Selecting a filter will reload the page.
Category
Brand
Brand

Choose from one of Legrand's brands.

Type
Type

Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application

Color
Color

The color of the product itself

Certifications
Product Certifications

Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.

SHOW MORE SHOW LESS
Standard
Standard

The industrial standard(s) to which a device is manufactured, operated, or tested.

SHOW MORE SHOW LESS
Frequency Band
Frequency Band

A Continuous Group, or Range, of Frequencies with an Upper Limit and a Lower Limit

Sensor Type
Sensor Type

The Device that Receives a Signal or Stimulus (As Heat or Pressure or Light or Motion Etc.) and Responds to it in a Distinctive Manner

Installation Location
Installation Location

Where a Device is or is to be Installed

NEMA Rating
NEMA Rating

National Electrical Manufacturers Association Ratings are Standards that are Useful in Defining the Types of Environments in Which an Electrical Enclosure can be Used

Compatibility
Compatibility

Capability of Being Used with or Connected to Different Types of Devices or Components without any Modifications

SHOW MORE SHOW LESS
Antenna
Antenna

A Conductor or Set of Conductors Used to Radiate RF Energy Into Space or to Collect RF Energy from Space or to Do Both

Indoor/Outdoor
Indoor/Outdoor

Enviromental Conditions rating on the product. Indoor Only, Outdoor, Both

Timer Duration
Timer Duration

Amount of Time a Timer can Last

Input Voltage
Input Voltage

The Difference of Electrical Potential Between Two Points of an Electrical or Electronic Circuit Entering a System

SHOW MORE SHOW LESS
Number of Buttons
Number of Buttons

The Number of Keys/Switches in the item Used for Selecting a Particular Function

Mounting Type
Mounting Type

The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.

SHOW MORE SHOW LESS
Has Battery
Has Battery

A Device for Converting Chemical Energy Into Electrical Energy a Group of Two or More Connected Voltaic Cells

Response Frequency
Response Frequency

Frequency response is the quantitative measure of the output spectrum of a system or device in response to a stimulus, and is used to characterize the dynamics of the system. It is a measure of magnitude and phase of the output as a function of frequency, in comparison to the input.

Wire Size
Wire Size

It is the Normal Size of the Conductors for Building Wire

Load Rating
Load Rating

The maximum load that a device is designed to withstand without breakage or loss of performance.

SHOW MORE SHOW LESS
Battery
Battery

A Device for Converting Chemical Energy Into Electrical Energy a Group of Two or More Connected Voltaic Cells

Encryption
Encryption

The Activity of Converting Data or Information Into Code

Connection Type
Connection TypeTooltip Title

Style or Type of Connection Used

Product Family
Product Family

Used to identify and differentiate offerings within a particular product line. Product families are typically treated as adjectives. It is not recommended to use the product line (ex: Wiremold®) and product family names (Evolution™) together. This will introduce a level of unnecessary confusion for the audience.

Sensing Range
Sensing Range

The total Possible Sensing Capability of the Sensor, Beginning After the Deadband, and Extending Out as Far as the Sensor is Able to Reach Effectively

SHOW MORE SHOW LESS
Operating Temperature
Operating Temperature

The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit

SHOW MORE SHOW LESS
Included
Included

The Supplementary items Supplied with the Product Which May be Necessary for the Optimum Operation of the Product

SHOW MORE SHOW LESS
Product Width
Product Width

The overall width of the product.

SHOW MORE SHOW LESS
Product Has Potential to Contribute to LEED
Product Has Potential to Contribute to LEED

This product contributes to earning credits in the LEED rating system.

Wire Connection Type
Wire Connection Type

Describes the method used to connect wires to the device, such as screw terminals, push-in connectors, or lead wires.

SHOW MORE SHOW LESS
Operating Temperature Min
Operating Temperature Min

Indicates the lowest possible temperature a device can be safely used without the risk of failure or damage.

Battery Life
Battery Life

Describes the approximate amount of time a battery can power a device before it needs to be recharged or replaced.

Security Method
Security Method

Describes the functions or methods used by a device or software to protect against unauthorized access to a device or software platform.

On Function
On Function

Describes the mode of operation for devices that can be turned on, indicating whether they stay on continuously or operate on a timer or sensor.

Battery Capacity
Battery Capacity

Describes the maximum amount of electrical charge that a battery can store and deliver. 

Engraving Type
Engraving Type

Refers to the available styles to mark or inscribe text, symbols, or patterns on a product.

Seismic Tested
Seismic Tested

Indicates whether a device has been tested to withstand and/or perform under certain seismic conditions.

Sensor Coverage
Sensor Coverage

Describes the total area, measured in square footage, within which a sensor can detect presence or movement.

SHOW MORE SHOW LESS
Antenna Pattern
Antenna Pattern

Captures the directional representation of how radio waves are sent and received by the antenna.

Sensitivity Adjustment
Sensitivity Adjustment

Refers to any customization settings, or range of adjustments for motion detection sensitivity, required to turn lights on.

Storage Temperature
Storage Temperature

Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.

Indicator
Indicator

Describes the type/specification of signaling a device uses to indicate abnormal and/or operating conditions.

Antenna Gain
Antenna Gain

A calculated measure of how effectively an antenna sends or receives radio signals in a particular direction, measured in dBi (Decibals relative to isotropic).

Timer Type
Timer Type

The mechanism by which the timer operates, such as mechanical, digital, or programmable.

Antenna Type
Antenna Type

Refers to the design or style of antenna used within a device, which can impact signal direction, range, and performance in wireless communication.

Product Depth
Product Depth

The overall depth of a product.

SHOW MORE SHOW LESS
Topology
Topology

The arrangement in which the Nodes of a LAN are connected to each other.

Sensor Coverage Pattern
Sensor Coverage Pattern

Describes the shape of the area that a sensor is able to detect presence or movement within, measured in degrees.

Horsepower Rating
Horsepower Rating

Refers to the power capacity of a device under normal load conditions, measured in horsepower (HP).

Current Draw
Current Draw

The amount of electrical current the device uses during operation, measured in amperes (or amps).

SHOW MORE SHOW LESS
Operating Humidity
Operating Humidity

Describes the range of humidity at which a device can be utilized safely without the risk of failure or damage.

Product Series
Product Series

A collection of related products that share a common design, technology, or purpose. Products within the series either maintain a cohesive brand / style identity or work together to serve a particular solution.

SHOW MORE SHOW LESS
Country of Origin
Product Height
Product Height

The overall height of a product.

SHOW MORE SHOW LESS
Switch Type
Switch Type

Refers to the style or operation method used by a switch to control lighting or other electrical devices.

Wireless Range
Wireless Range

Describes the maximum distance wireless devices can be separated while preserving signal quality and reliability.

Line Frequency
Line Frequency

The frequency of alternating current (AC) in an electrical power system, measured in Hz. Also commonly referred to as Utility Frequency, Power Line Frequency, or Mains Frequency.

Sensor Technology
Sensor Technology

The technology used by a device to sense a change in signal or stimulus.

Operating Temperature Max
Operating Temperature Max

Indicates the highest possible temperature a device can be safely used without the risk of failure or damage.

SHOW MORE SHOW LESS
Product Length
Product Length

The overall length of a product.

SHOW MORE SHOW LESS
Ultrasonic Frequency
Ultrasonic Frequency

Describes the specific frequency at which a sensor emits and detects sound waves in order to measure distances, detect objects, or perform other functions.

Light Level Adjustment
Light Level Adjustment

Captures the range over which a device can adjust the intensity of light in order to maintain the desired ambient light setpoint, enhancing comfort and energy savings.

Number of Rockers
Number of Rockers

The total number of rocker-type electrical switches included on a device. Typically used to switch between two or more functions.

Sensor Mounting Height
Sensor Mounting Height

Describes the optimal vertical distance at which a sensor should be installed to ensure reliable detection of motion or other target conditions.

SHOW MORE SHOW LESS
Location Rating
Location Rating

Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.

Application Sector
Application Sector

Refers to the expected environment(s) or intended usage(s) for a product (e.g. Residential, Commercial, Industrial, etc.).

Warranty Type
Warranty Type

The product warranty that accompanies the specific product.

Features
Features

Unique characteristics and functionality that set the product apart from others in its field.

SHOW MORE SHOW LESS
Finish
Finish

Describes the specific surface treatment applied to the outer product for either aesthetics and/or durability.

Material
Material

Indicates the primary material(s) used to construct a product.

Footprint

45 Products available
  • 1(current)
  • 2
  • 1(current)
  • 2