USB Charging Outlet vs. Device Compatibility Guide
June 30, 2026
A USB charging outlet offers less clutter and faster charging speeds than the traditional charging block set-up – plus you don’t have to go searching for a charging block whenever a battery runs low. As an increasingly popular alternative to standard wall outlets in the home, USB outlets are convenient and efficient. But before you install a USB charging outlet, consider the types of devices that will be charged and the location in the home.
What to Know About USB Outlet and Device Compatibility
When choosing the right USB outlet to install, one of the first things to consider is the types of devices that will be charged. Phones, tablets and laptops are common devices, but don’t forget about other items like speakers, gaming consoles, lights, headphones and more.
Type A USB Outlets: A Thing of the Past
USB‑A, the familiar rectangular port, worked well when phones needed minimal power. Most USB‑A outlets deliver 12 watts or less, which was fine for early smartphones. But modern devices are thinner, more powerful, and far more demanding.
Today’s smartphones and tablets require significantly more power to charge efficiently. Newer iPhone and iPad models, for example, draw between 20–35 watts for optimal charging. When plugged into a USB‑A outlet capped at 12W, charging can take twice as long—or fail to charge altogether.
The Upgrade: USB‑C with Power Delivery (PD)
USB‑A, the familiar rectangular port, worked well when phones needed minimal power. Most USB‑A outlets deliver 12 watts or less, which was fine for early smartphones. But modern devices are thinner, more powerful, and far more demanding.
Today’s smartphones and tablets require significantly more power to charge efficiently. Newer iPhone and iPad models, for example, draw between 20–35 watts for optimal charging. When plugged into a USB‑A outlet capped at 12W, charging can take twice as long—or fail to charge altogether.
The Upgrade: USB‑C with Power Delivery (PD)
USB‑C with Power Delivery (PD) is designed for modern device compatibility. PD is a smart charging technology that communicates directly with your device to deliver exactly the power it needs—no more, no less.
- A MacBook requests 65W → PD supplies 65W
- A smartphone requests 20W → PD automatically steps down
The result? Faster charging, no overheating and no wasted energy—every device charges safely and efficiently from the same outlet.
Next‑Gen Power: GaN Technology
Many high-quality USB Type-C PD outlets now use GaN (Gallium Nitride) technology, a major leap forward from traditional silicon. GaN improves efficiency and reduces heat, allowing outlets to deliver more power in a smaller, sleeker form factor—perfect for today’s homes and workspaces.
For reliable, future‑ready charging, USB‑C PD outlets—especially those powered by GaN—offer the best compatibility with today’s and tomorrow’s devices.
The wattage of a USB outlet is marketed to showcase the speed and efficiency of its charging capabilities. As the devices we use daily evolve, power and performance must as well. When selecting a USB outlet, carefully check the wattage per-port. Some brands will market the combined wattage on the packaging, but it’s important to carefully check the maximum output marked on the device specifically. The product’s landing page and specification documentation will also clearly state the per-port wattage.
Key Considerations When Choosing the Right USB for a Device
- The Right USB Type: USB Type-C is the way of the future. This is the standard for all new devices and is a good option for anyone uncertain about which option to choose. While you may still have some devices at home that use the Type-A port, they are being phased out in new devices.
- Appropriate Wattage: The higher the wattage the more powerful devices the outlet will charge. If you’re looking to charge phones, tablets and laptops, a 65W USB is the way to go.
- High-Quality Safety and Efficiency Features: Power Delivery and GaN Technology ensure that a device is charging at top speed while not damaging devices. These features are crucial for long-lasting, durable USB charging.