text.skipToContent text.skipToNavigation

How to Spot a High-Quality USB Outlet

June 30, 2026

The market of USB receptacles is overwhelming, and choosing a high-quality option seems to get more challenging by the day. From port type to device compatibility to critical safety features, a USB outlet must meet high standards to meet the rigors of everyday device charging. But with the amount of devices that need charging, it’s increasingly important to install a high-quality USB outlet. 

Upgrading a USB outlet offers a slew of benefits for the end user – convenience, future-readiness, added value. However, installing a low quality USB outlet might have the opposite effect. If you’re ready to swap out standard outlets, take the time to understand the real-world benefits of USB outlets and the key considerations for choosing the right fit. 

The Growing Need for USB Outlets in Today’s Homes 

The modern home is more connected than ever. In fact, the average U.S. household had 17 connected devices in 2023, according to Parks Associates. From smartphones and wireless earbuds to tablets, laptops, and smart home accessories, nearly everything we use now competes for daily charging space. 

At the same time, many manufacturers have stopped including wall adapters with new devices. Major brands like Apple, Samsung, and Google now ship products with USB‑C cables only, leaving homeowners to figure out how—and where—to plug them in. The result? A growing reliance on in-wall USB outlets to keep devices powered and accessible. 

This shift isn’t slowing down. USB technology is rapidly standardizing across the industry: 

  • USB Type‑C ports are growing at a 24% annual rate 
  • USB Power Delivery (PD) is seeing 19% annual growth, driven by faster charging and higher power demands 
  • California will require all small electronic devices sold by 2026 to use USB‑C, accelerating nationwide adoption 

As charging needs increase and standards evolve, USB outlets are no longer a nice‑to‑have feature—they’re becoming an essential part of modern residential power design. 

Key Considerations of High-Quality Outlets 

When it comes to the quality of an electrical device, there are a few features that hold true whether you’re purchasing a standard outlet or a USB outlet.  

  • Tamper-Resistance: NEC-required safety for residential outlets. Tamper-resistant outlets are designed to ensure that foreign objects cannot be inserted into an outlet, which is especially important for households with little ones. 
  • UL Listing: Proof the outlet meets electrical safety standards. A UL Listing provides confidence that the outlet has been rigorously tested and passed strict standards that ensure it is safe to use. Some counterfeit brands have been known to print false or misleading UL markings on a device, so be sure to check this carefully. 
  • Brand Reputation: Reliable engineering and verified test data — not just marketing promises. There is a growing number of companies selling low quality devices at a low cost; however, low cost can come with safety and efficiency concerns. 
  • Warranty/Customer Service: It might not be top of mind when buying an electrical wiring device, but a warranty-backed product and company that offers customer service is important. Not only does it provide peace of mind in case of an issue, but it also shows the company is confident in its product quality. 
  • High-impact-resistant materials: For safety and longevity, a device must be constructed with quality materials. Lightweight plastic has weak thermal management and can easily damage with use. 

Why Choose USB Type-C Outlets

A key consideration for a high-quality USB is that it’s a Type-C port, but why? Think about the devices throughout the home – phones, tablets, laptops, headphones, speakers, gaming consoles... the list goes on. These devices are standardized to include USB Type-C charging cables so that consumers don’t have to worry as much about constantly collecting new cables that become obsolete in a year. While there may be some devices in the home that still use USB Type-A ports and cables, new products are exclusively compatible with Type-C. 

Indicators of a Low-Quality USB Outlet

  • Dimensional non-compliance: The device may exceed NEMA standards and not properly fit into a standard wall box. 
  • Missing or misleading UL/ETL logos: Means the device isn’t actually certified safe. 
  • Missing overcurrent protection: The device can exceed the max current rating of USB connectors and cables. 
  • Mismatched colors/finishes: Low quality devices lack consistency of colors and finishes that can leave a project feeling unfinished or mismatched. 

Frequently Asked Questions about USB Quality Considerations

Is it Worth to Buy High Quality USBs?

Yes, it’s worth it – from both a safety and experience perspective. While it often comes with a higher price tag up front, it also comes with critical safety features that keep personal devices protected and outlets working properly. Plus, high quality outlets deliver faster charging speeds. 

Do USB outlets draw power when not in use?

Yes, every USB on the marketplace draws some level of current. It’s not the full level of wattage, you’re not losing energy, but  

Do USB wall outlets charge faster? 

Typically, yes, USB wall outlets charge faster than using an adapter and standard socket. A high-quality USB outlet with sufficient wattage to support the charging needs of a device is required. 

How many watts is a USB wall outlet?

Look closely at the packaging and spec materials of a USB wall outlet to determine the wattage, as it varies by device. Be careful about misleading marketing that will promote the combined wattage of USB ports, rather than the wattage of each individual port. At Legrand, our USB outlets are available with up to 65 watts.


Subscribe to our channel and catch all the videos in our Rated Right. Built Right. Series.