5
Browse 546 results for
"power outlets"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Brand
Choose from one of Legrand's brands.
Product Family
Used to identify and differentiate offerings within a particular product line. Product families are typically treated as adjectives. It is not recommended to use the product line (ex: Wiremold®) and product family names (Evolution™) together. This will introduce a level of unnecessary confusion for the audience.
Product Series
A collection of related products that share a common design, technology, or purpose. Products within the series either maintain a cohesive brand / style identity or work together to serve a particular solution.
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Outlet Type
Describes the unique qualities or characteristics of an electrical outlet that make it better suited to different uses. The listed qualities may give the outlet improved safety performance, increased efficiency, or additional functionality.
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
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
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
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
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
Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.
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
Denotes the number of different services that can be used within a product as a result of separated internal compartments, including electrical, low voltage, water, air, and more.
Operating Temperature
The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit
Operating Temperature Max
Indicates the highest possible temperature a device can be safely used without the risk of failure or damage.
Storage Temperature
Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.
Is the Device Prewired?
Denotes whether a product comes prewired for quicker installation.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
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
Indicates whether a device is designed with a raised edge/rim, on or around its receptacle, for superior strength, handling, or attachment to another object.
NEMA Configuration Code
Alpha-Numeric Code Applied to Connectors to Guarantee Consistency and Interchageability Between Manufacturers
Output Voltage
The Voltage Measured at the Output Terminals of a Power Supply
USB Amperage
Describes the maximum electrical current the conductor or device can carry through its USB ports before sustaining immediate or progressive deterioration.
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
Refers to the distance between power outlets or receptacles on a device, which can be important for planning the layout of plugs and connectors.
Knockout Size
Physical dimension of the knock-out size, could be diameter or a range
Core Hole Size
Physical Dimensions of the hole
Internal Depth
Refers to the distance from the surface level of a box to the area where internal devices are plugged in, illustrating the available space within to accommodate cords, receptacles, and large devices.
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
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
The GO Wireway is a portable, pluggable wireway solution that installs on top of any flooring surface and plugs directly into any existing wall outlet.
To support power distribution requirements in network and server racks and cabinets, Legrand manufactures a range of Power Distribution Units (PDU) to meet the needs of your installation.
View adorne Power Outlets installed right by the bed in The Gates Hotel at Midtown Chicago.
View adorne Paddle Switches and Power/USB Outlets in the headboard of the Dream Hollywood’s guest beds.
Add power, USB charging, and switching connections directly to your furniture with the adorne Furniture Power Center. See how to elevate your furniture here.
The dash Desktop Power Center provides configurable and convenient access to power and data at the work surface with a high-end aesthetic.
View adorne Power and USB Outlets installed above this Quirk Hotel Richmond desk area in the guest room.
View adorne Power and USB Charging Outlets installed in the guest room at AC Miami Aventura.
View white adorne Outlets installed in the headboards at The Gates Hotel South Beach.
Legrand, a longstanding leader in the innovation and manufacture of electrical wiring devices, has announced the launch of their first Electric Vehicle (EV) Charger for residential applications.
What color options are available? Charging stations are available in black, bronze and silver, as well as custom colors. We can also add custom logos to the pedestal if desired. Can the station be used indoors or only outdoors? Technically, you could use the charging station indoors assuming you sink the L bolts into concrete. However, it is designed to offer maximum durability and to align with the UL requirements for outdoor use.
Legrand Expands Furniture Power Offerings Enabling Properties To Deliver Power Wherever Occupant Demand Requires.
View white adorne Outlets installed in the headboard of The Gates Hotel South Beach guest room bed.
Take a closer look at white adorne Outlets installed in The Gates Hotel South Beach guest room.
View adorne Power and USB Outlets installed above the desk in The Gates Hotel at Midtown Chicago.
View a headboard installation of adorne® Power and USB Outlets from the JW Marriott Mall of America guest room.
View adorne Power Outlets placed on either side of the bed of The Gates Hotel at Midtown Chicago guest room.
Legrand’s solutions transform hotel spaces, from lobby to guest room and beyond. Browse options for power and charging, connectivity, smart control and more.
View adorne® Switches and Outlets installed in the headboard of the Hilton Garden Inn Foxborough Patriot Place guest room bed.
View adorne® Power and USB Outlets mounted in the headboard for the JW Marriott Mall of America.
Understand the basics of USB charging, USB Type C and USB Type C connections, USB wall outlet charging benefits and why it’s time to update your chargers.
Lehigh University installs Legrand’s ModPower System in 110 desks across campus with enough power and charging for their students.
View how the Hilton Garden Inn Foxborough Patriot Place installed adorne Power and USB Charging Outlets above the desk in guest rooms.
View adorne Power and USB Outlets installed in the headboard of the JW Marriott Mall of America guest bed.
The adorne® Under-Cabinet Lighting and Power System uses an array of modular components that swap out so easily, you can reconfigure whenever the mood strikes.
Starline offers an innovative overhead power distribution system designed to supply and monitor critical power with a simple, safe, fast, reliable approach.
Take a look at how the adorne Furniture Power Center brings USB charging to JW Marriott Mall of America’s guest rooms—without sacrificing any style.
See how the AC Miami Aventura installed adorne® Switches and Outlets right in the headboard of the guest room bed.
View the guest room of JW Marriott Mall of America, where the bedside charging station is created with adorne Power and USB Outlets.
The new data center PDU represents a groundbreaking advancement in rack mount power strips by allowing the outlet to easily conform to any combination of hardware power configuration needs.