5
Browse 1,882 results for
"outlet"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Brand
Choose from one of Legrand's brands.
Product Family
Used to identify and differentiate offerings within a particular product line. Product families are typically treated as adjectives. It is not recommended to use the product line (ex: Wiremold®) and product family names (Evolution™) together. This will introduce a level of unnecessary confusion for the audience.
Product Series
A collection of related products that share a common design, technology, or purpose. Products within the series either maintain a cohesive brand / style identity or work together to serve a particular solution.
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Timer Type
The mechanism by which the timer operates, such as mechanical, digital, or programmable.
Outlet Type
Describes the unique qualities or characteristics of an electrical outlet that make it better suited to different uses. The listed qualities may give the outlet improved safety performance, increased efficiency, or additional functionality.
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
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
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
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
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
Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.
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
Describes the mode of operation for devices that can be turned on, indicating whether they stay on continuously or operate on a timer or sensor.
Lighting Types
Different forms of light a device is able to provide.
Service Capacity
Denotes the number of different services that can be used within a product as a result of separated internal compartments, including electrical, low voltage, water, air, and more.
Throw Type
Describes the method of switch operation, indicating whether it controls one circuit (single-throw) or switches between two circuits (double-throw).
Operating Temperature
The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit
Operating Temperature Max
Indicates the highest possible temperature a device can be safely used without the risk of failure or damage.
Storage Temperature
Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.
Is the Device Prewired?
Denotes whether a product comes prewired for quicker installation.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
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
Indicates whether a device is designed with a raised edge/rim, on or around its receptacle, for superior strength, handling, or attachment to another object.
Line Frequency
The frequency of alternating current (AC) in an electrical power system, measured in Hz. Also commonly referred to as Utility Frequency, Power Line Frequency, or Mains Frequency.
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
Describes the maximum electrical current the conductor or device can carry through its USB ports before sustaining immediate or progressive deterioration.
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
The total Possible Sensing Capability of the Sensor, Beginning After the Deadband, and Extending Out as Far as the Sensor is Able to Reach Effectively
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
A Convention or Standard that Controls or Enables the Connection, Communication, and Data Transfer Between Two Computing Endpoints, the Rules Governing the Syntax, Semantics, and Synchronization of Communication
Single/Multimode
Describes the mode of fiber either utilized or accepted by a device to transmit or receive a fiber optic signal.
Circular Outlet Diameter
Refers to the diameter of the circular opening in a wall plate, which should match the diameter of the outlet it is intended to cover.
Receptacle Spacing
Refers to the distance between power outlets or receptacles on a device, which can be important for planning the layout of plugs and connectors.
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
Refers to the distance from the surface level of a box to the area where internal devices are plugged in, illustrating the available space within to accommodate cords, receptacles, and large devices.
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
Publishing Date Range
Date article, blog, or press release was published.
Filter by Product Category
Filter downloadable resources by the product category they relate or are relevant to.
Brand
Choose from one of Legrand's brands.
Resource Type
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
Increase productivity and value provided to customers as you transform where people live and work with tools, resources and the solutions you need. Learn more.
Legrand is a global leader in network infrastructure solutions, with a broad range of copper and fiber connectivity, racks, cabinets and cable management.
Rhode Island has adopted a new building code, joining numerous cities and states in 2019 that have moved toward more stringent standards to increase energy efficiency and performance in commercial buildings.
Lighting industry leader, Legrand, has partnered with HGTV to be the exclusive supplier of the lighting controls charging and power outlets used throughout the HGTV® Smart Home 2017.
Legrand® Showcases Electrical Wiring Solutions Designed to Prevent Sanitation Issues, Corrosion, while Reducing Downtime at 2017 IPPE
Explore how Legrand products and solutions are used by our partners to improve their data center facilities needs.
Simplify and streamline your home network setup with the spacious On-Q 15" Plastic Enclosure. Offers easy installation, Wi-Fi-friendly design, and universal device compatibility - made in the USA.
Raritan’s CommandCenter® Secure Gateway (CC-SG) is an easy to deploy, plug-and-play appliance that provides IT administrators and lab managers with a secure, single point of remote access and control. With CC-SG, users can access and control their entire IT infrastructure from a single system, featuring BIOS-level, out-of-band KVM and serial access to a wide variety of computer and serial devices.
Integrate intelligent lighting controls at the luminaire level, offering granular control based on occupancy, daylighting, zones and more. View LLLC Solutions from Wattstopper.
Provide IT and network administrators secure, serial-over-IP access and control of serial devices with a powerful and easy-to use console server. Learn more.
Chroma Link™, a revolutionary color-indexed fiber optic cabling solution designed for hyper-dense AI and machine learning networks. Chroma Link offers a turnkey approach to connectivity that transforms data center deployments.
Legrand's Infinium Quantum™ Fiber System has been independently verified by Multilane to improve network performance and reduce CAPEX and OPEX.
Charge phones, tablets and small laptops up to 2X faster with USB C Power Delivery outlets with dual Type-C ports featuring up to 65 watts of power.
Simplify device mounting and cable management in the enclosure with On-Q solutions including Ratchet and Keyhole Post Clips, Cable Channels, and more.
The Connectrac Flex Raceways and ModPower System are adaptable solutions make reconfiguring spaces easy while maintaining power and data access. Learn More.
New connector innovations make it easier to make the right choices to provide more fiber optic connections in less space.
Legrand North & Central America today announced the availability of the Wattstopper Wireless DLM system. Wireless DLM builds upon the success of the original wired DLM system by extending its capabilities into IP-based wireless control.
Legrand announced an agreement with Florida-based Minto Communities to provide its On-Q and Pass & Seymour (P&S) products for more than 9,000 homes to be built in Daytona Beach, Fla., and Hilton Head, S.C.
Legrand announced that its radiant® RF (radio frequency) Lighting Control and adorne® Wi-Fi Ready Lighting systems now work with the Google Assistant for seamless voice control.
Legrand announced that its radiant® RF Lighting Control and adorne® Wi-Fi Ready Lighting systems now work with Amazon Alexa.
Lighting controls enable flexible lighting designs that meet needs of both patients and staff in emergency departments. Explore innovative solutions for the care environment.
Learn how to Specify the right lighting solution to optimize patient-centric care by taking these 11 lighting design tips for hospitals into consideration.
New Matter-enabled devices from the radiant® Collection, developed using Amazon’s Alexa Connect Kit for Matter, are on preview at the 2024 Consumer Electronics Show.
Significant changes are underway for commercial buildings with the 2015 Michigan Energy Code taking effect on September 20, 2017. This is the first commercial energy efficiency code update in more than six years for the state. The new code introduces a bevy of significant lighting control provision changes, which can be both confusing and daunting.
Legrand will showcase many innovative, productivity enhancing products at the 2018 National Electrical Contractors Association Show
To support power distribution requirements in network and server racks and cabinets, Legrand manufactures a range of Power Distribution Units (PDU) to meet the needs of your installation.
Vantage’s InFusion controller allows for future expendability, an important component for the owner as additional upgrades are planned.
Meta Description: Legrand has released a new demo case for dealers to elegantly showcase Designer Series Decorative Brackets and matching hembar endcaps to customers.
Consider some of these ideas for your next weekend project and add a little something extra, fresh, and new to your home.
Explore Legrand’s industry-leading structured wiring solutions from On-Q and Luxul products. Learn more today.