5
Browse 944 results for
"adorne"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Brand
Choose from one of Legrand's brands.
Product Type
Select a Product Type to find products that share the same basic form and function, such as switches, cables, panels, or electrical boxes.
Connector
A Device that Establishes a Connection Between Two or More Units.
Number of Receptacles
The Number of Electrical Wall Outlets Designed for Use with a Plug
Sensor Type
The Device that Receives a Signal or Stimulus (As Heat or Pressure or Light or Motion Etc.) and Responds to it in a Distinctive Manner
Amperage
Maximum electrical current the conductor or device can carry before sustaining immediate or progressive deterioration
Installation Location
Where a Device is or is to be Installed
Load
The Maximum Amount of Power Which the item can withstand or Operate without any performance Loss
NEMA Rating
National Electrical Manufacturers Association Ratings are Standards that are Useful in Defining the Types of Environments in Which an Electrical Enclosure can be Used
Phase
The Factional Part of the Period of a Sinusoidal Wave, Usually Expressed in Electrical Degrees and Referenced to the origin
Availability
Product is available to buy on Legrand.us
Compatibility
Capability of Being Used with or Connected to Different Types of Devices or Components without any Modifications
Product Certifications
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
Is Tamper-Resistant
Tamper resistance is resistance to tampering (intentional malfunction or sabotage) by either the normal users of a product, package, or system or others with physical access to it.
Number of Gangs
The amount of switches on the plate.
Connection
Between Discrete Points Allows the Flow of Electrons (Electric Current)
Temperature Rating
The Designated / Rated / Maximum / Range Temperature at Which the Instrument May be Used in Continuous Operation without Loss of its Basic Properties and performance
Is Weather Resistant
Is this product listed as Weather Resistant ?
Frequency Rating
The Number of Occurrences within a Given Time Period, the Rate at Which Alternating Current Makes a Complete Cycle of Reversals
Indoor/Outdoor
Enviromental Conditions rating on the product. Indoor Only, Outdoor, Both
Number of Ports
The Number of Application-Specific or Process-Specific Software Construct Serving as a Communication Endpoint / is Generally a Specific Place for Being Physically Connected to Some Other Device /A Number of Physical Access Point(S) Between a Conductor and
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Timer Duration
Amount of Time a Timer can Last
Input Voltage
The Difference of Electrical Potential Between Two Points of an Electrical or Electronic Circuit Entering a System
Number of Wires
The Number of Pliable Metallic Strand or Rod Made in Many Lengths and Diameters and are Electrically Insulated, Used Conduct Electricity
Timing Range
The Time Span for Which the System/Device is in Desired Active/Working Mode
Thickness
The Dimension Through an Object as Opposed to its Length or Width
Load Type
Denotes the type(s) of load that can be applied to a dimmer, which determines its compatible light sources.
Mounting Type
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
Current Rating
Maximum Amount of Current a Cable can Carry Before Sustaining Damage or Deterioration
Sensitivity
The Minimum Input Which the Device can Sense and Produce the Output
Number of Ways
The Number of Connections the Unit can Provide
Number of USBs
Number of USB ports
Wall Plate Color
Color of the Plate that Covers a Switch on a Wall
Contact
A Device that Joins Electric Conductors Mechanically and Electrically to Other Conductors and to the Terminals of Apparatus and Equipment
Wire Size
It is the Normal Size of the Conductors for Building Wire
Enclosure Type
Style, Type, Size, Etc. of the Enclosure of a Device
Construction
The Act or Process of Constructing Which Includes Design and Manufacture Type
Cord Length
The Linear Extent of Cord in Space from one End to the Other
Orientation
The Position or Alignment Relative to Points of the Compass or Other Specific Directions
NEMA Configuration Code
Alpha-Numeric Code Applied to Connectors to Guarantee Consistency and Interchageability Between Manufacturers
Load Rating
The maximum load that a device is designed to withstand without breakage or loss of performance.
Battery
A Device for Converting Chemical Energy Into Electrical Energy a Group of Two or More Connected Voltaic Cells
Wattage
amount of watts used
Connection TypeTooltip Title
Style or Type of Connection Used
Lighting Types
Different forms of light a device is able to provide.
Receptacle Type
The physical character of a Receptacle. The Type/Specification of a Contact Device Installed at the Outlet for the Connection of an Attachment Plug a Single Receptacle is a Single Contact Device with No Other Contact Device on the Same Yoke a Multiple Receptacle is Two or More Contact Devices.
Protocol
A Convention or Standard that Controls or Enables the Connection, Communication, and Data Transfer Between Two Computing Endpoints, the Rules Governing the Syntax, Semantics, and Synchronization of Communication
Color
The color of the product itself
Sensing Range
The total Possible Sensing Capability of the Sensor, Beginning After the Deadband, and Extending Out as Far as the Sensor is Able to Reach Effectively
Number of Switches
Number of electrical switches
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
Supply Voltage
The Specified Amount and Type Voltage / Voltage Range for Which the Equipment is Rated for Operation
Product Width
The overall width of the product.
Product Has Potential to Contribute to LEED
This product contributes to earning credits in the LEED rating system.
Wire Connection Type
Describes the method used to connect wires to the device, such as screw terminals, push-in connectors, or lead wires.
Preset
Denotes whether a dimmer returns lights to their previously-selected light level when turned on.
On Function
Describes the mode of operation for devices that can be turned on, indicating whether they stay on continuously or operate on a timer or sensor.
Seismic Tested
Indicates whether a device has been tested to withstand and/or perform under certain seismic conditions.
Sensor Coverage
Describes the total area, measured in square footage, within which a sensor can detect presence or movement.
Standard
The industrial standard(s) to which a device is manufactured, operated, or tested.
Cutout Shape
The geometric form of the cutout area, which must match the shape of the device or component being installed.
Device Front Face Size
Describes the general proportions of a product's front face relative to the overall device.
USB Wattage
Describes the maximum electrical power a USB receptacle can safely output.
Dimming Compatibility
Describes the method(s) used by a device or system to adjust the brightness of a lighting load.
Application Sector
Refers to the expected environment(s) or intended usage(s) for a product (e.g. Residential, Commercial, Industrial, etc.).
Trim/Adjustment Level
A control feature that allows the adjustment of the minimum and maximum light levels to prevent issues such as flickering at lower brightness levels, ensuring smooth and stable dimming performance.
Product Depth
The overall depth of a product.
Wall Plate Included
Indicates if the device comes with a cover plate for aesthetic integration with the wall.
Works With
Need to ensure your choice works with your device, system, or software? Select your needs using this filter to confirm compatibility.
Sensor Coverage Pattern
Describes the shape of the area that a sensor is able to detect presence or movement within, measured in degrees.
Dimming Phase
Refers to the point in the AC power cycle at which the dimmer begins to reduce voltage to the light. "Leading Edge" dimmers cut the initial phase and are typically used for incandescent bulbs, while "Trailing Edge" dimmers cut the end phase, which is more suitable for LEDs.
Horsepower Rating
Refers to the power capacity of a device under normal load conditions, measured in horsepower (HP).
Requires Neutral Wire
Indicates whether a device requires a neutral wire to function properly.
Wall Plate Type
Refers to the style or intended usage of a wall plate.
Operating Humidity
Describes the range of humidity at which a device can be utilized safely without the risk of failure or damage.
Connection Location
Specifies where on the device the electrical connections are made, which can affect installation.
Product Height
The overall height of a product.
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Throw Type
Describes the method of switch operation, indicating whether it controls one circuit (single-throw) or switches between two circuits (double-throw).
Line Frequency
The frequency of alternating current (AC) in an electrical power system, measured in Hz. Also commonly referred to as Utility Frequency, Power Line Frequency, or Mains Frequency.
Maximum Humidity
The highest level of atmospheric moisture a device can withstand without compromising functionality or safety.
Features
Unique characteristics and functionality that set the product apart from others in its field.
Number of Phases
Indicates the number of electrical phases a device utilizes.
Sensor Technology
The technology used by a device to sense a change in signal or stimulus.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
Internal Depth
Refers to the distance from the surface level of a box to the area where internal devices are plugged in, illustrating the available space within to accommodate cords, receptacles, and large devices.
Warranty Type
The product warranty that accompanies the specific product.
Wall Plate Size
The general size of the the included wall plate. The size may determine whether it suits your personal application!
Terminal Accommodation
Describes the type and size of wire that the receptacle's terminals can securely hold (typically provided as a range in gauge size).
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
Bulb Compatibility
Indicates the type(s) of lighting a dimmer or controller is designed to work with, ensuring proper functionality and performance.
Device Backbody Size
Describes the general proportions of a product's backbody relative to the overall device.
Outlet Type
Describes the unique qualities or characteristics of an electrical outlet that make it better suited to different uses. The listed qualities may give the outlet improved safety performance, increased efficiency, or additional functionality.
Location Rating
Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.
Category Performance Application
Refers to the specific standard used to define an ethernet cable's capabilities and its intended usage. Most commonly shortened to"Cat" and a number (e.g. Cat5e; Cat6; Cat6a).
Material
Indicates the primary material(s) used to construct a product.
Wiring Method
Describes the design and ways of connecting various parts of a device with cable and/or wire.
USB Amperage
Describes the maximum electrical current the conductor or device can carry through its USB ports before sustaining immediate or progressive deterioration.
Filter to Specific Product Groups
Filter by named groups of related products, including product families, series, systems, and solutions. Groupings may indicate similar styles of products, or signify how they're designed to operate together as a complete solution.
Stock Level
Filter your results to only in-stock products sold directly on legrand.us.
Brand
Choose from one of Legrand's brands.
Category
Our brands, products, resources, and pages are group into divisions. Filter and find a product, resource, or page you are looking for based on a Legrand category.
Filter by Product Category
Filter downloadable resources by the product category they relate or are relevant to.
Brand
Choose from one of Legrand's brands.
Resource Type
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
Check out our tips for upgrading your at-home workspace, featuring ways to maximize efficiency while including your own personal touch.
Read how blogger Leslie upgraded her kitchen into a colorful masterpiece, complete with Brushed Brass Wall Plates from the adorne® Collection.
Read how blogger Molly fell in love with the Pop-Out Outlet from the adorne® Collection during her bathroom upgrade.
Read how blogger Leslie used Brushed Brass Wall Plates from the adorne® Collection to enhance her space.
Read how Orlando Soria, interior designer and founder of Hommemaker, brightened up his space with designer switches and outlets from the adorne® Collection.
Start 2020 right; read our roundup of the top design trends for the new decade!
Summer is almost over. Whether your student will be heading back to class in person or online, here are some tools to help foster success this fall.
Read how bloggers Chris and Julia tackled three problem areas in their home, all in a single afternoon.
Legrand offers smart lighting solutions to fit every lifestyle, application or project.
Explore the year’s biggest design trends from Dallas Market 2019.
See how blogger Charlene transformed drab dimmers on her accent wall into a custom, touch-enabled statement piece with adorne.
Legrand’s solutions transform hotel spaces, from lobby to guest room and beyond. Browse options for power and charging, connectivity, smart control and more.
From apps to keep track of school supplies and schedule, to faster USB outlets with Power Delivery, here are our picks for Back to School tech.
Read how blogger Anne upgraded her home with designer switches and outlets from the adorne® Collection.
Designer switches and outlets are the perfect finishing touch. Explore options for elevating your property and enhancing the guest experience.
See how designer switches and outlets can enhance your space with clutter-free wireless charging and dimming capability.
Upgraded outlets in the playroom with built-in nightlights perfect for kids.
Blogger Colleen of Lemon Thistle upgraded her outlet to help her kids navigate the room more safely at night.
See how designer switches and outlets from the radiant Collection are available in a smooth nickel finish that perfectly complements a wide range of kitchen hardware.
See how designer switches and outlets can equip your kitchen with the necessary power to keep your mixer, blender, tablet and phone within reach.
See how designer switches and outlets can add modern functionality without compromising your space’s charm.
See how adorne and radiant can elevate the spaces where you celebrate, entertain, or share a delicious meal, with our photo gallery.
See how radiant Smart Lighting pairs with digital assistants like Google Home.
Spruce up the space you’ll be enjoying all summer, with these ideas for fantastic outdoor remodels and makeovers.
Nickel radiant switches and outlets add style and functionality to this master bathroom.
See how radiant GFCI outlets not only keep you safe, but look great too.
Stylish radiant outlet with built-in nightlight is perfect for the bathroom.
Less waste, less worry, with timed lighting control from the radiant® Collection. Never accidentally leave the lights again.