5
Browse 1,866 results for
"supports"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Product Family
Used to identify and differentiate offerings within a particular product line. Product families are typically treated as adjectives. It is not recommended to use the product line (ex: Wiremold®) and product family names (Evolution™) together. This will introduce a level of unnecessary confusion for the audience.
Product Series
A collection of related products that share a common design, technology, or purpose. Products within the series either maintain a cohesive brand / style identity or work together to serve a particular solution.
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Bottom Type
Bottom of Cable Tray
Enclosure Type
Style, Type, Size, Etc. of the Enclosure of a Device
Wall Plate Type
Refers to the style or intended usage of a wall plate.
Connector Type
The Type of Connectors / Terminals that Tool can Crimp to Wire or Cable
Connectivity Footprint
Refers to the unique application or solution that products like connectivity adapters, jacks, or panels can fit within or are compatible with.
Product Certifications
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
Features
Unique characteristics and functionality that set the product apart from others in its field.
Availability
Product is available to buy on Legrand.us
Material
Indicates the primary material(s) used to construct a product.
Mounting
Something that Serves as a Support, Setting, or Backing for the item
Mounting Type
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
Standard
The industrial standard(s) to which a device is manufactured, operated, or tested.
Amperage
Maximum electrical current the conductor or device can carry before sustaining immediate or progressive deterioration
Input Voltage
The Difference of Electrical Potential Between Two Points of an Electrical or Electronic Circuit Entering a System
Voltage
The Rate at Which Energy is Drawn from a Source that Produces a Flow of Electricity in a Circuit
Application Sector
Refers to the expected environment(s) or intended usage(s) for a product (e.g. Residential, Commercial, Industrial, etc.).
Indoor/Outdoor
Enviromental Conditions rating on the product. Indoor Only, Outdoor, Both
Installation Location
Where a Device is or is to be Installed
Mounting Hole Type
Describes the style of holes or openings used to either mount a device or mount to a device.
Compatibility
Capability of Being Used with or Connected to Different Types of Devices or Components without any Modifications
Load Capacity
The Greatest Amount of Loading that a Instrument can Receive without Violating Quality Standards
Operating Temperature
The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit
Operating Temperature Max
Indicates the highest possible temperature a device can be safely used without the risk of failure or damage.
Is the Device Prewired?
Denotes whether a product comes prewired for quicker installation.
Working Load
The maximum load that can be routinely applied to a component in straight tension.
Termination Style
The style of connection used for electrical termination between two devices.
Return Loss
Refers to the loss of power in the signal returned/reflected by a discontinuity in a transmission line or optical fiber.
Conductor Size
The Physical Dimension of Current Carrying Member of the Cable
Conductor Stranding
Indicates the configuration of wires used for electrical conduction. Solid conductors provide greater current capacity and increased durability, while stranded conductors provide greater flexibility.
Mesh Length
The overall length of a grip's mesh portion, which provides strength and protection to the cable.
Rung Spacing
Describes the distance between individual rungs in cable tray sections.
Tray Height
Refers to the approximate height of a cable tray used for specifying. Selecting a specific height will show cable trays with that height, as well as cable tray accessories compatible with that height.
Tray Length
Refers to the approximate length of a cable tray used for specifying. Selecting a specific length will show cable trays with that length.
Tray Width
Refers to the approximate width of a cable tray used for specifying. Selecting a specific width will show cable trays with that width, as well as cable tray accessories compatible with that width.
Cable Diameter Range
The range of cable diameters that the grip can accommodate, ensuring a proper fit.
Wire Gauge
Measuring and Indicating a Quantity of Wire
Rack Depth
Refers to the depth of a rack that is usable to support rackmount equipment.
Rack Units Rack Units_030104
Unit Used to Describe the Height of Equipment Intended for Mounting
Number of Gangs
The amount of switches on the plate.
Publishing Date Range
Date article, blog, or press release was published.
Filter by Product Category
Filter downloadable resources by the product category they relate or are relevant to.
Brand
Choose from one of Legrand's brands.
Resource Type
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
Find Legrand's Data Communications Training and Education Contractor Certification Courses here.
New line of PDU and UPS products provide a high-value, cost-effective power solution to complement existing physical infrastructure and connectivity portfolios.
Visit Legrand’s Lightapalooza booth and see how Vantage Lighting Controls and Legrand Shading Systems integrate for a fully customizable lighting experience.
Explore how Legrand’s approach to data center sustainability moves beyond power consumption and PUE towards a holistic way to address Scope 1, 2 and 3 emissions.
The Operations Management Program offers associates interested in industrial engineering or manufacturing leadership an accelerated path to joining the next generation of Legrand North and Central America (LNCA) operations leaders.
Creating accessible spaces for everyone is increasingly important in today's diverse environments. The Americans with Disabilities Act (ADA) of 1990 and the 2010 Standards for Public Accommodations, along with the Title III Requirements for Commercial Facilities, establish crucial regulations that ensure compliance with accessibility standards in commercial buildings. These guidelines not only promote inclusivity but also hold building owners accountable for designing accessible spaces that cater to the needs of all individuals, including those with disabilities.
Enjoy complete control over your home’s lighting with the touch of a button, with Legrand RF Lighting Control.
Get audited and controlled access to sensitive IT assets in your data center’s white space. Learn more about this economical and scalable solution.
Convention Center Series Floor Boxes are an industry leading solution for providing multiple utilities and services directly to the show floor.
Learn the basics of EV charging so you can make an informed decision when it comes to selecting and offering EV charging amenities. Learn more.
Design is what unifies our employees and separates us from our competition. Design is the very core of our culture.
Your guide to achieving better optical performance, increasing scalability, and lowering costs by phasing out cassette-based forms of cable management.
Smart Wi-Fi Light switches and dimmers from Legrand allow users to easily control light and power from a smart home lighting system or Matter hub.
Legrand is a trusted partner in realizing the sustainability goals and benefits of High Performance Buildings in the 21st century. Learn how to make your building a High Performance Building.
Leverage evolving technology and real-time data analytics to overcome facility manager challenges associated with post-COVID workplaces. Read the article to learn more.
Decarbonization of buildings and measuring embodied carbon of products is a growing trend in the building industry. In this blog post, Legrand summarizes major market initiatives and showcases our commitment to reducing our carbon footprint.
Vantage lighting controls helped this hotel meet its sustainability and design needs through freedom of design and providing energy-efficient lighting control.
Legrand®, a global specialist in electrical and digital building infrastructures, announced its sixth consecutive global Corporate Social Responsibility (CSR) Roadmap, outlining aspirational goals for 2025-2027.
From reliable infrastructure products to feature-rich smart systems, On-Q’s industry-leading solutions work together to form the backbone of the connected home. Learn more.
The T6 Server Cabinet is designed to address the challenges associated with high density server applications; cable management, airflow and load capacity.
Paint and Plate Pairings to Make Yours Walls a Work of Art.
Legrand donated Vantage lighting control and Legrand Shading Systems solutions to help provide more accessibility and freedom in customized R.I.S.E smart home
Legrand offers swing out wall mount cabinets and vertical wall mount cabinets ideal for environments where floor space is limited or only a small amount of networking is needed. Explore Legrand’s networking wall-mount cabinets.
Legrand, North & Central America recently announced the promotion of Amy Hahne as the new Vice President and General Manager of Shading Systems for its Building Controls Systems (BCS) division.
Extended height WattStopper occupancy sensor allows more facilities to benefit from digital lighting control solutions
Legrand announced a wide array of new products for the residential custom install market from several of its key brands that will be showcased across three booths at CEDIA 2016.
In the world of data centers, efficient and reliable power distribution is crucial for the smooth operation of AI servers.
Cisco selected the Infinium acclAIM Fiber Solution to run their Network Operation Center (NOC) at this year’s Cisco Live event in Las Vegas, NV.
The disaster-relief fundraiser for the American Red Cross will make a total contribution of $65,175 directed to individuals and regions affected by Hurricane Florence and Hurricane Michael.
All proceeds will be directed to individuals and regions affected by Hurricane Florence and Hurricane Michael.