5
Browse 1,025 results for
"dimmer"
Brand
Choose from one of Legrand's brands.
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Product Certifications
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
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
National Electrical Manufacturers Association Ratings are Standards that are Useful in Defining the Types of Environments in Which an Electrical Enclosure can be Used
Contact Rating
The Voltage, Current, and Power Capacities of Relay Contacts Under Specified Environmental Conditions
Compatibility
Capability of Being Used with or Connected to Different Types of Devices or Components without any Modifications
Is Tamper-Resistant
Tamper resistance is resistance to tampering (intentional malfunction or sabotage) by either the normal users of a product, package, or system or others with physical access to it.
Number of Gangs
The amount of switches on the plate.
Connection
Between Discrete Points Allows the Flow of Electrons (Electric Current)
Antenna
A Conductor or Set of Conductors Used to Radiate RF Energy Into Space or to Collect RF Energy from Space or to Do Both
Is Weather Resistant
Is this product listed as Weather Resistant ?
Contact Configuration
Different Switching Functions of the Relay Contacts
Frequency Rating
The Number of Occurrences within a Given Time Period, the Rate at Which Alternating Current Makes a Complete Cycle of Reversals
Indoor/Outdoor
Enviromental Conditions rating on the product. Indoor Only, Outdoor, Both
Timer Duration
Amount of Time a Timer can Last
Input Voltage
The Difference of Electrical Potential Between Two Points of an Electrical or Electronic Circuit Entering a System
Number of Wires
The Number of Pliable Metallic Strand or Rod Made in Many Lengths and Diameters and are Electrically Insulated, Used Conduct Electricity
Timing Range
The Time Span for Which the System/Device is in Desired Active/Working Mode
Availability
Product is available to buy on Legrand.us
Number of Receptacles
The Number of Electrical Wall Outlets Designed for Use with a Plug
Coil Voltage
The Electrical Pressure, the force Which Causes Current to Flow Through a Conductor
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
Dimmer
Devices Used to Vary the Brightness of a Light by Decreasing or Increasing the Rms Voltage and Hence the Mean Power to the Lamp it is Possible to Vary the Intensity of the Light Output
Sensitivity
The Minimum Input Which the Device can Sense and Produce the Output
Number of USBs
Number of USB ports
Wall Plate Color
Color of the Plate that Covers a Switch on a Wall
Mounting Type
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
Has Battery
A Device for Converting Chemical Energy Into Electrical Energy a Group of Two or More Connected Voltaic Cells
Response Frequency
Frequency response is the quantitative measure of the output spectrum of a system or device in response to a stimulus, and is used to characterize the dynamics of the system. It is a measure of magnitude and phase of the output as a function of frequency, in comparison to the input.
Wire Size
It is the Normal Size of the Conductors for Building Wire
Enclosure Type
Style, Type, Size, Etc. of the Enclosure of a Device
Construction
The Act or Process of Constructing Which Includes Design and Manufacture Type
Action
The Controlling Function performed by the Switch
Orientation
The Position or Alignment Relative to Points of the Compass or Other Specific Directions
NEMA Configuration Code
Alpha-Numeric Code Applied to Connectors to Guarantee Consistency and Interchageability Between Manufacturers
Speed Range
The Distance Traveled/Number of Revolutions in a Specific Interval of Time
Load Rating
The maximum load that a device is designed to withstand without breakage or loss of performance.
Battery
A Device for Converting Chemical Energy Into Electrical Energy a Group of Two or More Connected Voltaic Cells
Encryption
The Activity of Converting Data or Information Into Code
Connection TypeTooltip Title
Style or Type of Connection Used
Product Family
Used to identify and differentiate offerings within a particular product line. Product families are typically treated as adjectives. It is not recommended to use the product line (ex: Wiremold®) and product family names (Evolution™) together. This will introduce a level of unnecessary confusion for the audience.
Lighting Types
Different forms of light a device is able to provide.
Protocol
A Convention or Standard that Controls or Enables the Connection, Communication, and Data Transfer Between Two Computing Endpoints, the Rules Governing the Syntax, Semantics, and Synchronization of Communication
Target Size
The Dimensional Specification of the Object Which is Set as a Target for the Sensor
Sensing Range
The total Possible Sensing Capability of the Sensor, Beginning After the Deadband, and Extending Out as Far as the Sensor is Able to Reach Effectively
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
Battery Life
Describes the approximate amount of time a battery can power a device before it needs to be recharged or replaced.
On Function
Describes the mode of operation for devices that can be turned on, indicating whether they stay on continuously or operate on a timer or sensor.
Number of Connections
The number of connections a product is able to make to other devices.
Battery Capacity
Describes the maximum amount of electrical charge that a battery can store and deliver.
Engraving Type
Refers to the available styles to mark or inscribe text, symbols, or patterns on a product.
Seismic Tested
Indicates whether a device has been tested to withstand and/or perform under certain seismic conditions.
Sensor Coverage
Describes the total area, measured in square footage, within which a sensor can detect presence or movement.
Antenna Pattern
Captures the directional representation of how radio waves are sent and received by the antenna.
Sensitivity Adjustment
Refers to any customization settings, or range of adjustments for motion detection sensitivity, required to turn lights on.
Storage Temperature
Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.
Device Front Face Size
Describes the general proportions of a product's front face relative to the overall device.
Indicator
Describes the type/specification of signaling a device uses to indicate abnormal and/or operating conditions.
Timer Type
The mechanism by which the timer operates, such as mechanical, digital, or programmable.
Antenna Type
Refers to the design or style of antenna used within a device, which can impact signal direction, range, and performance in wireless communication.
Dimming Compatibility
Describes the method(s) used by a device or system to adjust the brightness of a lighting load.
Trim/Adjustment Level
A control feature that allows the adjustment of the minimum and maximum light levels to prevent issues such as flickering at lower brightness levels, ensuring smooth and stable dimming performance.
Topology
The arrangement in which the Nodes of a LAN are connected to each other.
Wall Plate Included
Indicates if the device comes with a cover plate for aesthetic integration with the wall.
Works With
Need to ensure your choice works with your device, system, or software? Select your needs using this filter to confirm compatibility.
Sensor Coverage Pattern
Describes the shape of the area that a sensor is able to detect presence or movement within, measured in degrees.
Dimming Phase
Refers to the point in the AC power cycle at which the dimmer begins to reduce voltage to the light. "Leading Edge" dimmers cut the initial phase and are typically used for incandescent bulbs, while "Trailing Edge" dimmers cut the end phase, which is more suitable for LEDs.
Horsepower Rating
Refers to the power capacity of a device under normal load conditions, measured in horsepower (HP).
Current Draw
The amount of electrical current the device uses during operation, measured in amperes (or amps).
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
A collection of related products that share a common design, technology, or purpose. Products within the series either maintain a cohesive brand / style identity or work together to serve a particular solution.
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Wireless Range
Describes the maximum distance wireless devices can be separated while preserving signal quality and reliability.
Throw Type
Describes the method of switch operation, indicating whether it controls one circuit (single-throw) or switches between two circuits (double-throw).
Line Frequency
The frequency of alternating current (AC) in an electrical power system, measured in Hz. Also commonly referred to as Utility Frequency, Power Line Frequency, or Mains Frequency.
Maximum Humidity
The highest level of atmospheric moisture a device can withstand without compromising functionality or safety.
Maximum Horsepower Rating
The maximum power load the device can handle before the risk of damage or failure.
Number of Phases
Indicates the number of electrical phases a device utilizes.
Sensor Technology
The technology used by a device to sense a change in signal or stimulus.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
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
Ultrasonic Frequency
Describes the specific frequency at which a sensor emits and detects sound waves in order to measure distances, detect objects, or perform other functions.
Bulb Compatibility
Indicates the type(s) of lighting a dimmer or controller is designed to work with, ensuring proper functionality and performance.
Device Backbody Size
Describes the general proportions of a product's backbody relative to the overall device.
Outlet Type
Describes the unique qualities or characteristics of an electrical outlet that make it better suited to different uses. The listed qualities may give the outlet improved safety performance, increased efficiency, or additional functionality.
Number of Rockers
The total number of rocker-type electrical switches included on a device. Typically used to switch between two or more functions.
Sensor Mounting Height
Describes the optimal vertical distance at which a sensor should be installed to ensure reliable detection of motion or other target conditions.
Location Rating
Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.
Number of Relays
Denotes the number of controlled loads a device can support.
USB Amperage
Describes the maximum electrical current the conductor or device can carry through its USB ports before sustaining immediate or progressive deterioration.
Electrical Rating
The maximum load or capacity of electrical power a dimmer switch is rated to manage when linked to a specific type of light bulb.
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
Publishing Date Range
Date article, blog, or press release was published.
Category
Our brands, products, resources, and pages are group into divisions. Filter and find a product, resource, or page you are looking for based on a Legrand category.
Resource Type
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
Brand
Choose from one of Legrand's brands.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - Discontinued - LS Series Incandescent Slide Dimmer, Brown | Sub LS603PLS1003P Pass and SeymourINCAN 3W PRESET SLDE 1000W
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - Discontinued - LS Series Incandescent Slide Dimmer, BrownLS600P Pass and SeymourLS Series Incandescent Slide Dimmer
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage Selections
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - Discontinued - Wide Slide Series Dimmer, White95681W Pass and SeymourWide Slide Series Dimmer
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage Selections
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - Discontinued - Leandro Incandescent Preset Dimmer, Light AlmondD1000MLAV Pass and SeymourLeandro Incandescent Preset Dimmer
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - Discontinued - Scene Director Low-Voltage Dimmer, IvorySCELV300IV Pass and SeymourScene Director Low-Voltage Dimmer
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - Discontinued - Trademaster Magnetic Low-Voltage Toggle Dimmer, Black | Sub TSDLV703PBKTDLV703PBK Pass and SeymourVersatile toggle dimmer, provides easy ON/OFF toggle plus a separate preset allows convenient dimming control. Preset, Single Pole/3-Way, available in 5 colors: white, black, light almond, ivory and brown.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - Discontinued - Trademaster Magnetic Low-Voltage Toggle Dimmer, Brown | Sub TSDLV1103PTDLV1103P Pass and SeymourVersatile toggle dimmer, provides easy ON/OFF toggle plus a separate preset allows convenient dimming control. Preset, Single Pole/3-Way available in 5 colors: white, black, light almond, ivory and brown.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - Discontinued - Harmony® 120V CFL/LED Dimmer, WhiteHCL453PW Pass and Seymour120 V, 60 Hz, 450 Watts. CFL/LED, Single Pole and 3-Way, Preset. White.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - adorne® 700W Incandescent/Halogen Paddle Dimmer, Magnesium, with Microban®ADPD703HM4 adorne CollectionStylish and precise light level control.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - adorne® 1100W Incandescent/Halogen Paddle Dimmer, White, with Microban®ADPD1103HW4 adorne CollectionStylish and precise light level control for incandescent/halogen dimmable bulbs or fixtures.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - Discontinued - LS Series Incandescent Slide Dimmer, BlackLS603PBK Pass and SeymourLS Series Incandescent Slide Dimmer
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - Discontinued - Harmony® 0-10V LED|Fluorescent 4-Wire Dimmer, WhiteH4FBL3PW Pass and Seymour4-wire, single-pole/3-way 0-10V dimmer with integrated power pack.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - adorne® 450W CFL/LED Paddle Dimmer, Magnesium, with Microban®ADPD453LM2 adorne CollectionStylish and precise light level control.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - Discontinued - Trademaster® Wide Slide 1100W Preset Incandescent Dimmer, White Interchangeable Face ColorWS1103PW Pass and Seymour120V, 1100W preset, incandescent single-pole/3-way dimmer w/ white interchangeable face color
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - Discontinued - Harmony® Tru-Universal Dimmer with 3 Interchangeable Face ColorsH703PTUTC Pass and SeymourWorks with every dimmable lamp, load, and fixture on typical residential and light commercial wiring (except for 0-10V loads -- see Harmony, Wide Slide, or Titan 0-10V Dimmers). Includes three interchangeable face colors.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage Selections
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - Discontinued - Harmony® 120V CFL/LED Dimmer, Three Interchangeable Face ColorsHCL453PTC Pass and Seymour120 V, 60 Hz, 450 Watts. CFL/LED, Single Pole and 3-Way, Preset. Three interchangeable face colors.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage Selections
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - Discontinued - Wide Slide Series Dimmer, White91180W Pass and SeymourWide Slide Series Dimmer
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - Discontinued - radiant® 120V, 1100W Incandescent Single Pole/3-Way Dimmer, WhiteRH1103PW radiant CollectionDelivers precise light level control of incandescent dimmable bulbs, with classic style.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - adorne® 1100W Incandescent/Halogen Whisper® Dimmer, MagnesiumADWR1103HM4 adorne CollectionWhisper switch on/off plus smooth sliding dimmer control for incandescent/halogen bulbs or fixtures.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - Discontinued - LS Series Dual Fan Speed Control|Dimmer, WhiteLSDV25WV Pass and SeymourLS Series Dual Fan Speed Control/Dimmer
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - Titan Series LED 4-Wire Single-Pole Dimmer, BlackCD4FBLBK Pass and SeymourFour-wire, single-pole, slide-to-OFF 0-10V narrow dimmer with integrated power pack.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - Discontinued - Harmony® Tru-Universal Dimmer, WhiteH703PTUW Pass and SeymourWorks with every dimmable lamp, load, and fixture on typical residential and light commercial wiring (except 0-10V loads -- see Harmony, Wide Slide, or Titan 0-10V dimmers).
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - Titan Series LED 4-Wire Single-Pole/3-Way Preset Dimmer, GrayCD4FBL3PGRY Pass and SeymourFour-wire, single-pole/3-way preset 0-10V narrow dimmer with integrated power pack.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - Discontinued - Trademaster CFL/LED/Incandescent Single Pole/3-Way Toggle Dimmer, Brown | Sub TSDCL303PTDCL453P Pass and SeymourWorks with select dimmable CFL/LED or incandescent lighting loads and features a sleek, sculpted ergonomic design for smooth, easy operation and precise control.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - Discontinued - Rotary Dual Fan Speed/Dimmer Control, Ivory94331I Pass and SeymourRotary Dual Fan Speed/Dimmer Control
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDiscontinued - Discontinued - Harmony® Incandescent Single Pole/3-Way Dimmer Switch, 3 Interchangeable Face ColorsH703PTC Pass and SeymourReduces energy by up to 30% and extends bulb life. Three interchangeable face colors.
Easily adjust the maximum and minimum brightness of your smart dimmer switch in the Legrand Home + Control App. Settings also eliminate flickering and other issues.
If your dimmer lights are flickering, there are numerous causes like light bulb and switch incompatibility, improper wiring or a loose connection.
Elevate any space with the exceptional style and innovative functionality of designer dimmers from the adorne and radiant Collections.
Select the perfect dimming solution for your bulb or fixture, and gain precise light level control to match any mood.
Any bulb, always compatible. Tru-Universal Dimmers were designed to work with virtually any dimmable bulb, eliminating flicker and allowing precise light level control with style and ease.
Designer switches and dimmers form the heart of the adorne® Collection. Whether you favor a simple touch (like on your smartphone), a satisfying click, or even the simple wave of a hand, adorne® makes it a delight to hit the lights.
Watch this short how-to video for a step-by-step guide to installing adorne dimmers.
Dive deeper into Legrand's switches and dimmers. Learn about functionality, dimmer & switch types, installation guidance, safety, colors, designs and more!
See how designer switches and outlets set the perfect light level for an evening of food and fun.
See how designer switches and outlets can enhance your space with clutter-free wireless charging and dimming capability.
See how to easily install an adorne® or radiant® with Netatmo Smart Tru-Universal Dimmer.
See how adorne magnesium dimmers and screwless wall plates can elevate this gray modern bedroom suite.
See how designer switches and outlets let you adjust that atmosphere for entertaining with easy and precision.
Upgrading switches to add dimming control is easier than you think. Start learning how to safely do it yourself with a few basic tools and these simple steps.
sofTap Tru-Universal Dimmers lets you create your ideal atmosphere with just a few little taps.
Cleaner spaces start with cleaner control. Browse touchless light switches and dimmers as well as options with built-in Microban antimicrobial protection.
See how adorne illuminates this blue and gray coastal bedroom while adding to the style.
“Wherever you like your lights, you can have them. It’s as simple as that!”
See adorne graphite dimmers, outlets and wall plates in this bold bathroom.
See how adorne sofTap switches and dimmers illuminate this bedroom entryway while adding a bold wall plate.
Watch for a step-by-step guide to installing an adorne Tru-Universal Dimmer, compatible with virtually any dimmable bulb.
Dimmable lighting is an easy upgrade with plenty of benefits, but how do you get started? Learn if, where, what and how about swapping in dimmers at home.
See the adorne® Collection’s sofTap™ Dimmer and Switch
From standard LED dimming to stylish smart lighting, Legrand offers a full spectrum of residential lighting and fan controls to meet any home’s needs.
Elevate any space with the innovative functionality of hands-free touchless light switches and dimmers from the adorne and radiant Collections.
Legrand, North and Central America today launched the Wattstopper® DCLV2 0-10V Decorator Dimmer that controls and smoothly dims low voltage lighting loads, including the latest LED and fluorescent fixtures.
Discover Legrand's radiant® LED Advanced Dimmer, engineered for seamless LED dimming. With advanced circuitry, it eliminates common issues, offering precise control and compatibility with modern LED bulbs and fixtures.
Learn the benefits of LED dimming controls, LED light bulbs standardization and common dimming FAQs in our guide to dimming LED lights in the home.
With designer switches and outlets from the radiant® Collection, upgrading your space with style and innovation starts at the wall
Featuring leading Microban technology, meet Legrand’s switches, dimmers and wall plates with built-in antimicrobial protection for cleaner spaces.