text.skipToContent text.skipToNavigation

How to Install an adorne® Pop-Out Outlet (Step-by-Step Guide)

July 31, 2026

Looking to upgrade your space with a sleek, hidden power solution? The adorne® Pop-Out Outlet offers an innovative way to keep outlets out of sight until you need them – perfect for kitchens, home offices and high-traffic living areas. 

This step-by-step guide walks you through how to install your pop-out outlet safely and successfully.

Why Choose a Pop-Out Outlet?

Looking to upgrade your space with a sleek, hidden power solution? The adorne® Pop-Out Outlet offers an innovative way to keep outlets out of sight until you need them – perfect for kitchens, home offices and high-traffic living areas. 

This step-by-step guide walks you through how to install your pop-out outlet safely and successfully. 

How does it work? 

  • Press once → outlet pops out 
  • Press again → outlet retracts for a clean, flush look 

Before You Get Started

Before starting your installation, keep these key points in mind: 

  • Always turn off power at the breaker panel to avoid shock or electrocution  
  • Ensure your electrical box meets minimum depth requirements (generally 3–3.5 inches depending on box type) 
  • Use only with the Legrand adorne system 
  • Install in wall applications only – not in countertops or similar surfaces  

If you’re unsure about any step, consult a qualified electrician. 

Prep: Collect all Tools 

  • Screwdriver 
  • Wire stripper (if needed) 
  • Wire nuts (included) 
  • Pro Tip: Pre-fold wires into the wall box to make installation easier later. 

Step 1: Remove the Existing Outlet 

If you’re replacing an outlet, label all wires before disconnecting 

You’ll typically be working with: 

  • Hot (black) 
  • Neutral (white) 
  • Ground (bare copper)  

Step 2: Prepare the Wires

Trim and strip wires as needed using the guide on the back of the outlet. Ensure clean, properly sized wire ends for secure connections. 

Step 3: Connect the Ground Wire

The outlet includes a 6-inch ground pigtail wire, which will need to be connected to: 

  • The existing ground wire 
  • The metal box (if applicable) 

Secure with the provided wire nut and fold wires neatly into the back of the box. 

⚠️ Proper grounding is critical for a safe installation. 

Step 4: Wire and Mount the Outlet

  • Insert wires into the correct terminals and tighten the screws firmly. 
  • Match wire sizes—do not mix different gauges in the same terminal without a pigtail. 
  • Carefully fold wires into the box, align the outlet frame with the wall and secure the device with screws. 

Take care not to damage the wall surface during installation.

Step 5: Install the Wall Plate

Once the outlet is installed, snap the adorne Wall Plate onto the frame. Adjust the positioning using the built-in click stops for a flush fit. 

Tip: To remove later, gently pry using a flat screwdriver.

Final Safety Check

Before restoring power: 

✔ All wires securely connected 

✔ Ground wire properly installed 

✔ Device firmly mounted 

Then turn the power back on and test functionality. 


Get regular updates sent directly to your inbox to learn more about Legrand’s residential products, including the Pop-Out Outlet, the Kitchen Countertop Outlet, USB Outlets, Lighting Controls and beyond.

Our support team is here to help with installing Legrand products. Find helpful installation guides, step-by-step how-to instructions and more by visiting our installation hub. Our support team is here to help with installing Legrand products. Find helpful installation guides, step-by-step how-to instructions and more by visiting our installation hub.