5
Browse 927 results for
"adorne"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Brand
Choose from one of Legrand's brands.
Product Family
Used to identify and differentiate offerings within a particular product line. Product families are typically treated as adjectives. It is not recommended to use the product line (ex: Wiremold®) and product family names (Evolution™) together. This will introduce a level of unnecessary confusion for the audience.
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Outlet Type
Describes the unique qualities or characteristics of an electrical outlet that make it better suited to different uses. The listed qualities may give the outlet improved safety performance, increased efficiency, or additional functionality.
Sensor Type
The Device that Receives a Signal or Stimulus (As Heat or Pressure or Light or Motion Etc.) and Responds to it in a Distinctive Manner
Enclosure Type
Style, Type, Size, Etc. of the Enclosure of a Device
Wall Plate Type
Refers to the style or intended usage of a wall plate.
Product Certifications
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
Features
Unique characteristics and functionality that set the product apart from others in its field.
Availability
Product is available to buy on Legrand.us
Material
Indicates the primary material(s) used to construct a product.
Mounting Type
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
Standard
The industrial standard(s) to which a device is manufactured, operated, or tested.
Load Rating
The maximum load that a device is designed to withstand without breakage or loss of performance.
Load Type
Denotes the type(s) of load that can be applied to a dimmer, which determines its compatible light sources.
Amperage
Maximum electrical current the conductor or device can carry before sustaining immediate or progressive deterioration
Input Voltage
The Difference of Electrical Potential Between Two Points of an Electrical or Electronic Circuit Entering a System
Voltage
The Rate at Which Energy is Drawn from a Source that Produces a Flow of Electricity in a Circuit
Sensor Technology
The technology used by a device to sense a change in signal or stimulus.
Application Sector
Refers to the expected environment(s) or intended usage(s) for a product (e.g. Residential, Commercial, Industrial, etc.).
Indoor/Outdoor
Enviromental Conditions rating on the product. Indoor Only, Outdoor, Both
Installation Location
Where a Device is or is to be Installed
Requires Neutral Wire
Indicates whether a device requires a neutral wire to function properly.
Location Rating
Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.
Compatibility
Capability of Being Used with or Connected to Different Types of Devices or Components without any Modifications
Works With
Need to ensure your choice works with your device, system, or software? Select your needs using this filter to confirm compatibility.
Bulb Compatibility
Indicates the type(s) of lighting a dimmer or controller is designed to work with, ensuring proper functionality and performance.
On Function
Describes the mode of operation for devices that can be turned on, indicating whether they stay on continuously or operate on a timer or sensor.
Lighting Types
Different forms of light a device is able to provide.
Category Performance Application
Refers to the specific standard used to define an ethernet cable's capabilities and its intended usage. Most commonly shortened to"Cat" and a number (e.g. Cat5e; Cat6; Cat6a).
Throw Type
Describes the method of switch operation, indicating whether it controls one circuit (single-throw) or switches between two circuits (double-throw).
Operating Temperature
The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
Number of Wires
The Number of Pliable Metallic Strand or Rod Made in Many Lengths and Diameters and are Electrically Insulated, Used Conduct Electricity
Wire Connection Type
Describes the method used to connect wires to the device, such as screw terminals, push-in connectors, or lead wires.
Timing Range
The Time Span for Which the System/Device is in Desired Active/Working Mode
Connection TypeTooltip Title
Style or Type of Connection Used
Line Frequency
The frequency of alternating current (AC) in an electrical power system, measured in Hz. Also commonly referred to as Utility Frequency, Power Line Frequency, or Mains Frequency.
NEMA Configuration Code
Alpha-Numeric Code Applied to Connectors to Guarantee Consistency and Interchageability Between Manufacturers
Terminal Accommodation
Describes the type and size of wire that the receptacle's terminals can securely hold (typically provided as a range in gauge size).
USB Amperage
Describes the maximum electrical current the conductor or device can carry through its USB ports before sustaining immediate or progressive deterioration.
USB Wattage
Describes the maximum electrical power a USB receptacle can safely output.
Wiring Method
Describes the design and ways of connecting various parts of a device with cable and/or wire.
Sensing Range
The total Possible Sensing Capability of the Sensor, Beginning After the Deadband, and Extending Out as Far as the Sensor is Able to Reach Effectively
Sensor Coverage
Describes the total area, measured in square footage, within which a sensor can detect presence or movement.
Sensor Coverage Pattern
Describes the shape of the area that a sensor is able to detect presence or movement within, measured in degrees.
Protocol
A Convention or Standard that Controls or Enables the Connection, Communication, and Data Transfer Between Two Computing Endpoints, the Rules Governing the Syntax, Semantics, and Synchronization of Communication
Internal Depth
Refers to the distance from the surface level of a box to the area where internal devices are plugged in, illustrating the available space within to accommodate cords, receptacles, and large devices.
Thickness
The Dimension Through an Object as Opposed to its Length or Width
Wall Plate Size
The general size of the the included wall plate. The size may determine whether it suits your personal application!
Cord Length
The Linear Extent of Cord in Space from one End to the Other
Number of Gangs
The amount of switches on the plate.
Number of Switches
Number of electrical switches
Number of Phases
Indicates the number of electrical phases a device utilizes.
Number of Receptacles
The Number of Electrical Wall Outlets Designed for Use with a Plug
Number of USBs
Number of USB ports
Filter by Product Category
Filter downloadable resources by the product category they relate or are relevant to.
Brand
Choose from one of Legrand's brands.
Resource Type
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
Bright ideas abound with adorne® illumination products. When it comes to brilliant solutions, the adorne® Collection really shines.
See how to bind lights throughout your home for the adorne Whole House Lighting System.
See how to program your adorne Tru-Universal Dimmer for precise light level control, no matter your lighting type.
Watch to see how easy it is to add power right where you need it, with the adorne Furniture Power Center.
Easily upgrade your outlets with the designer style of adorne. Watch this video to see how.
Watch this short how-to video for a step-by-step guide to installing adorne switches.
Give your guests a stay to remember by focusing on the details. With the adorne Collection, choose from an array of finishes and colors that match your hotel’s decor.
Warranty information for products from the adorne® Collection of designer switches and outlets.
Browse images to see how adorne switches, outlets and USB charging were a stylish, easy solution for the historic building turned hotel: Quirk Richmond.
Designer switches and dimmers form the heart of the adorne® Collection. Whether you favor a simple touch (like on your smartphone), a satisfying click, or even the simple wave of a hand, adorne® makes it a delight to hit the lights.
Take a quick peek at some designer switches and outlets from the adorne® Collection with this TV spot highlighting innovative products like the Pop-Out Outlet and Wave Switch.
Pairing the adorne Switches in magnesium with a sleek dark Wall Plate
Upgrade to devices both brilliant and beautiful. Check out the adorne® Collection of designer switches and outlets.
Say goodbye to outdated switches and outlets. Say hello to The adorne® Collection.
Watch this short how-to video for a step-by-step guide to installing adorne dimmers.
See how designer switches and outlets can provide code-compliant ground fault protection in a clever, contemporary design.
See how designer switches and outlets can provide power wherever you need it.
See how designer switches and outlets can offer convenience and germ-free control.
The ideal smart lighting solutions for whole-home use, meet adorne® & radiant® with Netatmo.
View the guest room of JW Marriott Mall of America, where the bedside charging station is created with adorne Power and USB Outlets.
The designer switches and outlets from adorne feature modern style and function, including the latest technologies for control and charging.
The adorne® Collection makes life simply beautiful, putting a stylish and innovative finishing touch on your home. Turn ordinary into extraordinary with designer switches and outlets.
Say goodbye to boring switches and hello to breathtaking design elements, with the adorne® Collection's elegant selection of designer switches and outlets.
The designer switches, dimmers, outlets and more from the adorne® Collection can take your home from basic to stylishly functional.
See how adorne outlets can charge your devices while matching the aesthetic of your room.
Adding the wow factor to any upgrade. Catch the adorne® Touch Switch in this TV spot from 2018.
Turn the lights on with a simple touch. Check out the clever Touch Switch from the adorne® Collection.
“How awesome is that?!” Check out the awesome adorne® USB Outlet in this TV spot from 2018.
Easily find your switch or dimmer in the dark, with a simple-to-install locator light. Watch to see how.