5
Browse 1,051 results for
"dimmer"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Brand
Choose from one of Legrand's brands.
Product Family
Used to identify and differentiate offerings within a particular product line. Product families are typically treated as adjectives. It is not recommended to use the product line (ex: Wiremold®) and product family names (Evolution™) together. This will introduce a level of unnecessary confusion for the audience.
Product Series
A collection of related products that share a common design, technology, or purpose. Products within the series either maintain a cohesive brand / style identity or work together to serve a particular solution.
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Timer Type
The mechanism by which the timer operates, such as mechanical, digital, or programmable.
Outlet Type
Describes the unique qualities or characteristics of an electrical outlet that make it better suited to different uses. The listed qualities may give the outlet improved safety performance, increased efficiency, or additional functionality.
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
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
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
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
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
Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.
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
Electrical Rating
The maximum load or capacity of electrical power a dimmer switch is rated to manage when linked to a specific type of light bulb.
On Function
Describes the mode of operation for devices that can be turned on, indicating whether they stay on continuously or operate on a timer or sensor.
Lighting Types
Different forms of light a device is able to provide.
Throw Type
Describes the method of switch operation, indicating whether it controls one circuit (single-throw) or switches between two circuits (double-throw).
Operating Temperature
The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit
Operating Temperature Max
Indicates the highest possible temperature a device can be safely used without the risk of failure or damage.
Storage Temperature
Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
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
The frequency of alternating current (AC) in an electrical power system, measured in Hz. Also commonly referred to as Utility Frequency, Power Line Frequency, or Mains Frequency.
NEMA Configuration Code
Alpha-Numeric Code Applied to Connectors to Guarantee Consistency and Interchageability Between Manufacturers
Terminal Accommodation
Describes the type and size of wire that the receptacle's terminals can securely hold (typically provided as a range in gauge size).
USB Amperage
Describes the maximum electrical current the conductor or device can carry through its USB ports before sustaining immediate or progressive deterioration.
Contact Configuration
Different Switching Functions of the Relay Contacts
Contact Rating
The Voltage, Current, and Power Capacities of Relay Contacts Under Specified Environmental Conditions
Sensing Range
The total Possible Sensing Capability of the Sensor, Beginning After the Deadband, and Extending Out as Far as the Sensor is Able to Reach Effectively
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
A Convention or Standard that Controls or Enables the Connection, Communication, and Data Transfer Between Two Computing Endpoints, the Rules Governing the Syntax, Semantics, and Synchronization of Communication
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
Publishing Date Range
Date article, blog, or press release was published.
Filter by Product Category
Filter downloadable resources by the product category they relate or are relevant to.
Brand
Choose from one of Legrand's brands.
Resource Type
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
Easily adjust the maximum and minimum brightness of your smart dimmer switch in the Legrand Home + Control App. Settings also eliminate flickering and other issues.
If your dimmer lights are flickering, there are numerous causes like light bulb and switch incompatibility, improper wiring or a loose connection.
Elevate any space with the exceptional style and innovative functionality of designer dimmers from the adorne and radiant Collections.
Select the perfect dimming solution for your bulb or fixture, and gain precise light level control to match any mood.
Any bulb, always compatible. Tru-Universal Dimmers were designed to work with virtually any dimmable bulb, eliminating flicker and allowing precise light level control with style and ease.
Dive deeper into Legrand's switches and dimmers. Learn about functionality, dimmer & switch types, installation guidance, safety, colors, designs and more!
Designer switches and dimmers form the heart of the adorne® Collection. Whether you favor a simple touch (like on your smartphone), a satisfying click, or even the simple wave of a hand, adorne® makes it a delight to hit the lights.
Watch this short how-to video for a step-by-step guide to installing adorne dimmers.
See how designer switches and outlets set the perfect light level for an evening of food and fun.
See how designer switches and outlets can enhance your space with clutter-free wireless charging and dimming capability.
See how to easily install an adorne® or radiant® with Netatmo Smart Tru-Universal Dimmer.
See how adorne magnesium dimmers and screwless wall plates can elevate this gray modern bedroom suite.
See how designer switches and outlets let you adjust that atmosphere for entertaining with easy and precision.
Upgrading switches to add dimming control is easier than you think. Start learning how to safely do it yourself with a few basic tools and these simple steps.
sofTap Tru-Universal Dimmers lets you create your ideal atmosphere with just a few little taps.
See how adorne illuminates this blue and gray coastal bedroom while adding to the style.
“Wherever you like your lights, you can have them. It’s as simple as that!”
See adorne graphite dimmers, outlets and wall plates in this bold bathroom.
Cleaner spaces start with cleaner control. Browse touchless light switches and dimmers as well as options with built-in Microban antimicrobial protection.
Dimmable lighting is an easy upgrade with plenty of benefits, but how do you get started? Learn if, where, what and how about swapping in dimmers at home.
See how adorne sofTap switches and dimmers illuminate this bedroom entryway while adding a bold wall plate.
Watch for a step-by-step guide to installing an adorne Tru-Universal Dimmer, compatible with virtually any dimmable bulb.
See the adorne® Collection’s sofTap™ Dimmer and Switch
From standard LED dimming to stylish smart lighting, Legrand offers a full spectrum of residential lighting and fan controls to meet any home’s needs.
Elevate any space with the innovative functionality of hands-free touchless light switches and dimmers from the adorne and radiant Collections.
Discover Legrand's radiant® LED Advanced Dimmer, engineered for seamless LED dimming. With advanced circuitry, it eliminates common issues, offering precise control and compatibility with modern LED bulbs and fixtures.
Legrand, North and Central America today launched the Wattstopper® DCLV2 0-10V Decorator Dimmer that controls and smoothly dims low voltage lighting loads, including the latest LED and fluorescent fixtures.
Learn the benefits of LED dimming controls, LED light bulbs standardization and common dimming FAQs in our guide to dimming LED lights in the home.
With designer switches and outlets from the radiant® Collection, upgrading your space with style and innovation starts at the wall
Featuring leading Microban technology, meet Legrand’s switches, dimmers and wall plates with built-in antimicrobial protection for cleaner spaces.