5
Browse 1,885 results for
"outlet"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Brand
Choose from one of Legrand's brands.
Product Family
Used to identify and differentiate offerings within a particular product line. Product families are typically treated as adjectives. It is not recommended to use the product line (ex: Wiremold®) and product family names (Evolution™) together. This will introduce a level of unnecessary confusion for the audience.
Product Series
A collection of related products that share a common design, technology, or purpose. Products within the series either maintain a cohesive brand / style identity or work together to serve a particular solution.
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Timer Type
The mechanism by which the timer operates, such as mechanical, digital, or programmable.
Outlet Type
Describes the unique qualities or characteristics of an electrical outlet that make it better suited to different uses. The listed qualities may give the outlet improved safety performance, increased efficiency, or additional functionality.
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
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
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
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
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
Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.
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
Describes the mode of operation for devices that can be turned on, indicating whether they stay on continuously or operate on a timer or sensor.
Lighting Types
Different forms of light a device is able to provide.
Service Capacity
Denotes the number of different services that can be used within a product as a result of separated internal compartments, including electrical, low voltage, water, air, and more.
Throw Type
Describes the method of switch operation, indicating whether it controls one circuit (single-throw) or switches between two circuits (double-throw).
Operating Temperature
The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit
Operating Temperature Max
Indicates the highest possible temperature a device can be safely used without the risk of failure or damage.
Storage Temperature
Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.
Is the Device Prewired?
Denotes whether a product comes prewired for quicker installation.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
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
Indicates whether a device is designed with a raised edge/rim, on or around its receptacle, for superior strength, handling, or attachment to another object.
Line Frequency
The frequency of alternating current (AC) in an electrical power system, measured in Hz. Also commonly referred to as Utility Frequency, Power Line Frequency, or Mains Frequency.
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
Describes the maximum electrical current the conductor or device can carry through its USB ports before sustaining immediate or progressive deterioration.
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
The total Possible Sensing Capability of the Sensor, Beginning After the Deadband, and Extending Out as Far as the Sensor is Able to Reach Effectively
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
A Convention or Standard that Controls or Enables the Connection, Communication, and Data Transfer Between Two Computing Endpoints, the Rules Governing the Syntax, Semantics, and Synchronization of Communication
Single/Multimode
Describes the mode of fiber either utilized or accepted by a device to transmit or receive a fiber optic signal.
Circular Outlet Diameter
Refers to the diameter of the circular opening in a wall plate, which should match the diameter of the outlet it is intended to cover.
Receptacle Spacing
Refers to the distance between power outlets or receptacles on a device, which can be important for planning the layout of plugs and connectors.
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
Refers to the distance from the surface level of a box to the area where internal devices are plugged in, illustrating the available space within to accommodate cords, receptacles, and large devices.
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
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
Learn how to gain the convenience of multi-location control with elevated style. Just follow these simple steps for wiring adorne® or radiant® 3-way switches.
Top smart home trends in 2024 are building off 2023 momentum with smart lighting, Matter smart home standard, and smart refrigerators expected to gain popularity.
Compact yet powerful. Get fast Level 2 charging for electric vehicles with Legrand’s safe, easy and efficient EV chargers. Available for home or commercial use.
Cleaner spaces start with cleaner control. Browse touchless light switches and dimmers as well as options with built-in Microban antimicrobial protection.
Legrand, a global specialist in electrical and network infrastructure solutions, will showcase its portfolio of hospitality-focused products at HD Expo 2017
Select the perfect dimming solution for your bulb or fixture, and gain precise light level control to match any mood.
Legrand offers an extensive selection of innovative solutions designed to bring additional comfort, convenience, safety and more, to residential spaces.
Flexibility is a priority in commercial interior spaces. Legrand offers innovative and stylish solutions that provide power, data, and charging connections exactly where it is needed.
CES 2019, Legrand will demonstrate a suite of leading connected devices that underscore the company’s continued commitment to developing technologies that are more intuitive, maximize comfort and safety.
Lehigh University installs Legrand’s ModPower System in 110 desks across campus with enough power and charging for their students.
Legrand offers smart lighting solutions to fit every lifestyle, application or project.
Legrand offers a family of lighting control products fully enabled to interface with Apple HomeKit.
Upgrade your infrastructure with our heavy-duty covers to embrace a new era of safe and stylish charging and power. Click to learn more.
Light switch timers and occupancy/vacancy sensors offer automated control for convenience and energy savings in the home while allowing for precise lighting control.
Increase productivity and value provided to customers as you transform where people live and work with tools, resources and the solutions you need. Learn more.
At Legrand, we are your dedicated partner in creating dynamic, high-performance spaces. We understand today’s challenges and are uniquely positioned to be your trusted partner in navigating the path toward a more sustainable built environment.
Luxul is the leading innovator of simple-to-deploy professional grade IP networking solutions for use by custom installation professionals.
Step-by-step instructions to create custom settings for Netatmo smart lights using Amazon’s Alexa voice commands.
Get rack PDUs trusted by the top Fortune 500; architected with components, features and more that ensure the most reliable infrastructure possible. Learn more.
Trust the industry's largest provider of end-to-end wire and cable management solutions for indoor and outdoor applications. Explore the Wiremold product line.
It’s time for a deeper clean. Get to know Microban technology and how it provides antimicrobial protection for products like light switches, dimmers and more.
Annual fundraiser generates $76,000 for Building Homes for Heroes
Legrand announced an agreement with Florida-based Minto Communities to provide its On-Q and Pass & Seymour (P&S) products for more than 9,000 homes to be built in Daytona Beach, Fla., and Hilton Head, S.C.
Starline offers an innovative overhead power distribution system designed to supply and monitor critical power with a simple, safe, fast, reliable approach.
Read our blog post to learn how you can create an energy efficient building by integrating automatic plug load controls that reduce operating costs, reduce energy use, and help meet the energy code requirements of IECC, ASHRAE 90.1, and CA Title 24.
Learn the basics of EV charging so you can make an informed decision when it comes to selecting and offering EV charging amenities. Learn more.
Find answers to common questions about the Connectrac Flex Raceway System, including installation codes, compliance information, product details, and more.
Meta Description: Legrand has released a new demo case for dealers to elegantly showcase Designer Series Decorative Brackets and matching hembar endcaps to customers.
Matter-enabled devices offer a convenient way to integrate multiple types of devices into a smart home system so they all communicate with each other.
Consider some of these ideas for your next weekend project and add a little something extra, fresh, and new to your home.