5
Browse 1,885 results for
"outlet"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Brand
Choose from one of Legrand's brands.
Product Family
Used to identify and differentiate offerings within a particular product line. Product families are typically treated as adjectives. It is not recommended to use the product line (ex: Wiremold®) and product family names (Evolution™) together. This will introduce a level of unnecessary confusion for the audience.
Product Series
A collection of related products that share a common design, technology, or purpose. Products within the series either maintain a cohesive brand / style identity or work together to serve a particular solution.
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Timer Type
The mechanism by which the timer operates, such as mechanical, digital, or programmable.
Outlet Type
Describes the unique qualities or characteristics of an electrical outlet that make it better suited to different uses. The listed qualities may give the outlet improved safety performance, increased efficiency, or additional functionality.
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
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
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
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
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
Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.
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
Describes the mode of operation for devices that can be turned on, indicating whether they stay on continuously or operate on a timer or sensor.
Lighting Types
Different forms of light a device is able to provide.
Service Capacity
Denotes the number of different services that can be used within a product as a result of separated internal compartments, including electrical, low voltage, water, air, and more.
Throw Type
Describes the method of switch operation, indicating whether it controls one circuit (single-throw) or switches between two circuits (double-throw).
Operating Temperature
The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit
Operating Temperature Max
Indicates the highest possible temperature a device can be safely used without the risk of failure or damage.
Storage Temperature
Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.
Is the Device Prewired?
Denotes whether a product comes prewired for quicker installation.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
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
Indicates whether a device is designed with a raised edge/rim, on or around its receptacle, for superior strength, handling, or attachment to another object.
Line Frequency
The frequency of alternating current (AC) in an electrical power system, measured in Hz. Also commonly referred to as Utility Frequency, Power Line Frequency, or Mains Frequency.
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
Describes the maximum electrical current the conductor or device can carry through its USB ports before sustaining immediate or progressive deterioration.
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
The total Possible Sensing Capability of the Sensor, Beginning After the Deadband, and Extending Out as Far as the Sensor is Able to Reach Effectively
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
A Convention or Standard that Controls or Enables the Connection, Communication, and Data Transfer Between Two Computing Endpoints, the Rules Governing the Syntax, Semantics, and Synchronization of Communication
Single/Multimode
Describes the mode of fiber either utilized or accepted by a device to transmit or receive a fiber optic signal.
Circular Outlet Diameter
Refers to the diameter of the circular opening in a wall plate, which should match the diameter of the outlet it is intended to cover.
Receptacle Spacing
Refers to the distance between power outlets or receptacles on a device, which can be important for planning the layout of plugs and connectors.
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
Refers to the distance from the surface level of a box to the area where internal devices are plugged in, illustrating the available space within to accommodate cords, receptacles, and large devices.
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
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
Smart Wi-Fi Light switches and dimmers from Legrand allow users to easily control light and power from a smart home lighting system or Matter hub.
If your dimmer lights are flickering, there are numerous causes like light bulb and switch incompatibility, improper wiring or a loose connection.
WEST HARTFORD, CONN. — March 17, 2017 — During two annual sales meetings earlier this year, three Legrand divisions – Electrical Wiring Systems, Building Control Systems, and Data Communications – held fundraisers to benefit Building Homes for Heroes.
View the industry's most comprehensive selection of plug load controls for your commercial space and help you meet ASHRAE 90.1 and Title 24 requirements.
Legrand can meet the demands of any building network installation with a full line of both copper and fiber optic connectivity products. Explore our connectivity solutions.
Warranty information for Smart Lighting devices from the radiant Collection.
Overhead power distribution using track busway systems is rapidly becoming the solution of choice in data centers, industrial and manufacturing plants, and other facilities that require continuous uptime and faster adaptability.
Outdoor power and charging solutions have become more versatile and efficient, catering to the needs of a variety of applications and end-users. Learn how to best select the right outdoor power and charging solutions for your unique outdoor power needs.
Legrand’s Microban-treated offering – which will include all adorne switches and dimmers (excluding smart devices at this time) as well as the matching plastic wall plates – features innovative technology that works at the cellular level to inhibit the growth of microbes for cleaner and more durable devices.
Looking to reduce your energy consumption in 2024? Upgrade your residential lighting with LED bulbs, monitor consumption and install dimming switches.
Wattstopper Digital Lighting Management (DLM) System is now qualified as an Interior system in the DesignLights Consortium (DLC) Qualified Product List (QPL), an important distinction as DLC certification is a requirement for many utility rebate programs.
Read our Tribeca case study to learn how Vantage Controls InFusion system and easy-to-install user interfaces made it the clear choice for this project.
Legrand has announced it has been listed among the "World’s Best Employers” by FORBES.
Legrand continues to show its proud support of those who serve our country by providing product donations and volunteering time to complete the latest Building Homes for Heroes® home gifted to a local injured veteran last week.
Setting up your first smart home system opens your home to a world of efficient, secure and convenient solutions.
LFI 2016: Legrand Showcases Code Compliant Control Solutions for Indoor and Outdoor LED Luminaires
Legrand, North America announced today major updates to the Wattstopper LMCS configuration software and Wattstopper Segment Manager Network software that extend the power of the Digital Lighting Management (DLM) control platform.
Legrand raised more than $16,000 (USD) for Building Homes for Heroes, which will be used towards the construction of new homes for returning wounded and disabled veterans.
Legrand Introduces PlugTail® Commercial Specification Grade USB Charging Receptacles.
The aviation industry is soaring toward a greener future, fueled by a pressing need to reduce its carbon footprint and adapt to stringent emissions regulations. At the forefront of this transformation is the trend towards airside equipment electrification, which offers airports a runway to cleaner, more sustainable operations.
The success of implementing a reliable intelligent building depends on an efficient structured cabling infrastructure.
Easily upgrade a rental with these smart tech upgrades that will update your current space, and can move on with you.
Legrand announced that its radiant® RF Lighting Control and adorne® Wi-Fi Ready Lighting systems now work with Amazon Alexa.
Traditional conduit electrical distribution systems limit the flexibility to scale or change facilities, busway systems provide a better solution.
New Matter-enabled devices from the radiant® Collection, developed using Amazon’s Alexa Connect Kit for Matter, are on preview at the 2024 Consumer Electronics Show.
Discover Legrand's latest innovations in lighting control solutions. Explore cutting-edge innovations for seamless LED dimming and advanced lighting control experiences.
New line of PDU and UPS products provide a high-value, cost-effective power solution to complement existing physical infrastructure and connectivity portfolios.
With good planning and the use of energy monitoring and home automation technologies, we can all do our part to reduce the flow of energy consumption.
Legrand introduced a new low-voltage dual-relay output accessory device and a low-voltage input interface device, both of which extend the capabilities of the Wattstopper® Digital Lighting Management (DLM) system.
This recall involves all Wiremold and Plugmold under-cabinet power and lighting strips with part number PX1001.