5
Browse 1,699 results for
"switch"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Product Family
Used to identify and differentiate offerings within a particular product line. Product families are typically treated as adjectives. It is not recommended to use the product line (ex: Wiremold®) and product family names (Evolution™) together. This will introduce a level of unnecessary confusion for the audience.
Product Series
A collection of related products that share a common design, technology, or purpose. Products within the series either maintain a cohesive brand / style identity or work together to serve a particular solution.
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Timer Type
The mechanism by which the timer operates, such as mechanical, digital, or programmable.
Outlet Type
Describes the unique qualities or characteristics of an electrical outlet that make it better suited to different uses. The listed qualities may give the outlet improved safety performance, increased efficiency, or additional functionality.
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
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
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
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
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
Sensor Technology
The technology used by a device to sense a change in signal or stimulus.
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
Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.
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
Bulb Compatibility
Indicates the type(s) of lighting a dimmer or controller is designed to work with, ensuring proper functionality and performance.
Electrical Rating
The maximum load or capacity of electrical power a dimmer switch is rated to manage when linked to a specific type of light bulb.
On Function
Describes the mode of operation for devices that can be turned on, indicating whether they stay on continuously or operate on a timer or sensor.
Lighting Types
Different forms of light a device is able to provide.
Throw Type
Describes the method of switch operation, indicating whether it controls one circuit (single-throw) or switches between two circuits (double-throw).
Operating Temperature
The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit
Operating Temperature Max
Indicates the highest possible temperature a device can be safely used without the risk of failure or damage.
Storage Temperature
Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.
Is the Device Prewired?
Denotes whether a product comes prewired for quicker installation.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
Number of Wires
The Number of Pliable Metallic Strand or Rod Made in Many Lengths and Diameters and are Electrically Insulated, Used Conduct Electricity
Wire Connection Type
Describes the method used to connect wires to the device, such as screw terminals, push-in connectors, or lead wires.
Timing Range
The Time Span for Which the System/Device is in Desired Active/Working Mode
Connection TypeTooltip Title
Style or Type of Connection Used
Line Frequency
The frequency of alternating current (AC) in an electrical power system, measured in Hz. Also commonly referred to as Utility Frequency, Power Line Frequency, or Mains Frequency.
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
Describes the maximum electrical current the conductor or device can carry through its USB ports before sustaining immediate or progressive deterioration.
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
Contact Configuration
Different Switching Functions of the Relay Contacts
Contact Rating
The Voltage, Current, and Power Capacities of Relay Contacts Under Specified Environmental Conditions
Sensing Range
The total Possible Sensing Capability of the Sensor, Beginning After the Deadband, and Extending Out as Far as the Sensor is Able to Reach Effectively
Sensor Coverage
Describes the total area, measured in square footage, within which a sensor can detect presence or movement.
Sensor Coverage Pattern
Describes the shape of the area that a sensor is able to detect presence or movement within, measured in degrees.
Wireless Range
Describes the maximum distance wireless devices can be separated while preserving signal quality and reliability.
Protocol
A Convention or Standard that Controls or Enables the Connection, Communication, and Data Transfer Between Two Computing Endpoints, the Rules Governing the Syntax, Semantics, and Synchronization of Communication
Data Transfer Rate
The Speed at Which Data is Transferred from one Location to Another with in the Time Frame
Maximum Horsepower Rating
The maximum power load the device can handle before the risk of damage or failure.
Max Distance Support
Refers to the maximum range a signal can be effectively supported to by a device.
Receptacle Spacing
Refers to the distance between power outlets or receptacles on a device, which can be important for planning the layout of plugs and connectors.
Box Depth
The measurement from the front opening to the back of an electrical box, indicating the volume of wiring it can contain.
Enclosure Size
The approximate height of the compatible wiring enclosure.
Knockout Size
Physical dimension of the knock-out size, could be diameter or a range
Internal Depth
Refers to the distance from the surface level of a box to the area where internal devices are plugged in, illustrating the available space within to accommodate cords, receptacles, and large devices.
Thickness
The Dimension Through an Object as Opposed to its Length or Width
Wall Plate Size
The general size of the the included wall plate. The size may determine whether it suits your personal application!
Cable Length
The Longest Dimension of Insulated Conductors
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
The Different Types of Receptacles Providing a Place in a Wiring System Where Current can be Taken to Supply Electrical Devices
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
Publishing Date Range
Date article, blog, or press release was published.
Filter by Product Category
Filter downloadable resources by the product category they relate or are relevant to.
Brand
Choose from one of Legrand's brands.
Resource Type
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
The start of every New Year is a time for building owners, managers, and homeowners to make improvements or upgrades they’ve been considering for weeks, months, or maybe, since last New Year.
Discover our On-Q® Enhanced Plastic Enclosures. USA-made and Wi-Fi ready, our enclosures feature design enhancements to save installers time and money. Learn more.
Get installation support and more, with our robust library of how-to videos, installation instructions and FAQs for the adorne and radiant Collections.
Building controls can help meet Fitwel Certification standards and contribute to a healthier building for occupants’ well-being. Read the blog post to learn more.
Extended height WattStopper occupancy sensor allows more facilities to benefit from digital lighting control solutions
View our network cabinet and hot aisle containment resources on this resource page; featuring brochures, data sheets, white papers, videos and more.
Legrand announced a wide array of new products for the residential custom install market from several of its key brands that will be showcased across three booths at CEDIA 2016.
Legrand reaffirms its commitment to Cisco’s Digital Building Solutions as an ecosystem partner with the on-going development of new products to support the evolving intelligent building landscape.
Legrand, the global specialist in electrical and digital building infrastructures, announced it is now shipping the WP-9000 power supply in-wall extension kit.
WattStopper launches first dual loop photosensor for reliable, energy-efficient control of spaces with skylights
When the U.S. Green Building Council (USGBC) team sought out a lighting and plug load controls solution to help it stay within the rigorous LEED Platinum standard, it turned to Legrand.
Discover Legrand’s home builder technology solutions like smart lighting, USB charging outlets, wifi readiness, AV connectivity, home theater connections, etc.
Legrand’s Shading and Residential Controls business recently announced that Charlie Derk, Director of Product Marketing for the company’s QMotion and Vantage brands.
Lighting, Shading, and Networking Technologies Help Restore Independence for Injured Marine Sergeant in Customized Smart Home.
Access all the specification tools and resources you need for your next project.
WattStopper’s Next Generation Outdoor Sensors
In the midst of the pandemic, commercial spaces, offices in particular, have been greatly impacted by social distancing requirements. As we look to our future return to the workplace, adjusting to new health and safety restrictions will require innovative solutions to keep employees safe.
Leagrand puts stylish design and modern conveniences at homeowners’ fingertips with affordable switches, outlets and home automation controls.
Legrand's Infinium acclAIM platform redefines backbone connectivity by replacing traditional cassette-based designs with direct mating breakout connections. This architecture supports ultra-high-density fiber deployments, up to 288 fibers per rack unit, effectively doubling the density of conventional LC-based panels while maintaining exceptional optical performance through precision ceramic ferrule technology.
Legrand North and Central America will showcase a range of new products at Greenbuild 2019.
Enabling connected outdoor lighting systems for smarter, more energy efficient, and data-driven applications
Get prepped and ready for the season of visitors and overnight guests, with these tips for holiday hosting.
Want to control your lights from anywhere? With the Netatmo Solutions and Legrand Home + Control app, you can manage and monitor lights from anywhere.
Looking to replace standard outlets with built-in USB charging ports? Here are our favorite spots to add one.
The success of implementing a reliable intelligent building depends on an efficient structured cabling infrastructure.
Legrand® Launches Wattstopper® Fixture Integrated Outdoor/High Bay Sensors with Bluetooth® Commissioning
Legrand, North & Central America announced today the development of new Wattstopper FDP-300 Series sensors.
Get inspired for your next project. See how designer switches and outlets can elevate any space, with our video gallery.
Legrand, North & Central America is displaying the latest innovations within the Wattstopper® integrated lighting controls line at LIGHTFAIR International 2018 Booth #1843.