5
Browse 1,094 results for
"dimmer"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Brand
Choose from one of Legrand's brands.
Product Family
Used to identify and differentiate offerings within a particular product line. Product families are typically treated as adjectives. It is not recommended to use the product line (ex: Wiremold®) and product family names (Evolution™) together. This will introduce a level of unnecessary confusion for the audience.
Product Series
A collection of related products that share a common design, technology, or purpose. Products within the series either maintain a cohesive brand / style identity or work together to serve a particular solution.
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Timer Type
The mechanism by which the timer operates, such as mechanical, digital, or programmable.
Outlet Type
Describes the unique qualities or characteristics of an electrical outlet that make it better suited to different uses. The listed qualities may give the outlet improved safety performance, increased efficiency, or additional functionality.
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
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
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
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
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
Sensor Technology
The technology used by a device to sense a change in signal or stimulus.
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
Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.
Compatibility
Capability of Being Used with or Connected to Different Types of Devices or Components without any Modifications
Works With
Need to ensure your choice works with your device, system, or software? Select your needs using this filter to confirm compatibility.
Bulb Compatibility
Indicates the type(s) of lighting a dimmer or controller is designed to work with, ensuring proper functionality and performance.
Electrical Rating
The maximum load or capacity of electrical power a dimmer switch is rated to manage when linked to a specific type of light bulb.
On Function
Describes the mode of operation for devices that can be turned on, indicating whether they stay on continuously or operate on a timer or sensor.
Lighting Types
Different forms of light a device is able to provide.
Throw Type
Describes the method of switch operation, indicating whether it controls one circuit (single-throw) or switches between two circuits (double-throw).
Operating Temperature
The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit
Operating Temperature Max
Indicates the highest possible temperature a device can be safely used without the risk of failure or damage.
Storage Temperature
Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
Number of Wires
The Number of Pliable Metallic Strand or Rod Made in Many Lengths and Diameters and are Electrically Insulated, Used Conduct Electricity
Wire Connection Type
Describes the method used to connect wires to the device, such as screw terminals, push-in connectors, or lead wires.
Timing Range
The Time Span for Which the System/Device is in Desired Active/Working Mode
Connection TypeTooltip Title
Style or Type of Connection Used
Line Frequency
The frequency of alternating current (AC) in an electrical power system, measured in Hz. Also commonly referred to as Utility Frequency, Power Line Frequency, or Mains Frequency.
NEMA Configuration Code
Alpha-Numeric Code Applied to Connectors to Guarantee Consistency and Interchageability Between Manufacturers
Terminal Accommodation
Describes the type and size of wire that the receptacle's terminals can securely hold (typically provided as a range in gauge size).
USB Amperage
Describes the maximum electrical current the conductor or device can carry through its USB ports before sustaining immediate or progressive deterioration.
Contact Configuration
Different Switching Functions of the Relay Contacts
Contact Rating
The Voltage, Current, and Power Capacities of Relay Contacts Under Specified Environmental Conditions
Sensing Range
The total Possible Sensing Capability of the Sensor, Beginning After the Deadband, and Extending Out as Far as the Sensor is Able to Reach Effectively
Sensor Coverage
Describes the total area, measured in square footage, within which a sensor can detect presence or movement.
Sensor Coverage Pattern
Describes the shape of the area that a sensor is able to detect presence or movement within, measured in degrees.
Wireless Range
Describes the maximum distance wireless devices can be separated while preserving signal quality and reliability.
Protocol
A Convention or Standard that Controls or Enables the Connection, Communication, and Data Transfer Between Two Computing Endpoints, the Rules Governing the Syntax, Semantics, and Synchronization of Communication
Maximum Horsepower Rating
The maximum power load the device can handle before the risk of damage or failure.
Thickness
The Dimension Through an Object as Opposed to its Length or Width
Number of Gangs
The amount of switches on the plate.
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
Publishing Date Range
Date article, blog, or press release was published.
Filter by Product Category
Filter downloadable resources by the product category they relate or are relevant to.
Brand
Choose from one of Legrand's brands.
Resource Type
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
See how fast this tablet charges with radiant USB type A and Type C outlets.
See how the radiant wireless charger is the ultimate power charging station for your home.
Get inspired for your next project. See how designer switches and outlets can elevate any space, with our photo gallery.
Leagrand puts stylish design and modern conveniences at homeowners’ fingertips with affordable switches, outlets and home automation controls.
Nightlights built into outlets make for easy children to see in the dark.
See how Smart Lighting from the radiant® Collection controls your lights on your schedule.
Upgraded outlets in the playroom with built-in nightlights perfect for kids.
Blogger Colleen of Lemon Thistle upgraded her outlet to help her kids navigate the room more safely at night.
See how adorne and radiant can elevate kitchens by saving space and adding convenience, with our photo gallery.
See how designer switches and outlets can provide the most convenient and aesthetic way to safely meet code for ground-fault protection.
radiant switch and timer switch for automatic and manual lighting control.
See how designer switches and outlets can provide code-compliant ground fault protection in a clever, contemporary design.
See how designer wall plates can elevate your next kitchen renovation.
See how designer switches and outlets can provide power wherever you need it.
See how designer switches and outlets can offer convenience and germ-free control.
See how designer switches and outlets give access to three plugs simultaneously, then disappears back into the wall or counter
See how designer switches and outlets from the radiant Collection are available in a smooth nickel finish that perfectly complements a wide range of kitchen hardware.
The Macassar Wall Plate from the adorne® Collection uses one of the world’s most beautiful woods to engage the eye with its bold contrast and texture.
The Brushed Black Nickel Wall Plate plays off other dark-hued elements, while the brushed texture specifically softens it to better coordinate with cooler, lighter shades of green and blue.
See how designer switches and outlets can equip your kitchen with the necessary power to keep your mixer, blender, tablet and phone within reach.
See how designer switches and outlets can add modern functionality without compromising your space’s charm.
See how adorne and radiant can elevate the spaces where you celebrate, entertain, or share a delicious meal, with our photo gallery.
See how designer switches and outlets can light up a soft and classic dining room
See how radiant Smart Lighting pairs with digital assistants like Google Home.
Complement the décor of your home with designer switches and outlets from the radiant Collection.
Vanilla Ice showcases how he used custom Wall Plates from adorne® to compliment the look of gorgeous wallpaper. Can you see these in your home? #adornemyhome
See how designer switches and outlets can elevate bedrooms and master suites, with our photo gallery.
These adorne® Switches with Locator Light mean never ever fumbling in the dark to hit the lights.