5
Browse 1,643 results for
"outlet"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Brand
Choose from one of Legrand's brands.
Product Family
Used to identify and differentiate offerings within a particular product line. Product families are typically treated as adjectives. It is not recommended to use the product line (ex: Wiremold®) and product family names (Evolution™) together. This will introduce a level of unnecessary confusion for the audience.
Product Series
A collection of related products that share a common design, technology, or purpose. Products within the series either maintain a cohesive brand / style identity or work together to serve a particular solution.
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Timer Type
The mechanism by which the timer operates, such as mechanical, digital, or programmable.
Outlet Type
Describes the unique qualities or characteristics of an electrical outlet that make it better suited to different uses. The listed qualities may give the outlet improved safety performance, increased efficiency, or additional functionality.
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
Floor Type
Floor construction product is designed to work in
Wall Plate Type
Refers to the style or intended usage of a wall plate.
Connector Style
The design or type of the connector used to join electrical circuits together.
Connector Type
The Type of Connectors / Terminals that Tool can Crimp to Wire or Cable
Product Certifications
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
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
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
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
Sensor Technology
The technology used by a device to sense a change in signal or stimulus.
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
Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.
Compatibility
Capability of Being Used with or Connected to Different Types of Devices or Components without any Modifications
Works With
Need to ensure your choice works with your device, system, or software? Select your needs using this filter to confirm compatibility.
Bulb Compatibility
Indicates the type(s) of lighting a dimmer or controller is designed to work with, ensuring proper functionality and performance.
On Function
Describes the mode of operation for devices that can be turned on, indicating whether they stay on continuously or operate on a timer or sensor.
Lighting Types
Different forms of light a device is able to provide.
Service Capacity
Denotes the number of different services that can be used within a product as a result of separated internal compartments, including electrical, low voltage, water, air, and more.
Throw Type
Describes the method of switch operation, indicating whether it controls one circuit (single-throw) or switches between two circuits (double-throw).
Operating Temperature
The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit
Operating Temperature Max
Indicates the highest possible temperature a device can be safely used without the risk of failure or damage.
Storage Temperature
Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.
Is the Device Prewired?
Denotes whether a product comes prewired for quicker installation.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
Number of Wires
The Number of Pliable Metallic Strand or Rod Made in Many Lengths and Diameters and are Electrically Insulated, Used Conduct Electricity
Wire Connection Type
Describes the method used to connect wires to the device, such as screw terminals, push-in connectors, or lead wires.
Timing Range
The Time Span for Which the System/Device is in Desired Active/Working Mode
Connection TypeTooltip Title
Style or Type of Connection Used
Flanged
Indicates whether a device is designed with a raised edge/rim, on or around its receptacle, for superior strength, handling, or attachment to another object.
Line Frequency
The frequency of alternating current (AC) in an electrical power system, measured in Hz. Also commonly referred to as Utility Frequency, Power Line Frequency, or Mains Frequency.
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
Describes the maximum electrical current the conductor or device can carry through its USB ports before sustaining immediate or progressive deterioration.
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
Number of Channels
The Number of Media Used to Convey Information
Number of Conductors
The Number of Materials/Strands/Pairs Which Contain Movable Electric Charges
Contact Configuration
Different Switching Functions of the Relay Contacts
Contact Rating
The Voltage, Current, and Power Capacities of Relay Contacts Under Specified Environmental Conditions
Sensing Range
The total Possible Sensing Capability of the Sensor, Beginning After the Deadband, and Extending Out as Far as the Sensor is Able to Reach Effectively
Sensor Coverage
Describes the total area, measured in square footage, within which a sensor can detect presence or movement.
Sensor Coverage Pattern
Describes the shape of the area that a sensor is able to detect presence or movement within, measured in degrees.
Wireless Range
Describes the maximum distance wireless devices can be separated while preserving signal quality and reliability.
Protocol
A Convention or Standard that Controls or Enables the Connection, Communication, and Data Transfer Between Two Computing Endpoints, the Rules Governing the Syntax, Semantics, and Synchronization of Communication
Single/Multimode
Describes the mode of fiber either utilized or accepted by a device to transmit or receive a fiber optic signal.
Circular Outlet Diameter
Refers to the diameter of the circular opening in a wall plate, which should match the diameter of the outlet it is intended to cover.
Receptacle Spacing
Refers to the distance between power outlets or receptacles on a device, which can be important for planning the layout of plugs and connectors.
Box Depth
The measurement from the front opening to the back of an electrical box, indicating the volume of wiring it can contain.
Knockout Size
Physical dimension of the knock-out size, could be diameter or a range
Core Hole Size
Physical Dimensions of the hole
Internal Depth
Refers to the distance from the surface level of a box to the area where internal devices are plugged in, illustrating the available space within to accommodate cords, receptacles, and large devices.
Thickness
The Dimension Through an Object as Opposed to its Length or Width
Wall Plate Size
The general size of the the included wall plate. The size may determine whether it suits your personal application!
Cable Length
The Longest Dimension of Insulated Conductors
Cord Length
The Linear Extent of Cord in Space from one End to the Other
Wire Gauge
Measuring and Indicating a Quantity of Wire
Number of Gangs
The amount of switches on the plate.
Number of Buttons
The Number of Keys/Switches in the item Used for Selecting a Particular Function
Number of Switches
Number of electrical switches
Number of Outlets
The Different Types of Receptacles Providing a Place in a Wiring System Where Current can be Taken to Supply Electrical Devices
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
Publishing Date Range
Date article, blog, or press release was published.
Filter by Product Category
Filter downloadable resources by the product category they relate or are relevant to.
Brand
Choose from one of Legrand's brands.
Resource Type
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
Get your home game-day ready with tips for creating the optimal sports viewing setup and more.
Explore lighting control solutions for commercial office spaces that can save energy and boost employee productivity.
Designating a space for working out at home? Here are some tips for an optimal home gym setup.
Get inspired for your next project. View our video gallery to see product highlights, featured projects, DIY installation tips and more.
Innovative WattStopper hi/low sensor for outdoor LED fixtures wins top honors in Consulting-Specifying Engineer reader survey
The radiant Easy Kits aren’t just simple to install – they are simple to upgrade. Here’s how to gain additional features like app control and voice command.
See how adorne and radiant can elevate kitchens by saving space and adding convenience, with our photo gallery.
Meet ASHRAE 90.1 energy code compliance with Legrand's tools and design guides for specific spaces found in common commercial building spaces. Learn more here.
Reduce the complexity of designing for energy code compliance with tools and design resources from Legrand. Explore IECC design recommendations and resources.
Completely Customizable Keypad Combines a Sleek Design With Programmable Buttons for One-Touch Scenes
First Sound Bar In Nuvo Player Portfolio Line Takes Center Stage at ISE
Learn how a stunning Hollywood Hills Home used Vantage Control products to make a smart home with our automation solutions.
Get inspired for your next project. See how designer switches and outlets can elevate any space, with our video gallery.
Legrand offers smart lighting solutions to fit every lifestyle, application or project.
Explore project ideas for every room to see how designer switches and outlets can elevate your space.
Access all the specification tools and resources you need for your next project.
Legrand offers a wide array of products that supply convenient power and charging access – including units that install directly into furniture. Learn more.
Read how blogger Amie, inspired by the HGTV Smart Home, upgraded her own home’s switches and outlets.
FIRST SOUND BAR IN NUVO PLAYER PORTFOLIO LINE TAKES CENTER STAGE AT ISE
LEGRAND LAUNCHES P500 PLAYER PORTFOLIO SOUND BAR
FIRST SOUND BAR IN NUVO PLAYER PORTFOLIO LINE FEATURED BY LEGRAND AT CEDIA 2017
Vantage to Debut New EasyTouch Glass Keypad at CEDIA Expo 2019
Find innovation for commercial, residential and industrial electrical wiring. Explore Pass & Seymour switches, receptacles, GFCI outlets, USB chargers and more.
Wattstopper lighting control products are designed to meet code, ensure ease of installation, and enable the control of light. Learn more.
Read how Orlando Soria, interior designer and founder of Hommemaker, brightened up his space with designer switches and outlets from the adorne® Collection.
With designer switches and outlets from the radiant® Collection, upgrading your space with style and innovation starts at the wall
Legrand introduced a new low-voltage dual-relay output accessory device and a low-voltage input interface device, both of which extend the capabilities of the Wattstopper® Digital Lighting Management (DLM) system.
Download all the necessary software and resources to run your Wattstopper digital light management or architectural dimming system.
Get inspired for your next project. See how designer switches and outlets can elevate any space, with our photo gallery.
Smart Wi-Fi Light switches and dimmers from Legrand allow users to easily control light and power from a smart home lighting system or Matter hub.