5
Browse 929 results for
"adorne"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Brand
Choose from one of Legrand's brands.
Connector
A Device that Establishes a Connection Between Two or More Units.
Number of Receptacles
The Number of Electrical Wall Outlets Designed for Use with a Plug
Sensor Type
The Device that Receives a Signal or Stimulus (As Heat or Pressure or Light or Motion Etc.) and Responds to it in a Distinctive Manner
Amperage
Maximum electrical current the conductor or device can carry before sustaining immediate or progressive deterioration
Installation Location
Where a Device is or is to be Installed
Load
The Maximum Amount of Power Which the item can withstand or Operate without any performance Loss
NEMA Rating
National Electrical Manufacturers Association Ratings are Standards that are Useful in Defining the Types of Environments in Which an Electrical Enclosure can be Used
Phase
The Factional Part of the Period of a Sinusoidal Wave, Usually Expressed in Electrical Degrees and Referenced to the origin
Availability
Product is available to buy on Legrand.us
Compatibility
Capability of Being Used with or Connected to Different Types of Devices or Components without any Modifications
Product Certifications
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
Is Tamper-Resistant
Tamper resistance is resistance to tampering (intentional malfunction or sabotage) by either the normal users of a product, package, or system or others with physical access to it.
Number of Gangs
The amount of switches on the plate.
Connection
Between Discrete Points Allows the Flow of Electrons (Electric Current)
Temperature Rating
The Designated / Rated / Maximum / Range Temperature at Which the Instrument May be Used in Continuous Operation without Loss of its Basic Properties and performance
Is Weather Resistant
Is this product listed as Weather Resistant ?
Frequency Rating
The Number of Occurrences within a Given Time Period, the Rate at Which Alternating Current Makes a Complete Cycle of Reversals
Indoor/Outdoor
Enviromental Conditions rating on the product. Indoor Only, Outdoor, Both
Number of Ports
The Number of Application-Specific or Process-Specific Software Construct Serving as a Communication Endpoint / is Generally a Specific Place for Being Physically Connected to Some Other Device /A Number of Physical Access Point(S) Between a Conductor and
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Timer Duration
Amount of Time a Timer can Last
Input Voltage
The Difference of Electrical Potential Between Two Points of an Electrical or Electronic Circuit Entering a System
Number of Wires
The Number of Pliable Metallic Strand or Rod Made in Many Lengths and Diameters and are Electrically Insulated, Used Conduct Electricity
Timing Range
The Time Span for Which the System/Device is in Desired Active/Working Mode
Thickness
The Dimension Through an Object as Opposed to its Length or Width
Load Type
Denotes the type(s) of load that can be applied to a dimmer, which determines its compatible light sources.
Mounting Type
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
Current Rating
Maximum Amount of Current a Cable can Carry Before Sustaining Damage or Deterioration
Sensitivity
The Minimum Input Which the Device can Sense and Produce the Output
Number of Ways
The Number of Connections the Unit can Provide
Number of USBs
Number of USB ports
Wall Plate Color
Color of the Plate that Covers a Switch on a Wall
Contact
A Device that Joins Electric Conductors Mechanically and Electrically to Other Conductors and to the Terminals of Apparatus and Equipment
Wire Size
It is the Normal Size of the Conductors for Building Wire
Enclosure Type
Style, Type, Size, Etc. of the Enclosure of a Device
Construction
The Act or Process of Constructing Which Includes Design and Manufacture Type
Cord Length
The Linear Extent of Cord in Space from one End to the Other
Orientation
The Position or Alignment Relative to Points of the Compass or Other Specific Directions
Product Family
Filter to specific families of related products that share common characteristics, designs, or functions.
NEMA Configuration Code
Alpha-Numeric Code Applied to Connectors to Guarantee Consistency and Interchageability Between Manufacturers
Load Rating
The maximum load that a device is designed to withstand without breakage or loss of performance.
Battery
A Device for Converting Chemical Energy Into Electrical Energy a Group of Two or More Connected Voltaic Cells
Connection TypeTooltip Title
Style or Type of Connection Used
Lighting Types
Different forms of light a device is able to provide.
Receptacle Type
The physical character of a Receptacle. The Type/Specification of a Contact Device Installed at the Outlet for the Connection of an Attachment Plug a Single Receptacle is a Single Contact Device with No Other Contact Device on the Same Yoke a Multiple Receptacle is Two or More Contact Devices.
Protocol
A Convention or Standard that Controls or Enables the Connection, Communication, and Data Transfer Between Two Computing Endpoints, the Rules Governing the Syntax, Semantics, and Synchronization of Communication
Sensing Range
The total Possible Sensing Capability of the Sensor, Beginning After the Deadband, and Extending Out as Far as the Sensor is Able to Reach Effectively
Number of Switches
Number of electrical switches
Voltage
The Rate at Which Energy is Drawn from a Source that Produces a Flow of Electricity in a Circuit
Operating Temperature
The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit
Included
The Supplementary items Supplied with the Product Which May be Necessary for the Optimum Operation of the Product
Supply Voltage
The Specified Amount and Type Voltage / Voltage Range for Which the Equipment is Rated for Operation
Product Has Potential to Contribute to LEED
This product contributes to earning credits in the LEED rating system.
Wire Connection Type
Describes the method used to connect wires to the device, such as screw terminals, push-in connectors, or lead wires.
Preset
Denotes whether a dimmer returns lights to their previously-selected light level when turned on.
On Function
Describes the mode of operation for devices that can be turned on, indicating whether they stay on continuously or operate on a timer or sensor.
Seismic Tested
Indicates whether a device has been tested to withstand and/or perform under certain seismic conditions.
Sensor Coverage
Describes the total area, measured in square footage, within which a sensor can detect presence or movement.
Standard
The industrial standard(s) to which a device is manufactured, operated, or tested.
Cutout Shape
The geometric form of the cutout area, which must match the shape of the device or component being installed.
Device Front Face Size
Describes the general proportions of a product's front face relative to the overall device.
USB Wattage
Describes the maximum electrical power a USB receptacle can safely output.
Dimming Compatibility
Describes the method(s) used by a device or system to adjust the brightness of a lighting load.
Application Sector
Refers to the expected environment(s) or intended usage(s) for a product (e.g. Residential, Commercial, Industrial, etc.).
Trim/Adjustment Level
A control feature that allows the adjustment of the minimum and maximum light levels to prevent issues such as flickering at lower brightness levels, ensuring smooth and stable dimming performance.
Wall Plate Included
Indicates if the device comes with a cover plate for aesthetic integration with the wall.
Works With
Need to ensure your choice works with your device, system, or software? Select your needs using this filter to confirm compatibility.
Sensor Coverage Pattern
Describes the shape of the area that a sensor is able to detect presence or movement within, measured in degrees.
Dimming Phase
Refers to the point in the AC power cycle at which the dimmer begins to reduce voltage to the light. "Leading Edge" dimmers cut the initial phase and are typically used for incandescent bulbs, while "Trailing Edge" dimmers cut the end phase, which is more suitable for LEDs.
Horsepower Rating
Refers to the power capacity of a device under normal load conditions, measured in horsepower (HP).
Requires Neutral Wire
Indicates whether a device requires a neutral wire to function properly.
Wall Plate Type
Refers to the style or intended usage of a wall plate.
Operating Humidity
Describes the range of humidity at which a device can be utilized safely without the risk of failure or damage.
Connection Location
Specifies where on the device the electrical connections are made, which can affect installation.
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Throw Type
Describes the method of switch operation, indicating whether it controls one circuit (single-throw) or switches between two circuits (double-throw).
Line Frequency
The frequency of alternating current (AC) in an electrical power system, measured in Hz. Also commonly referred to as Utility Frequency, Power Line Frequency, or Mains Frequency.
Maximum Humidity
The highest level of atmospheric moisture a device can withstand without compromising functionality or safety.
Features
Unique characteristics and functionality that set the product apart from others in its field.
Number of Phases
Indicates the number of electrical phases a device utilizes.
Sensor Technology
The technology used by a device to sense a change in signal or stimulus.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
Internal Depth
Refers to the distance from the surface level of a box to the area where internal devices are plugged in, illustrating the available space within to accommodate cords, receptacles, and large devices.
Warranty Type
The product warranty that accompanies the specific product.
Wall Plate Size
The general size of the the included wall plate. The size may determine whether it suits your personal application!
Terminal Accommodation
Describes the type and size of wire that the receptacle's terminals can securely hold (typically provided as a range in gauge size).
Environmental Conditions
Describes the relative range of climatic standards a device can safely operate within.
Finish
Describes the specific surface treatment applied to the outer product for either aesthetics and/or durability.
Bulb Compatibility
Indicates the type(s) of lighting a dimmer or controller is designed to work with, ensuring proper functionality and performance.
Device Backbody Size
Describes the general proportions of a product's backbody relative to the overall device.
Outlet Type
Describes the unique qualities or characteristics of an electrical outlet that make it better suited to different uses. The listed qualities may give the outlet improved safety performance, increased efficiency, or additional functionality.
Location Rating
Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.
Category Performance Application
Refers to the specific standard used to define an ethernet cable's capabilities and its intended usage. Most commonly shortened to"Cat" and a number (e.g. Cat5e; Cat6; Cat6a).
Material
Indicates the primary material(s) used to construct a product.
Wiring Method
Describes the design and ways of connecting various parts of a device with cable and/or wire.
USB Amperage
Describes the maximum electrical current the conductor or device can carry through its USB ports before sustaining immediate or progressive deterioration.
Filter to Specific Product Groups
Filter by named groups of related products, including product families, series, systems, and solutions. Groupings may indicate similar styles of products, or signify how they're designed to operate together as a complete solution.
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
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
Bright ideas abound with adorne® illumination products. When it comes to brilliant solutions, the adorne® Collection really shines.
See how to bind lights throughout your home for the adorne Whole House Lighting System.
See how to program your adorne Tru-Universal Dimmer for precise light level control, no matter your lighting type.
Watch to see how easy it is to add power right where you need it, with the adorne Furniture Power Center.
Easily upgrade your outlets with the designer style of adorne. Watch this video to see how.
Watch this short how-to video for a step-by-step guide to installing adorne switches.
Give your guests a stay to remember by focusing on the details. With the adorne Collection, choose from an array of finishes and colors that match your hotel’s decor.
Warranty information for products from the adorne® Collection of designer switches and outlets.
Browse images to see how adorne switches, outlets and USB charging were a stylish, easy solution for the historic building turned hotel: Quirk Richmond.
Designer switches and dimmers form the heart of the adorne® Collection. Whether you favor a simple touch (like on your smartphone), a satisfying click, or even the simple wave of a hand, adorne® makes it a delight to hit the lights.
Take a quick peek at some designer switches and outlets from the adorne® Collection with this TV spot highlighting innovative products like the Pop-Out Outlet and Wave Switch.
View the guest room of JW Marriott Mall of America, where the bedside charging station is created with adorne Power and USB Outlets.
Pairing the adorne Switches in magnesium with a sleek dark Wall Plate
Upgrade to devices both brilliant and beautiful. Check out the adorne® Collection of designer switches and outlets.
Say goodbye to outdated switches and outlets. Say hello to The adorne® Collection.
Watch this short how-to video for a step-by-step guide to installing adorne dimmers.
See how designer switches and outlets can provide code-compliant ground fault protection in a clever, contemporary design.
See how designer switches and outlets can provide power wherever you need it.
See how designer switches and outlets can offer convenience and germ-free control.
The designer switches and outlets from adorne feature modern style and function, including the latest technologies for control and charging.
The ideal smart lighting solutions for whole-home use, meet adorne® & radiant® with Netatmo.
The adorne® Collection makes life simply beautiful, putting a stylish and innovative finishing touch on your home. Turn ordinary into extraordinary with designer switches and outlets.
Say goodbye to boring switches and hello to breathtaking design elements, with the adorne® Collection's elegant selection of designer switches and outlets.
The designer switches, dimmers, outlets and more from the adorne® Collection can take your home from basic to stylishly functional.
See how adorne outlets can charge your devices while matching the aesthetic of your room.
Adding the wow factor to any upgrade. Catch the adorne® Touch Switch in this TV spot from 2018.
Turn the lights on with a simple touch. Check out the clever Touch Switch from the adorne® Collection.
“How awesome is that?!” Check out the awesome adorne® USB Outlet in this TV spot from 2018.
Easily find your switch or dimmer in the dark, with a simple-to-install locator light. Watch to see how.