5
Browse 2,049 results for
"switch"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Product Family
Used to identify and differentiate offerings within a particular product line. Product families are typically treated as adjectives. It is not recommended to use the product line (ex: Wiremold®) and product family names (Evolution™) together. This will introduce a level of unnecessary confusion for the audience.
Product Series
A collection of related products that share a common design, technology, or purpose. Products within the series either maintain a cohesive brand / style identity or work together to serve a particular solution.
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Timer Type
The mechanism by which the timer operates, such as mechanical, digital, or programmable.
Outlet Type
Describes the unique qualities or characteristics of an electrical outlet that make it better suited to different uses. The listed qualities may give the outlet improved safety performance, increased efficiency, or additional functionality.
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
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
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
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
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
Sensor Technology
The technology used by a device to sense a change in signal or stimulus.
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
Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.
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
Bulb Compatibility
Indicates the type(s) of lighting a dimmer or controller is designed to work with, ensuring proper functionality and performance.
Electrical Rating
The maximum load or capacity of electrical power a dimmer switch is rated to manage when linked to a specific type of light bulb.
On Function
Describes the mode of operation for devices that can be turned on, indicating whether they stay on continuously or operate on a timer or sensor.
Lighting Types
Different forms of light a device is able to provide.
Throw Type
Describes the method of switch operation, indicating whether it controls one circuit (single-throw) or switches between two circuits (double-throw).
Operating Temperature
The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit
Operating Temperature Max
Indicates the highest possible temperature a device can be safely used without the risk of failure or damage.
Storage Temperature
Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.
Is the Device Prewired?
Denotes whether a product comes prewired for quicker installation.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
Number of Wires
The Number of Pliable Metallic Strand or Rod Made in Many Lengths and Diameters and are Electrically Insulated, Used Conduct Electricity
Wire Connection Type
Describes the method used to connect wires to the device, such as screw terminals, push-in connectors, or lead wires.
Timing Range
The Time Span for Which the System/Device is in Desired Active/Working Mode
Connection TypeTooltip Title
Style or Type of Connection Used
Line Frequency
The frequency of alternating current (AC) in an electrical power system, measured in Hz. Also commonly referred to as Utility Frequency, Power Line Frequency, or Mains Frequency.
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
Describes the maximum electrical current the conductor or device can carry through its USB ports before sustaining immediate or progressive deterioration.
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
Contact Configuration
Different Switching Functions of the Relay Contacts
Contact Rating
The Voltage, Current, and Power Capacities of Relay Contacts Under Specified Environmental Conditions
Sensing Range
The total Possible Sensing Capability of the Sensor, Beginning After the Deadband, and Extending Out as Far as the Sensor is Able to Reach Effectively
Sensor Coverage
Describes the total area, measured in square footage, within which a sensor can detect presence or movement.
Sensor Coverage Pattern
Describes the shape of the area that a sensor is able to detect presence or movement within, measured in degrees.
Wireless Range
Describes the maximum distance wireless devices can be separated while preserving signal quality and reliability.
Protocol
A Convention or Standard that Controls or Enables the Connection, Communication, and Data Transfer Between Two Computing Endpoints, the Rules Governing the Syntax, Semantics, and Synchronization of Communication
Data Transfer Rate
The Speed at Which Data is Transferred from one Location to Another with in the Time Frame
Maximum Horsepower Rating
The maximum power load the device can handle before the risk of damage or failure.
Max Distance Support
Refers to the maximum range a signal can be effectively supported to by a device.
Receptacle Spacing
Refers to the distance between power outlets or receptacles on a device, which can be important for planning the layout of plugs and connectors.
Box Depth
The measurement from the front opening to the back of an electrical box, indicating the volume of wiring it can contain.
Enclosure Size
The approximate height of the compatible wiring enclosure.
Knockout Size
Physical dimension of the knock-out size, could be diameter or a range
Internal Depth
Refers to the distance from the surface level of a box to the area where internal devices are plugged in, illustrating the available space within to accommodate cords, receptacles, and large devices.
Thickness
The Dimension Through an Object as Opposed to its Length or Width
Wall Plate Size
The general size of the the included wall plate. The size may determine whether it suits your personal application!
Cable Length
The Longest Dimension of Insulated Conductors
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
The Different Types of Receptacles Providing a Place in a Wiring System Where Current can be Taken to Supply Electrical Devices
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
Publishing Date Range
Date article, blog, or press release was published.
Filter by Product Category
Filter downloadable resources by the product category they relate or are relevant to.
Brand
Choose from one of Legrand's brands.
Resource Type
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
Easily install the Smart Tru-Universal Dimmer from the radiant Collection.
Watch this short video to learn how to configure your radiant Collection Smart Lighting in multiple locations.
Elevate any space with the designer wall plates, made to exclusively fit switches and outlets from the adorne and radiant Collections.
See the simple set up of the Smart Plug-In Dimmer, Wi-Fi from the radiant Collection.
Setup Matter smart lights, dimmers and outlets in Amazon Alexa to control your home’s lighting with this step-by-step guide.
Using Microban’s innovative technology, Legrand’s newest switches, dimmers and wall plates feature built-in antimicrobial protection that will last the entire lifetime of a product.
Explore living room project ideas for every room to see how designer switches and outlets can elevate your space.
Read our top home upgrades and projects to support the transition of summer to back-to-school with new lighting controls, outlets and wall plates.
Explore bathroom project ideas for every room to see how designer switches and outlets can elevate your space.
Explore kitchen project ideas for every room to see how designer switches and outlets can elevate your space.
Explore bedroom project ideas for every room to see how designer switches and outlets can elevate your space.
Elevate any space with the exceptional style and innovative functionality of designer switches and outlets. Available in two distinct collections.
Learn to setup and use Smart Lighting devices for control through the Smart Lights app.
Check out the HGTV Smart Home, featuring devices from the adorne and radiant Collections of designer switches and outlets.
Read how blogger Amie, inspired by the HGTV Smart Home, upgraded her own home’s switches and outlets.
Get inspired with these 2020 trends for bathroom remodels and makeovers.
Wattstopper offers simple, scalable and flexible, energy-efficient networked lighting controls and solutions for commercial applications. Browse lighting control products and solutions for spaces where occupants learn, work, and heal.
Smart Wi-Fi Light switches and dimmers from Legrand allow users to easily control light and power from a smart home lighting system or Matter hub.
With multiple smart lighting solutions available, watch to discover which Legrand option works best for your home.
See how to program your adorne Tru-Universal Dimmer for precise light level control, no matter your lighting type.
Watch to see how easy it is to add power right where you need it, with the adorne Furniture Power Center.
Easily upgrade your outlets with the designer style of adorne. Watch this video to see how.
Watch this short how-to video for a step-by-step guide to installing adorne switches.
Legrand, North & Central America recently announced the promotion of Amy Hahne as the new Vice President and General Manager of Shading Systems for its Building Controls Systems (BCS) division.
View wallbox devices that are compatible with your commercial lighting controls system. Wattstopper offers dimmers, timers, switches, and more.
View wallbox devices that are compatible with your commercial lighting controls system. Wattstopper offers dimmers, timers, switches, and more.
Matter-enabled devices offer a convenient way to integrate multiple types of devices into a smart home system so they all communicate with each other.
Easily find your switch or dimmer in the dark, with a simple-to-install locator light. Watch to see how.
See how blogger Charlene transformed drab dimmers on her accent wall into a custom, touch-enabled statement piece with adorne.