5
Browse 1,758 results for
"outlet"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Brand
Choose from one of Legrand's brands.
Product Family
Used to identify and differentiate offerings within a particular product line. Product families are typically treated as adjectives. It is not recommended to use the product line (ex: Wiremold®) and product family names (Evolution™) together. This will introduce a level of unnecessary confusion for the audience.
Product Series
A collection of related products that share a common design, technology, or purpose. Products within the series either maintain a cohesive brand / style identity or work together to serve a particular solution.
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Timer Type
The mechanism by which the timer operates, such as mechanical, digital, or programmable.
Outlet Type
Describes the unique qualities or characteristics of an electrical outlet that make it better suited to different uses. The listed qualities may give the outlet improved safety performance, increased efficiency, or additional functionality.
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
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
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
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
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
Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.
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
Describes the mode of operation for devices that can be turned on, indicating whether they stay on continuously or operate on a timer or sensor.
Lighting Types
Different forms of light a device is able to provide.
Service Capacity
Denotes the number of different services that can be used within a product as a result of separated internal compartments, including electrical, low voltage, water, air, and more.
Throw Type
Describes the method of switch operation, indicating whether it controls one circuit (single-throw) or switches between two circuits (double-throw).
Operating Temperature
The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit
Operating Temperature Max
Indicates the highest possible temperature a device can be safely used without the risk of failure or damage.
Storage Temperature
Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.
Is the Device Prewired?
Denotes whether a product comes prewired for quicker installation.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
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
Indicates whether a device is designed with a raised edge/rim, on or around its receptacle, for superior strength, handling, or attachment to another object.
Line Frequency
The frequency of alternating current (AC) in an electrical power system, measured in Hz. Also commonly referred to as Utility Frequency, Power Line Frequency, or Mains Frequency.
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
Describes the maximum electrical current the conductor or device can carry through its USB ports before sustaining immediate or progressive deterioration.
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
The total Possible Sensing Capability of the Sensor, Beginning After the Deadband, and Extending Out as Far as the Sensor is Able to Reach Effectively
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
A Convention or Standard that Controls or Enables the Connection, Communication, and Data Transfer Between Two Computing Endpoints, the Rules Governing the Syntax, Semantics, and Synchronization of Communication
Single/Multimode
Describes the mode of fiber either utilized or accepted by a device to transmit or receive a fiber optic signal.
Circular Outlet Diameter
Refers to the diameter of the circular opening in a wall plate, which should match the diameter of the outlet it is intended to cover.
Receptacle Spacing
Refers to the distance between power outlets or receptacles on a device, which can be important for planning the layout of plugs and connectors.
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
Refers to the distance from the surface level of a box to the area where internal devices are plugged in, illustrating the available space within to accommodate cords, receptacles, and large devices.
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
Publishing Date Range
Date article, blog, or press release was published.
Filter by Product Category
Filter downloadable resources by the product category they relate or are relevant to.
Brand
Choose from one of Legrand's brands.
Resource Type
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
Light switch timers and occupancy/vacancy sensors offer automated control for convenience and energy savings in the home while allowing for precise lighting control.
Emergency Lighting Controls from Wattstopper ensure increased safety and energy-savings in commercial spaces. View the products.
Smart lighting schedules help automate lighting for convenience, energy efficiency and safety, all accessible through the Legrand Home + Control app.
Lighting industry leader, Legrand, has partnered with HGTV to be the exclusive supplier of the lighting controls charging and power outlets used throughout the HGTV® Smart Home 2017.
Find innovation for commercial, residential and industrial electrical wiring. Explore Pass & Seymour switches, receptacles, GFCI outlets, USB chargers and more.
Control your Legrand smart light switches in Google Home with voice commands using these step-by-step instructions.
Legrand announced that its radiant® RF (radio frequency) Lighting Control and adorne® Wi-Fi Ready Lighting systems now work with Amazon Alexa.
Legrand announced that its radiant® RF (radio frequency) Lighting Control and adorne® Wi-Fi Ready Lighting systems now work with the Google Assistant for seamless voice control.
Legrand announced that its radiant® RF Lighting Control and adorne® Wi-Fi Ready Lighting systems now work with Amazon Alexa.
New Matter-enabled devices from the radiant® Collection, developed using Amazon’s Alexa Connect Kit for Matter, are on preview at the 2024 Consumer Electronics Show.
Legrand will showcase new technologies and finishes for the connect home at IBS 2022 in Orlando, FL with Breegan Jane.
Legrand announces new partnership with Leanne Ford.
Consider some of these ideas for your next weekend project and add a little something extra, fresh, and new to your home.
Where to Install a Motion Sensor Light, motion sensor and light switch, motion sensor closet light
WattStopper's Eric Fournier Joins CABA Board of Directors
Pennsylvania is adopting a new energy conservation code effective Oct. 1, 2018 through an update of the Pennsylvania Uniform Construction Code (UCC). The 2015 IECC will be the new building efficiency standard statewide except for in the city of Philadelphia, which is adopting the newer 2018 IECC standard.
Legrand®, a global leader in electrical and digital building infrastructures, today announced the launch of the Wattstopper Graphic Switch Touchscreen.
Legrand, a global specialist in electrical and network infrastructure solutions, will showcase its portfolio of hospitality-focused products at HD Expo 2017
Discover Legrand’s home builder technology solutions like smart lighting, USB charging outlets, wifi readiness, AV connectivity, home theater connections, etc.
Completely Customizable Keypad Combines a Sleek Design With Programmable Buttons for One-Touch Scenes
CES 2019, Legrand will demonstrate a suite of leading connected devices that underscore the company’s continued commitment to developing technologies that are more intuitive, maximize comfort and safety.
Legrand continues to show its proud support of those who serve our country by providing product donations and volunteering time to complete the latest Building Homes for Heroes® home gifted to a local injured veteran last week.
Legrand, North America is previewing the latest Wattstopper solutions that bring effortless and integrated lighting controls into modern commercial spaces at LEDucation 2017.
Vantage to Debut New EasyTouch Glass Keypad at CEDIA Expo 2019
Get more accomplished while working remotely with these tips for boosting your productivity.
Utah recently passed its Construction Code Modifications bill, updating the commercial building energy efficiency code from the 2015 International Energy Conservation Code (IECC) to the 2018 IECC effective July 1, 2019.
As technology experts, AV Integrators seamlessly integrate lighting control, shading, audio, video and home automation systems to function cohesively.
Rhode Island has adopted a new building code, joining numerous cities and states in 2019 that have moved toward more stringent standards to increase energy efficiency and performance in commercial buildings.
From cutsheets to installation guides, download all your Wattstopper Architectural Dimming resources from one convenient spot!
Read to learn about the five must-have lighting control integrations that create a smooth, technology-forward experience for both students, faculty, and staff.