5
Browse 101 results for
"High Density Fiber"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Brand
Choose from one of Legrand's brands.
Product Type
Select a Product Type to find products that share the same basic form and function, such as switches, cables, panels, or electrical boxes.
Mounting
Something that Serves as a Support, Setting, or Backing for the item
Connector Type
The Type of Connectors / Terminals that Tool can Crimp to Wire or Cable
Cable Type
The Type of a Assembly of one or More Insulated Conductors, or Optical Fibers
Compatibility
Capability of Being Used with or Connected to Different Types of Devices or Components without any Modifications
Product Certifications
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
Connector
Refers to the specific types of connections a device uses to join electrical conductors and create an electrical circuit. When you select the first desired connector, a second filter will appear listing any connectors on the opposite end of your selected connector on a device.
Capacity
The Load for Which a Generating Unit, Generating Plant or Other Electrical Apparatus is Rated Either by the User or by the Manufacturer, Electrical Phenomenon Whereby an Electric Charge is Stored
Number of Ports
The Number of Application-Specific or Process-Specific Software Construct Serving as a Communication Endpoint / is Generally a Specific Place for Being Physically Connected to Some Other Device /A Number of Physical Access Point(S) Between a Conductor and
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Gauge
Indicates the specific thickness or diameter of wire or cable, which determines the amount of electrical current that can be safely carried.
Outside Diameter
A Straight Line Passing Through the Center of a Circle or Sphere and Meeting the Circumference or Surface at Each End
Form Factor
The Size, Configuration, or Physical Arrangement of the Unit
Rack Units Rack Units_030104
Unit Used to Describe the Height of Equipment Intended for Mounting
Construction
The Act or Process of Constructing Which Includes Design and Manufacture Type
Shielded/Unshielded
Denotes whether a cable is designed with an extra layer of metal foil or braid surrounding the inner conductor to protect against electromagnetic interference (EMI).
Simplex/Duplex
A Communications Network can Provide one-Way / Multi-Way Communication Service
Cable Length
The Longest Dimension of Insulated Conductors
Color
The color of the product itself
Operating Temperature
The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit
Included
The Supplementary items Supplied with the Product Which May be Necessary for the Optimum Operation of the Product
Product Width
The overall width of the product.
Product Has Potential to Contribute to LEED
This product contributes to earning credits in the LEED rating system.
Operating Temperature Min
Indicates the lowest possible temperature a device can be safely used without the risk of failure or damage.
Jacket Material
The outer material used to insulate a cord or cable's wiring.
Fanout Cable Length
How long the individual legs are for the cords that have been broken out of the primary cable assembly.
Polish Type
The polish method used on the final fiber end face of a device.
Panel Configuration
The specific layout and organization of the panels that house the fiber optic connections.
Standard
The industrial standard(s) to which a device is manufactured, operated, or tested.
Storage Temperature
Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.
Maximum Insertion Loss
The maximum loss in load power due to the insertion of a component or device at some point in a transmission system.
Frame
Describes characteristics of a device's frame that make it more suited for specific applications.
Fiber Size
The outer diameter of an optical fiber core, cladding and coating, expressing microns.
Application Sector
Refers to the expected environment(s) or intended usage(s) for a product (e.g. Residential, Commercial, Industrial, etc.).
Polarity Type
The specific configuration used to map the "transmit" and "receive" fibers within a fiber optic system.
Fiber Optic Cable Type
The different types and characteristics of fiber optical cable designed for specific applications.
Shelves
Refers to the number of shelves either present or possible within a rack cabinet or enclosure.
Product Depth
The overall depth of a product.
Durability
Indicates whether a device is designed for standard or rugged usage.
Connector Color
Refers to the color of a device's electrical or data connector.
Operating Humidity
Describes the range of humidity at which a device can be utilized safely without the risk of failure or damage.
Jacket Application
Describes the specific application(s) a cable's jacket is designed to be used in, such as in-wall, plenum, or riser.
Product Height
The overall height of a product.
Connectivity Footprint
Refers to the unique application or solution that products like connectivity adapters, jacks, or panels can fit within or are compatible with.
Compliance
Denotes any established standards a product is built to or behaves in accordance to.
Number of Fanout Cables
The quantity of individual fanout cables that branch out at the end of a cable.
Single/Multimode
Describes the mode of fiber either utilized or accepted by a device to transmit or receive a fiber optic signal.
Features
Unique characteristics and functionality that set the product apart from others in its field.
Bend Radius
The minimum radius a cable, cord, or wire can bend without kinking it, damaging it, or shortening its life.
Fanout Cable Diameter
Measure of the outer diameter of the jacket of each fanout cord within the cable assembly.
Operating Temperature Max
Indicates the highest possible temperature a device can be safely used without the risk of failure or damage.
Warranty Type
The product warranty that accompanies the specific product.
Typical Insertion Loss
Refers to the most common amount of signal lost at a connection/mating point, measured in decibels (dB).
Finish
Describes the specific surface treatment applied to the outer product for either aesthetics and/or durability.
Product Length
The overall length of a product.
Return Loss
Refers to the loss of power in the signal returned/reflected by a discontinuity in a transmission line or optical fiber.
Performance Level/Tier
Describes the specific variation of performance capabilities a device is designed to support.
Jacket Rating
Denotes the NEC (National Electric Code) standards the outer casing/jacket surrounding a cable or cord's internal wiring and insulation is rated to.
Shuttered Adapters
Refers to to the cap/door mechanism on a panel or insert that remains closed to help prevent contaminants from entering the ferrule end face, but can be opened to insert/install a connector.
Fiber Density
Denotes the capacity optical fibers have to carry video signals or data streams at various resolutions.
Material
Indicates the primary material(s) used to construct a product.
Cable Diameter
The typical outer diameter of a cable.
Filter to Specific Product Groups
Filter by named groups of related products, including product families, series, systems, and solutions. Groupings may indicate similar styles of products, or signify how they're designed to operate together as a complete solution.
Stock Level
Filter your results to only in-stock products sold directly on legrand.us.
Publishing Date Range
Date article, blog, or press release was published.
Brand
Choose from one of Legrand's brands.
Category
Our brands, products, resources, and pages are group into divisions. Filter and find a product, resource, or page you are looking for based on a Legrand category.
Filter by Product Category
Filter downloadable resources by the product category they relate or are relevant to.
Brand
Choose from one of Legrand's brands.
Resource Type
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
Legrand's Infinium High Density fiber optic solutions offer the same advanced performance and reliability that you've come to expect from our standard density product line. Explore high density fiber today.
Explore our acclAIM solution, which offers high-density fiber infrastructure and is key to increasing data center network efficiency, capacity, and performance.
Legrand's newest Clarity® jack and panel products solve density challenges without sacrificing performance. Learn about Ortronics High Density Copper today.
Legrand delivered a smart, scalable data center solution that empowered a global social media platform to optimize performance, efficiency, and growth with future-ready infrastructure.
Cisco selected the Infinium acclAIM Fiber Solution to run their Network Operation Center (NOC) at this year’s Cisco Live event in Las Vegas, NV.
Legrand is a global leader in network infrastructure solutions, with a broad range of copper and fiber connectivity, racks, cabinets and cable management.
Chroma Link™, a revolutionary color-indexed fiber optic cabling solution designed for hyper-dense AI and machine learning networks. Chroma Link offers a turnkey approach to connectivity that transforms data center deployments.
Legrand offers fiber optic solutions that are designed to deliver the most advanced network performance, with a variety of density and connector options for maximum compatibility. Explore Legrand’s Fiber Optic Solutions today.
New Fiber Enclosure designed to simplify cable management, visibility and versatility.
The Infinium™ HD-Enhanced Enclosure is an ideal solution for fiber networks in data centers and building networks. Find the ideal solution for your fiber networks today.
Legrand pre-terminated fiber trunk cable assemblies offer a streamlined approach to network design. View Ortronics Fiber Trunk Cable System today.
Fiber Optic brochures, white papers, videos, solution guides and data sheets. Download Legrand Fiber Optic resources today!
Legrand solutions have supported the Cisco Live NOC for several years, with 2025 marking the fourth consecutive year that Legrand's acclAIM high-density fiber system has played a key role.
New connector innovations make it easier to make the right choices to provide more fiber optic connections in less space.
Legrand Introduces The Infinium acclAIM™ Fiber Solution — With Direct Connectivity To Replace MTP/MPO Cassette-Based Solutions.
Data center complexity is on the rise. Hyperscale, edge and cloud computing are experiencing rampant growth. To address emerging infrastructure design challenges, data center managers’ mantra has become “less is more.”
Your guide to achieving better optical performance, increasing scalability, and lowering costs by phasing out cassette-based forms of cable management.
Modularity is at the heart of data center mobility and scalability, enabled by innovative solutions to set up and change over critical cabling components.
Legrand's Infinium acclAIM platform redefines backbone connectivity by replacing traditional cassette-based designs with direct mating breakout connections. This architecture supports ultra-high-density fiber deployments, up to 288 fibers per rack unit, effectively doubling the density of conventional LC-based panels while maintaining exceptional optical performance through precision ceramic ferrule technology.
Enjoy unsurpassed network performance within your data center or building network with fiber, copper, active networking solutions and more. Learn more.
Infinium acclAIM redefines cable connectivity by replacing pre-terminated cassette-based connectors with direct connections enabling significantly simplified install, the lowest optical loss and lower costs
Company helps Cisco connect tens of thousands of people year after year with innovative digital infrastructure solutions.
Offered under their shared brand, nCompass Systems, the new Extended Distance product enables data and power transport at distances exceeding TIA standards
Legrand, unveils four new Active Optical (AOC) HDMI cables that can distribute high-definition HDMI signals, including 4K UltraHD and HDR content, and other high-speed, high-performance AV features, to distances of up to 75 meters (246 feet).
Legrand can meet the demands of any building network installation with a full line of both copper and fiber optic connectivity products. Explore our connectivity solutions.
Legrand Ortronics® network infrastructure solutions combine flexibility and efficiency, with superior design, to ensure that facilities operate flawlessly.
These cables provide a cost-effective solution at extended lengths while meeting 4K UltraHD specifications, as compared to more expensive fiber optic HDMI and HDBaseT2 alternatives.
Legrand's Infinium Access UHD+ Enclosure has been named among the best in the industry by the esteemed 2024 Lightwave Innovation Reviews.
One thing is clear with data centers: The demand for computing power will continue to increase, and data centers will constantly evolve to keep pace. Data center networks are powerhouses. Data generation is ballooning with the uptake of cutting-edge technologies, such as IoT and AI.
Five Data Infrastructure Solutions Recognized with Innovators Awards at BICSI Fall 2019