5
Browse 75 results for
"digital timers"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Brand
Choose from one of Legrand's brands.
Product Family
Used to identify and differentiate offerings within a particular product line. Product families are typically treated as adjectives. It is not recommended to use the product line (ex: Wiremold®) and product family names (Evolution™) together. This will introduce a level of unnecessary confusion for the audience.
Product Series
A collection of related products that share a common design, technology, or purpose. Products within the series either maintain a cohesive brand / style identity or work together to serve a particular solution.
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Timer Type
The mechanism by which the timer operates, such as mechanical, digital, or programmable.
Sensor Type
The Device that Receives a Signal or Stimulus (As Heat or Pressure or Light or Motion Etc.) and Responds to it in a Distinctive Manner
Lens Type
The type of lens that the adapter is fixing to.
Product Certifications
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
Features
Unique characteristics and functionality that set the product apart from others in its field.
Availability
Product is available to buy on Legrand.us
Material
Indicates the primary material(s) used to construct a product.
Mounting Type
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
Standard
The industrial standard(s) to which a device is manufactured, operated, or tested.
Load Rating
The maximum load that a device is designed to withstand without breakage or loss of performance.
Load Type
Denotes the type(s) of load that can be applied to a dimmer, which determines its compatible light sources.
Amperage
Maximum electrical current the conductor or device can carry before sustaining immediate or progressive deterioration
Input Voltage
The Difference of Electrical Potential Between Two Points of an Electrical or Electronic Circuit Entering a System
Voltage
The Rate at Which Energy is Drawn from a Source that Produces a Flow of Electricity in a Circuit
Sensor Technology
The technology used by a device to sense a change in signal or stimulus.
Application Sector
Refers to the expected environment(s) or intended usage(s) for a product (e.g. Residential, Commercial, Industrial, etc.).
Indoor/Outdoor
Enviromental Conditions rating on the product. Indoor Only, Outdoor, Both
Installation Location
Where a Device is or is to be Installed
Requires Neutral Wire
Indicates whether a device requires a neutral wire to function properly.
Location Rating
Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.
Compatibility
Capability of Being Used with or Connected to Different Types of Devices or Components without any Modifications
Bulb Compatibility
Indicates the type(s) of lighting a dimmer or controller is designed to work with, ensuring proper functionality and performance.
Electrical Rating
The maximum load or capacity of electrical power a dimmer switch is rated to manage when linked to a specific type of light bulb.
On Function
Describes the mode of operation for devices that can be turned on, indicating whether they stay on continuously or operate on a timer or sensor.
Throw Type
Describes the method of switch operation, indicating whether it controls one circuit (single-throw) or switches between two circuits (double-throw).
Operating Temperature
The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit
Operating Temperature Max
Indicates the highest possible temperature a device can be safely used without the risk of failure or damage.
Storage Temperature
Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
Wire Connection Type
Describes the method used to connect wires to the device, such as screw terminals, push-in connectors, or lead wires.
Timing Range
The Time Span for Which the System/Device is in Desired Active/Working Mode
Connection TypeTooltip Title
Style or Type of Connection Used
Line Frequency
The frequency of alternating current (AC) in an electrical power system, measured in Hz. Also commonly referred to as Utility Frequency, Power Line Frequency, or Mains Frequency.
Terminal Accommodation
Describes the type and size of wire that the receptacle's terminals can securely hold (typically provided as a range in gauge size).
Wattage
amount of watts used
Contact Rating
The Voltage, Current, and Power Capacities of Relay Contacts Under Specified Environmental Conditions
Sensing Range
The total Possible Sensing Capability of the Sensor, Beginning After the Deadband, and Extending Out as Far as the Sensor is Able to Reach Effectively
Sensor Coverage
Describes the total area, measured in square footage, within which a sensor can detect presence or movement.
Sensor Coverage Pattern
Describes the shape of the area that a sensor is able to detect presence or movement within, measured in degrees.
Wireless Range
Describes the maximum distance wireless devices can be separated while preserving signal quality and reliability.
Product Length
The overall length of a product.
Number of Gangs
The amount of switches on the plate.
Number of Buttons
The Number of Keys/Switches in the item Used for Selecting a Particular Function
Number of Switches
Number of electrical switches
Brand
Choose from one of Legrand's brands.
Category
Our brands, products, resources, and pages are group into divisions. Filter and find a product, resource, or page you are looking for based on a Legrand category.
Filter by Product Category
Filter downloadable resources by the product category they relate or are relevant to.
Brand
Choose from one of Legrand's brands.
Resource Type
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
Less waste, less worry, with timed lighting control from the radiant® Collection. Never accidentally leave the lights again.
Light switch timers and occupancy/vacancy sensors offer automated control for convenience and energy savings in the home while allowing for precise lighting control.
Visitors to Lightfair 2018 will be able to see a sneak peek of upcoming state-of-the art wireless lighting control solutions, touchscreen interface, and design tool for Wattstopper Digital Lighting Management (DLM), the industry’s most powerful and easy-to-use lighting controls platform from Legrand® North & Central America. These latest DLM solutions and capabilities are on display at LIGHTFAIR International 2018 at booth #1843.
Leagrand puts stylish design and modern conveniences at homeowners’ fingertips with affordable switches, outlets and home automation controls.
In the midst of the pandemic, commercial spaces, offices in particular, have been greatly impacted by social distancing requirements. As we look to our future return to the workplace, adjusting to new health and safety restrictions will require innovative solutions to keep employees safe.
Wattstopper lighting control products are designed to meet code, ensure ease of installation, and enable the control of light. Learn more.
Digital Lighting Management enhanced room controllers allow users to monitor the electrical current (amperage) passing through the device at any moment in time.
See how designer switches and outlets can elevate bedrooms and master suites, with our photo gallery.
Daylight savings is coming to an end, meaning less natural light and a higher demand for lighting control will be in season. Many homeowners and facility managers may find their energy consumption increases during the fall and winter months, which is why Legrand’s Building Control Systems division has put together a guide to help homeowners and facility managers make simple changes to reduce their energy footprint and save on electricity bills.
Explore bedroom project ideas for every room to see how designer switches and outlets can elevate your space.
Enhance resilient design through access to backup power and reduce light pollution.
Pennsylvania is adopting a new energy conservation code effective Oct. 1, 2018 through an update of the Pennsylvania Uniform Construction Code (UCC). The 2015 IECC will be the new building efficiency standard statewide except for in the city of Philadelphia, which is adopting the newer 2018 IECC standard.
Legrand Provides Brilliant Ideas for Gifts and Resolutions to Brighten Your Spaces This Holiday Season
Get inspired for your next project. See how designer switches and outlets can elevate any space, with our photo gallery.
LFI 2016: Legrand Showcases Code Compliant Control Solutions for Indoor and Outdoor LED Luminaires
Legrand announces that three of its Wattstopper products have been accepted into the 2017 IES (Illuminating Engineering Society) Progress report which seeks to highlight developments in the art and science of lighting throughout the world.
Vantage has partnered with CoolAutomation for HVAC integration. View answers to frequently asked questions about the Vantage & CoolAutomation Integration.
Alliance Pairs Vantage’s Customizable Lighting Controls With Proluxe by American Lighting Fixtures to Deliver Dynamic End-to-End Lighting Solution
Alliance Pairs Vantage’s Customizable Lighting Controls With AiSPiRE’s Human-Centric Luminaires to Deliver End-to-End Dynamic Lighting Solution
Alliance Pairs Vantage’s Customizable Lighting Controls With Environmental Lights’LED LightingFixturesto Deliver Dynamic,End-to-End Lighting Solution
With good planning and the use of energy monitoring and home automation technologies, we can all do our part to reduce the flow of energy consumption.