5
Browse 1,094 results for
"dimmer"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Brand
Choose from one of Legrand's brands.
Product Family
Used to identify and differentiate offerings within a particular product line. Product families are typically treated as adjectives. It is not recommended to use the product line (ex: Wiremold®) and product family names (Evolution™) together. This will introduce a level of unnecessary confusion for the audience.
Product Series
A collection of related products that share a common design, technology, or purpose. Products within the series either maintain a cohesive brand / style identity or work together to serve a particular solution.
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Timer Type
The mechanism by which the timer operates, such as mechanical, digital, or programmable.
Outlet Type
Describes the unique qualities or characteristics of an electrical outlet that make it better suited to different uses. The listed qualities may give the outlet improved safety performance, increased efficiency, or additional functionality.
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
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
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
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
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
Sensor Technology
The technology used by a device to sense a change in signal or stimulus.
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
Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.
Compatibility
Capability of Being Used with or Connected to Different Types of Devices or Components without any Modifications
Works With
Need to ensure your choice works with your device, system, or software? Select your needs using this filter to confirm compatibility.
Bulb Compatibility
Indicates the type(s) of lighting a dimmer or controller is designed to work with, ensuring proper functionality and performance.
Electrical Rating
The maximum load or capacity of electrical power a dimmer switch is rated to manage when linked to a specific type of light bulb.
On Function
Describes the mode of operation for devices that can be turned on, indicating whether they stay on continuously or operate on a timer or sensor.
Lighting Types
Different forms of light a device is able to provide.
Throw Type
Describes the method of switch operation, indicating whether it controls one circuit (single-throw) or switches between two circuits (double-throw).
Operating Temperature
The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit
Operating Temperature Max
Indicates the highest possible temperature a device can be safely used without the risk of failure or damage.
Storage Temperature
Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
Number of Wires
The Number of Pliable Metallic Strand or Rod Made in Many Lengths and Diameters and are Electrically Insulated, Used Conduct Electricity
Wire Connection Type
Describes the method used to connect wires to the device, such as screw terminals, push-in connectors, or lead wires.
Timing Range
The Time Span for Which the System/Device is in Desired Active/Working Mode
Connection TypeTooltip Title
Style or Type of Connection Used
Line Frequency
The frequency of alternating current (AC) in an electrical power system, measured in Hz. Also commonly referred to as Utility Frequency, Power Line Frequency, or Mains Frequency.
NEMA Configuration Code
Alpha-Numeric Code Applied to Connectors to Guarantee Consistency and Interchageability Between Manufacturers
Terminal Accommodation
Describes the type and size of wire that the receptacle's terminals can securely hold (typically provided as a range in gauge size).
USB Amperage
Describes the maximum electrical current the conductor or device can carry through its USB ports before sustaining immediate or progressive deterioration.
Contact Configuration
Different Switching Functions of the Relay Contacts
Contact Rating
The Voltage, Current, and Power Capacities of Relay Contacts Under Specified Environmental Conditions
Sensing Range
The total Possible Sensing Capability of the Sensor, Beginning After the Deadband, and Extending Out as Far as the Sensor is Able to Reach Effectively
Sensor Coverage
Describes the total area, measured in square footage, within which a sensor can detect presence or movement.
Sensor Coverage Pattern
Describes the shape of the area that a sensor is able to detect presence or movement within, measured in degrees.
Wireless Range
Describes the maximum distance wireless devices can be separated while preserving signal quality and reliability.
Protocol
A Convention or Standard that Controls or Enables the Connection, Communication, and Data Transfer Between Two Computing Endpoints, the Rules Governing the Syntax, Semantics, and Synchronization of Communication
Maximum Horsepower Rating
The maximum power load the device can handle before the risk of damage or failure.
Thickness
The Dimension Through an Object as Opposed to its Length or Width
Number of Gangs
The amount of switches on the plate.
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
Publishing Date Range
Date article, blog, or press release was published.
Filter by Product Category
Filter downloadable resources by the product category they relate or are relevant to.
Brand
Choose from one of Legrand's brands.
Resource Type
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
See how to set the exact lighting you need – from anywhere, with Smart Lighting from the radiant Collection.
Enjoy complete control over your home’s lighting with the touch of a button, with Legrand RF Lighting Control.
Read how blogger Leslie upgraded her kitchen into a colorful masterpiece, complete with Brushed Brass Wall Plates from the adorne® Collection.
Looking to reduce your energy consumption in 2024? Upgrade your residential lighting with LED bulbs, monitor consumption and install dimming switches.
Smart Lighting Control Systems help to automate and control lighting and power in the home, enabling scheduling and timing to support your lifestyle.
Take a quick peek at some designer switches and outlets from the adorne® Collection with this TV spot highlighting innovative products like the Pop-Out Outlet and Wave Switch.
Upgrade to devices both brilliant and beautiful. Check out the adorne® Collection of designer switches and outlets.
Say goodbye to outdated switches and outlets. Say hello to The adorne® Collection.
“How awesome is that?!” Check out the awesome adorne® USB Outlet in this TV spot from 2018.
Start 2020 right; read our roundup of the top design trends for the new decade!
Learn more about installing Smart Lighting from the radiant Collection.
Read how bloggers Chris and Julia tackled three problem areas in their home, all in a single afternoon.
Just wave. Check out the ingenious Wave Switch from the adorne® Collection.
Adding the wow factor to any upgrade. Catch the adorne® Touch Switch in this TV spot from 2018.
Turn the lights on with a simple touch. Check out the clever Touch Switch from the adorne® Collection.
Unplug from ordinary with the adorne® Pop-Out™ Outlet. This clever solution hides your outlet until you need it. Simply push on the square face to "pop out" the outlets, then push the face back in for a smooth finish.
Innovative and easy, see the adorne® Wave Switch in action, in this TV spot from 2018.
See how simple it is to set schedules and scenes for your perfect lighting with this short video from Danny Winget.
See how easy it is to install Smart Lighting from the radiant Collection, with this short tutorial from Danny Winget.
Explore the year’s biggest design trends from Dallas Market 2019.
“You’ve got to see this.” Check out the uniquely brilliant adorne® Pop-Out Outlet in this TV spot from 2018.
Sometimes the simplest changes make the biggest difference, and nowhere is design detail more important than in a luxury home.
Read how blogger Anne upgraded her home with designer switches and outlets from the adorne® Collection.
Designer switches and outlets are the perfect finishing touch. Explore options for elevating your property and enhancing the guest experience.
Discover Legrand's latest innovations in lighting control solutions. Explore cutting-edge innovations for seamless LED dimming and advanced lighting control experiences.
adorne® GFCI Outlet with Brushed Stainless Steel Wall Plate adds stunning style to this bathroom space.
See how adorne outlets can charge your devices while matching the aesthetic of your room.
Smart Lighting from the radiant collection adds function and style to any room.
Pairing the adorne Switches in magnesium with a sleek dark Wall Plate