5
Browse 103 results for
"motion sensor"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Brand
Choose from one of Legrand's brands.
Product Type
Select a Product Type to find products that share the same basic form and function, such as switches, cables, panels, or electrical boxes.
Connector
A Device that Establishes a Connection Between Two or More Units.
Frequency Band
A Continuous Group, or Range, of Frequencies with an Upper Limit and a Lower Limit
Sensor Type
The Device that Receives a Signal or Stimulus (As Heat or Pressure or Light or Motion Etc.) and Responds to it in a Distinctive Manner
Amperage
Maximum electrical current the conductor or device can carry before sustaining immediate or progressive deterioration
Installation Location
Where a Device is or is to be Installed
NEMA Rating
National Electrical Manufacturers Association Ratings are Standards that are Useful in Defining the Types of Environments in Which an Electrical Enclosure can be Used
Availability
Product is available to buy on Legrand.us
Compatibility
Capability of Being Used with or Connected to Different Types of Devices or Components without any Modifications
Product Certifications
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
Number of Gangs
The amount of switches on the plate.
Connection
Between Discrete Points Allows the Flow of Electrons (Electric Current)
Antenna
A Conductor or Set of Conductors Used to Radiate RF Energy Into Space or to Collect RF Energy from Space or to Do Both
Indoor/Outdoor
Enviromental Conditions rating on the product. Indoor Only, Outdoor, Both
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Input Voltage
The Difference of Electrical Potential Between Two Points of an Electrical or Electronic Circuit Entering a System
Load Type
Denotes the type(s) of load that can be applied to a dimmer, which determines its compatible light sources.
Mounting Type
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
Number of Buttons
The Number of Keys/Switches in the item Used for Selecting a Particular Function
Sensitivity
The Minimum Input Which the Device can Sense and Produce the Output
Has Battery
A Device for Converting Chemical Energy Into Electrical Energy a Group of Two or More Connected Voltaic Cells
Response Frequency
Frequency response is the quantitative measure of the output spectrum of a system or device in response to a stimulus, and is used to characterize the dynamics of the system. It is a measure of magnitude and phase of the output as a function of frequency, in comparison to the input.
Wire Size
It is the Normal Size of the Conductors for Building Wire
Enclosure Type
Style, Type, Size, Etc. of the Enclosure of a Device
Load Rating
The maximum load that a device is designed to withstand without breakage or loss of performance.
Wattage
amount of watts used
Connection TypeTooltip Title
Style or Type of Connection Used
Target Size
The Dimensional Specification of the Object Which is Set as a Target for the Sensor
Color
The color of the product itself
Sensing Range
The total Possible Sensing Capability of the Sensor, Beginning After the Deadband, and Extending Out as Far as the Sensor is Able to Reach Effectively
Number of Switches
Number of electrical switches
Voltage
The Rate at Which Energy is Drawn from a Source that Produces a Flow of Electricity in a Circuit
Operating Temperature
The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit
Included
The Supplementary items Supplied with the Product Which May be Necessary for the Optimum Operation of the Product
Product Has Potential to Contribute to LEED
This product contributes to earning credits in the LEED rating system.
Wire Connection Type
Describes the method used to connect wires to the device, such as screw terminals, push-in connectors, or lead wires.
Operating Temperature Min
Indicates the lowest possible temperature a device can be safely used without the risk of failure or damage.
On Function
Describes the mode of operation for devices that can be turned on, indicating whether they stay on continuously or operate on a timer or sensor.
Engraving Type
Refers to the available styles to mark or inscribe text, symbols, or patterns on a product.
Seismic Tested
Indicates whether a device has been tested to withstand and/or perform under certain seismic conditions.
Sensor Coverage
Describes the total area, measured in square footage, within which a sensor can detect presence or movement.
Antenna Pattern
Captures the directional representation of how radio waves are sent and received by the antenna.
Standard
The industrial standard(s) to which a device is manufactured, operated, or tested.
Sensitivity Adjustment
Refers to any customization settings, or range of adjustments for motion detection sensitivity, required to turn lights on.
Storage Temperature
Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.
Device Front Face Size
Describes the general proportions of a product's front face relative to the overall device.
Indicator
Describes the type/specification of signaling a device uses to indicate abnormal and/or operating conditions.
Antenna Gain
A calculated measure of how effectively an antenna sends or receives radio signals in a particular direction, measured in dBi (Decibals relative to isotropic).
Timer Type
The mechanism by which the timer operates, such as mechanical, digital, or programmable.
Application Sector
Refers to the expected environment(s) or intended usage(s) for a product (e.g. Residential, Commercial, Industrial, etc.).
Trim/Adjustment Level
A control feature that allows the adjustment of the minimum and maximum light levels to prevent issues such as flickering at lower brightness levels, ensuring smooth and stable dimming performance.
Topology
The arrangement in which the Nodes of a LAN are connected to each other.
Wall Plate Included
Indicates if the device comes with a cover plate for aesthetic integration with the wall.
Works With
Need to ensure your choice works with your device, system, or software? Select your needs using this filter to confirm compatibility.
Sensor Coverage Pattern
Describes the shape of the area that a sensor is able to detect presence or movement within, measured in degrees.
Dimming Phase
Refers to the point in the AC power cycle at which the dimmer begins to reduce voltage to the light. "Leading Edge" dimmers cut the initial phase and are typically used for incandescent bulbs, while "Trailing Edge" dimmers cut the end phase, which is more suitable for LEDs.
Horsepower Rating
Refers to the power capacity of a device under normal load conditions, measured in horsepower (HP).
Current Draw
The amount of electrical current the device uses during operation, measured in amperes (or amps).
Requires Neutral Wire
Indicates whether a device requires a neutral wire to function properly.
Operating Humidity
Describes the range of humidity at which a device can be utilized safely without the risk of failure or damage.
Connection Location
Specifies where on the device the electrical connections are made, which can affect installation.
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Wireless Range
Describes the maximum distance wireless devices can be separated while preserving signal quality and reliability.
Line Frequency
The frequency of alternating current (AC) in an electrical power system, measured in Hz. Also commonly referred to as Utility Frequency, Power Line Frequency, or Mains Frequency.
Features
Unique characteristics and functionality that set the product apart from others in its field.
Sensor Technology
The technology used by a device to sense a change in signal or stimulus.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
Operating Temperature Max
Indicates the highest possible temperature a device can be safely used without the risk of failure or damage.
Warranty Type
The product warranty that accompanies the specific product.
Terminal Accommodation
Describes the type and size of wire that the receptacle's terminals can securely hold (typically provided as a range in gauge size).
Environmental Conditions
Describes the relative range of climatic standards a device can safely operate within.
Finish
Describes the specific surface treatment applied to the outer product for either aesthetics and/or durability.
Product Length
The overall length of a product.
Ultrasonic Frequency
Describes the specific frequency at which a sensor emits and detects sound waves in order to measure distances, detect objects, or perform other functions.
Light Level Adjustment
Captures the range over which a device can adjust the intensity of light in order to maintain the desired ambient light setpoint, enhancing comfort and energy savings.
Device Backbody Size
Describes the general proportions of a product's backbody relative to the overall device.
Number of Rockers
The total number of rocker-type electrical switches included on a device. Typically used to switch between two or more functions.
Sensor Mounting Height
Describes the optimal vertical distance at which a sensor should be installed to ensure reliable detection of motion or other target conditions.
Location Rating
Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.
Material
Indicates the primary material(s) used to construct a product.
Filter to Specific Product Groups
Filter by named groups of related products, including product families, series, systems, and solutions. Groupings may indicate similar styles of products, or signify how they're designed to operate together as a complete solution.
Stock Level
Filter your results to only in-stock products sold directly on legrand.us.
Publishing Date Range
Date article, blog, or press release was published.
Brand
Choose from one of Legrand's brands.
Category
Our brands, products, resources, and pages are group into divisions. Filter and find a product, resource, or page you are looking for based on a Legrand category.
Filter by Product Category
Filter downloadable resources by the product category they relate or are relevant to.
Brand
Choose from one of Legrand's brands.
Resource Type
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
Where to Install a Motion Sensor Light, motion sensor and light switch, motion sensor closet light
Light switch timers and occupancy/vacancy sensors offer automated control for convenience and energy savings in the home while allowing for precise lighting control.
Enabling connected outdoor lighting systems for smarter, more energy efficient, and data-driven applications
Elevate any space with the innovative functionality of hands-free touchless light switches and dimmers from the adorne and radiant Collections.
Planning spring home improvement projects? Update switches and outlets, upgrade to dimmer switches, add smart lighting controls or install an EV charger.
Monitor data center or facility environments in real-time with sensors engineered for easy deployment while providing accurate data and insight. Learn more.
Are you familiar with the different types of light switches for the home? Read our guide on the types and best use cases for your lighting control.
Learn more about how Passive Infrared Sensor systems react to energy sources, “noticing” the difference in the heat emitted between the human body and the background.
Legrand, North America today announced the availability of the Wattstopper FSP-202 and FSP-212 sensors, the latest IP66-rated additions to the FSP-200 Series line of occupancy sensors with daylight controls.
WattStopper’s Next Generation Outdoor Sensors
Wattstopper FSP-600 Series, a next-generation wireless in-fixture lighting control solution. Featuring 0–10V dimming with integrated motion sensing, daylight harvesting, and wireless networking, the FSP-600 delivers flexible, scalable control for a wide range of applications.
To create a greener lighting design that offers intelligent lighting, Vantage lighting controls were used at Hotel Verdant for optimal control and flexibility.
Vantage lighting controls helped this hotel meet its sustainability and design needs through freedom of design and providing energy-efficient lighting control.
Legrand® Launches Wattstopper® Fixture Integrated Outdoor/High Bay Sensors with Bluetooth® Commissioning
Legrand, North & Central America announced today the development of new Wattstopper FDP-300 Series sensors.
Read how bloggers Chris and Julia tackled three problem areas in their home, all in a single afternoon.
Extended height WattStopper occupancy sensor allows more facilities to benefit from digital lighting control solutions
Innovative WattStopper hi/low sensor for outdoor LED fixtures wins top honors in Consulting-Specifying Engineer reader survey
Explore bathroom project ideas for every room to see how designer switches and outlets can elevate your space.
Perfect for any kitchen and bathroom upgrade, touchless options for lighting control, sink faucets and more can add convenience while reducing mess.
See how designer switches and outlets can offer convenience and germ-free control.
Looking to reduce your energy consumption in 2024? Upgrade your residential lighting with LED bulbs, monitor consumption and install dimming switches.
From standard LED dimming to stylish smart lighting, Legrand offers a full spectrum of residential lighting and fan controls to meet any home’s needs.
Daylight savings is coming to an end, meaning less natural light and a higher demand for lighting control will be in season. Many homeowners and facility managers may find their energy consumption increases during the fall and winter months, which is why Legrand’s Building Control Systems division has put together a guide to help homeowners and facility managers make simple changes to reduce their energy footprint and save on electricity bills.
Elevate any space with the exceptional style and innovative functionality of designer switches from the adorne and radiant Collections.
Legrand, North & Central America is displaying the latest innovations within the Wattstopper® integrated lighting controls line at LIGHTFAIR International 2018 Booth #1843.
The designer switches and outlets from adorne feature modern style and function, including the latest technologies for control and charging.
Vantage announces partnership with CoolAutomation, a leader in smart climate control solutions. Learn more about their alliance and integration.
Elevate any space with the exceptional style and innovative functionality of designer dimmers from the adorne and radiant Collections.
San Jose, CA, September 15, 2016 – Consulting-Specifying Engineer Magazine Readers Award Wattstopper® with Two Product of the Year Awards.