5
Browse 488 results for
"wireless"
Brand
Choose from one of Legrand's brands.
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Product Certifications
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
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
National Electrical Manufacturers Association Ratings are Standards that are Useful in Defining the Types of Environments in Which an Electrical Enclosure can be Used
Contact Rating
The Voltage, Current, and Power Capacities of Relay Contacts Under Specified Environmental Conditions
Compatibility
Capability of Being Used with or Connected to Different Types of Devices or Components without any Modifications
Number of Gangs
The amount of switches on the plate.
Connection
Between Discrete Points Allows the Flow of Electrons (Electric Current)
Control
A Mechanism that Controls the Operation of a Machine
Antenna
A Conductor or Set of Conductors Used to Radiate RF Energy Into Space or to Collect RF Energy from Space or to Do Both
Contact Configuration
Different Switching Functions of the Relay Contacts
Indoor/Outdoor
Enviromental Conditions rating on the product. Indoor Only, Outdoor, Both
Number of Ports
The Number of Application-Specific or Process-Specific Software Construct Serving as a Communication Endpoint / is Generally a Specific Place for Being Physically Connected to Some Other Device /A Number of Physical Access Point(S) Between a Conductor and
Timer Duration
Amount of Time a Timer can Last
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
Style
The Style / Descriptive Style / Common Name for the Shape, Coating and Material / Design / Designated Type of Construction / the Specific Function / the Type of Application / the Generic Type of the item
Number of Buttons
The Number of Keys/Switches in the item Used for Selecting a Particular Function
Number of Knockouts
How many knockouts are there in the product
Current Rating
Maximum Amount of Current a Cable can Carry Before Sustaining Damage or Deterioration
Number of Devices
The amount of devices the product can connect to.
Number of Ways
The Number of Connections the Unit can Provide
Number of USBs
Number of USB ports
Wall Plate Color
Color of the Plate that Covers a Switch on a Wall
Gauge
Indicates the specific thickness or diameter of wire or cable, which determines the amount of electrical current that can be safely carried.
Mounting Type
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
Lens Type
The type of lens that the adapter is fixing to.
Has Battery
A Device for Converting Chemical Energy Into Electrical Energy a Group of Two or More Connected Voltaic Cells
Knockout Size
Physical dimension of the knock-out size, could be diameter or a range
Wire Size
It is the Normal Size of the Conductors for Building Wire
Enclosure Type
Style, Type, Size, Etc. of the Enclosure of a Device
Data Transfer Rate
The Speed at Which Data is Transferred from one Location to Another with in the Time Frame
Power Supply
The Specification of the Electrical Power or the Description of This Electrical Power Which is Required for the Proper Functioning of the item
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
Encryption
The Activity of Converting Data or Information Into Code
Wattage
amount of watts used
Connection TypeTooltip Title
Style or Type of Connection Used
Product Family
Used to identify and differentiate offerings within a particular product line. Product families are typically treated as adjectives. It is not recommended to use the product line (ex: Wiremold®) and product family names (Evolution™) together. This will introduce a level of unnecessary confusion for the audience.
Lighting Types
Different forms of light a device is able to provide.
Protocol
A Convention or Standard that Controls or Enables the Connection, Communication, and Data Transfer Between Two Computing Endpoints, the Rules Governing the Syntax, Semantics, and Synchronization of Communication
Number of Types of Sources
To the Quantity and Type of Inputs for Instance, Hdmi, S-Video, Etc., Connections on a Device
Sensing Range
The total Possible Sensing Capability of the Sensor, Beginning After the Deadband, and Extending Out as Far as the Sensor is Able to Reach Effectively
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
Battery Life
Describes the approximate amount of time a battery can power a device before it needs to be recharged or replaced.
Security Method
Describes the functions or methods used by a device or software to protect against unauthorized access to a device or software platform.
On Function
Describes the mode of operation for devices that can be turned on, indicating whether they stay on continuously or operate on a timer or sensor.
Output Power
Refers to the amount of power a component, circuit, or system can deliver at the output to a load, measured in Watts.
Number of Connections
The number of connections a product is able to make to other devices.
Battery Capacity
Describes the maximum amount of electrical charge that a battery can store and deliver.
Engraving Type
Refers to the available styles to mark or inscribe text, symbols, or patterns on a product.
Seismic Tested
Indicates whether a device has been tested to withstand and/or perform under certain seismic conditions.
Sensor Coverage
Describes the total area, measured in square footage, within which a sensor can detect presence or movement.
Antenna Pattern
Captures the directional representation of how radio waves are sent and received by the antenna.
Sensitivity Adjustment
Refers to any customization settings, or range of adjustments for motion detection sensitivity, required to turn lights on.
Storage Temperature
Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.
Device Front Face Size
Describes the general proportions of a product's front face relative to the overall device.
Indicator
Describes the type/specification of signaling a device uses to indicate abnormal and/or operating conditions.
Antenna Gain
A calculated measure of how effectively an antenna sends or receives radio signals in a particular direction, measured in dBi (Decibals relative to isotropic).
Timer Type
The mechanism by which the timer operates, such as mechanical, digital, or programmable.
Antenna Type
Refers to the design or style of antenna used within a device, which can impact signal direction, range, and performance in wireless communication.
Dimming Compatibility
Describes the method(s) used by a device or system to adjust the brightness of a lighting load.
Max Distance Support
Refers to the maximum range a signal can be effectively supported to by a device.
Topology
The arrangement in which the Nodes of a LAN are connected to each other.
Wall Plate Included
Indicates if the device comes with a cover plate for aesthetic integration with the wall.
Works With
Need to ensure your choice works with your device, system, or software? Select your needs using this filter to confirm compatibility.
Sensor Coverage Pattern
Describes the shape of the area that a sensor is able to detect presence or movement within, measured in degrees.
Horsepower Rating
Refers to the power capacity of a device under normal load conditions, measured in horsepower (HP).
Current Draw
The amount of electrical current the device uses during operation, measured in amperes (or amps).
Configuration
Describes the specific arrangement and/or structure of a device's components.
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
A collection of related products that share a common design, technology, or purpose. Products within the series either maintain a cohesive brand / style identity or work together to serve a particular solution.
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Wireless Range
Describes the maximum distance wireless devices can be separated while preserving signal quality and reliability.
Enclosure Size
The approximate height of the compatible wiring enclosure.
Line Frequency
The frequency of alternating current (AC) in an electrical power system, measured in Hz. Also commonly referred to as Utility Frequency, Power Line Frequency, or Mains Frequency.
Maximum Humidity
The highest level of atmospheric moisture a device can withstand without compromising functionality or safety.
Sensor Technology
The technology used by a device to sense a change in signal or stimulus.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
Operating Temperature Max
Indicates the highest possible temperature a device can be safely used without the risk of failure or damage.
Network
Refers to the method a device connects to other devices within a closed system.
Operating System
Refers to the software platform used by a device to manage and control its functions, features, and compatibility with other systems.
Device Interface
Refers to the type and/or specification of connectors used by a device to establish a connection with other devices or systems for data transfer.
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
Control Algorithm
Refers to the set of rules or calculations a device utilizes to automate and regulate its use to optimize performance.
Bulb Compatibility
Indicates the type(s) of lighting a dimmer or controller is designed to work with, ensuring proper functionality and performance.
Device Backbody Size
Describes the general proportions of a product's backbody relative to the overall device.
Software Requirements
Captures any software or firmware needed to utilize and/or operate a device.
Outlet Type
Describes the unique qualities or characteristics of an electrical outlet that make it better suited to different uses. The listed qualities may give the outlet improved safety performance, increased efficiency, or additional functionality.
Number of Rockers
The total number of rocker-type electrical switches included on a device. Typically used to switch between two or more functions.
Sensor Mounting Height
Describes the optimal vertical distance at which a sensor should be installed to ensure reliable detection of motion or other target conditions.
Location Rating
Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.
Number of Relays
Denotes the number of controlled loads a device can support.
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
Our brands, products, resources, and pages are group into divisions. Filter and find a product, resource, or page you are looking for based on a Legrand category.
Resource Type
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
Brand
Choose from one of Legrand's brands.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsWattstopper PLUS System Support Unit, SilverEN-SSU-X WattstopperThe System Support Unit (SSU) is a key component in the Wattstopper PLUS Lighting Control System.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage Selections
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsPower over Ethernet (PoE) Injector, BlackTPE-113GI WattstopperThe Gigabit Power over Ethernet Injector
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage Selections
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsPS 30 Power Supply, GrayPS-30 WattstopperThe PS 30 power supply has an output voltage of 24 VDC and output current of 1.3 A
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage Selections
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDLM 5.7" Graphic Switch Touchscreen with LMPB-100, WhiteLMGS-150-PB-W WattstopperThe LMGS-150 graphic switch is a native DLM wired device with a 5.7" capacitive touch LCD display that enables simple control for complex spaces
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDaylighting Sensor, Handheld remote control for LS-301 setupLSR-301-S WattstopperThe LightSaver LS-301 is a closed loop, ceiling mount, low voltage indoor photosensor that works with standard, 0–10 VDC electronic dimming ballasts or compatible LED drivers to dim lighting as daylight increasesOther Options Available
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsLED Dimmer Bypass AdapterDIMBPASS Pass and SeymourAn LED dimming load adapter, install in wall box or at the fixture to reduce flicker and ghosting.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsLMDL-600 Plenum Recessed Mounting KitLMDL-600-RPM WattstopperThe LMDL-600 is a wireless open loop photo sensor that measures the daylight contribution in order to automatically switch or dim multiple zones of lighting.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsHardware and 1st Year Remote Support Warranty For LMJA-9300-XRACCESS-6 WattstopperConnected Services (RACCESS) is hardware, installed on a compatible lighting control system, that enables secure access for remote diagnostics and real-time technical support from the Legrand Remote Operations Center (ROC).
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsHardware and 1st Year Remote Support Warranty For LMJA-9125-XRACCESS-3 WattstopperConnected Services (RACCESS) is hardware, installed on a compatible lighting control system, that enables secure access for remote diagnostics and real-time technical support from the Legrand Remote Operations Center (ROC).
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDLM Wirless Integrated Fixture Sensor & ControllerLMFS-601-W WattstopperThe LMFS-601 is a wireless fixture sensor and controller that is compatible with wireless DLM.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDLM JACE 9000, Max 300 RoomsLMJA-9300-SM WattstopperThe LMJA-9300-SM is a Network ControllerOther Options Available
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsWattstopper PLUS DALI LS PD Sensor, Ceiling MountedDALISENS-LSPD-CIG2 WattstopperThe DALI LS PD is a compact light and presence sensor that is ceiling mounted or attached to a luminaire.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsWattstopper PLUS DALI LS PD Sensor, Fixture IntegratedDALISENS-LSPD-LIG2 WattstopperThe DALI LS PD is a compact light and presence sensor that is ceiling mounted or attached to a luminaire.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsWattstopper PLUS DALI 2 Presence Detector, 7m²DP-EBDSPIR-DALI2 WattstopperThe DP-EBDSPIR-DALI2 is a flush mounted, ceiling sensor.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsWattstopper PLUS DALI 2 Presence Detector, 15m²DP-EBDMR-DALI2 WattstopperThe DP-EBDMR-DALI2 is a mid-range, flush mounted, ceiling sensor.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsNetwork accessory enclosure 9 routers, 16 port switchesLMNC-9 WattstopperThe LMNC is a surface-mount NEMA1-rated enclosure with DIN rails for mounting DLM network components.Other Options Available
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsNEMA1-Rated Small Enclosure for DLM Network Controller/RaccessLMNC-ENC1 WattstopperThe LMNC-ENC1 is a surface-mount NEMA1-rated enclosure with a DIN rail for mounting one LMJA Network Controller with a removable cover.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsEquinox 41 LCD TouchscreenEQ41-LCAP WattstopperEquinox 41 is a high bright LCD touchscreen that is always on and always available.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsEquinox 73 LCD TouchscreenEQ73-LCAP WattstopperEquinox 73 is a high bright LCD touchscreen that is always on and always available.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsDLM Plug Load RF TransmitterWRC-TX-LM WattstopperWireless Receptacle Control products facilitate Auto-On/Auto-Off occupancy-based control of plug loads without the need to wire receptacles to power packs.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsWattstopper PLUS DALI-2 LS PD High-Bay LI Sensor, 18 m²DALI-2SEN-LSPD-HB-LI WattstopperThe DALI-2 LS PD HB LI Sensor utilizes Passive Infrared (PIR) and Photo sensors to provide occupancy and light information.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsWattstopper PLUS DALI-2 LS PD High-Bay CM Sensor, 21 m²DALI-2SEN-LSPD-HB-CM WattstopperThe DALI-2 LS PD HB CM Sensor provides occupancy information using passive infrared (PIR).
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsWattstopper PLUS DALI-2 LS PD C CI Sensor, 40 m²DALI-2SEN-LSPD-C-CI WattstopperThe DALI-2 LS PD C CI Sensor utilizes Passive Infrared (PIR) and Photo Sensors to provide occupancy and light information.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsWattstopper PLUS DALI-2 LS PD O CI Sensor, 12 m²DALI-2SEN-LSPD-O-CI WattstopperThe DALI-2 LS PD O CI Sensor utilizes Passive Infrared (PIR) and Photo Sensors to provide occupancy and light information
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsWattstopper PLUS DALI-2 LS PD Wide CM Sensor, 24 m²DALI-2SEN-LSPD-W-CM WattstopperThe DALI-2 LS PD W CM Sensor utilizes Passive Infrared (PIR) and Photo sensors to provide occupancy and light information.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsWattstopper PLUS HF LS LI Sensor, WhiteHF-LS-LI WattstopperThe DALI HF LS LI is a High-Frequency Light Sensing Luminaire Integrated Sensor and Coupler
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsWattstopper PLUS LS PD MULTI3 CI Sensor, 6 m²LSPD-MULTI-CI WattstopperThe DALI LS PD MULTI3 CI is a compact ceiling mounted sensor
Building on its commitment to the delivery and control of power and light without sacrificing inspired design, Legrand introduces the first-to-market in-wall Wireless Charger from the radiant® collection.
Read for a quick overview of how wireless charging works.
Read how blogger Carrie simplified charging by adding the radiant® Wireless Charger throughout her home.
See how the radiant wireless charger is the ultimate power charging station for your home.
Luxul is the leading innovator of simple-to-deploy professional grade IP networking solutions for use by custom installation professionals.
See how designer switches and outlets can add modern functionality without compromising your space’s charm.
Read for tips to get organized with a stylish DIY charging station that will meet your family’s mobile device needs.
Legrand North & Central America today announced the launch and immediate availability of a new wireless networking solution for the Wattstopper® Digital Lighting Management (DLM) platform that brings together greater levels of simplicity, scalability, and security that are unparalleled in the market.
Read how blogger Ashley introduced unique features and accents to makeover her kitchen.
Legrand, North America today announced that two Wattstopper products, the Lighting Control and Automation Panel (LCAP) architectural dimming platform and Wireless Receptacle Controls (WRC) series, were recognized as 2016 Product Innovation Award (PIA) winners
Legrand will be displaying its latest solutions in Human Centric Lighting (HCL), Digital Lighting Management (DLM), Architectural Dimming, and commercial shading from brands Wattstopper and Solarfective at LightShow West 2017.
To keep devices charged, Legrand offers an extensive range of USB power outlets for commercial and residential spaces, including outdoor areas.
San Jose, CA, September 15, 2016 – Consulting-Specifying Engineer Magazine Readers Award Wattstopper® with Two Product of the Year Awards.
Wattstopper Digital Lighting Management platform provides solutions that incorporate lighting controls technology to facilitate optimal energy performance to meet commercial building requirements.
An easy upgrade, USB Outlets from the adorne® and radiant® Collections install quickly and include a variety of features to perfectly fit your charging needs.
Legrand North & Central America today announced the availability of the Wattstopper Wireless DLM system. Wireless DLM builds upon the success of the original wired DLM system by extending its capabilities into IP-based wireless control.
Discover Nuvo whole home audio systems by Legrand to add the freedom of music anywhere in your home easily controlled from your mobile devices.
EC&M recognized the Wattstopper DLM Wireless system as a Product of the Year 2019 Category Winner in Lighting Control Systems.
Experience the dynamic audio of Nuvo's Player Portfolio and the convenience of voice control from Amazon Alexa.
Summer is almost over. Whether your student will be heading back to class in person or online, here are some tools to help foster success this fall.
LEGRAND FEATURES PREMIUM WIRELESS TABLETOP SPEAKER FOR NUVO PLAYER PORTFOLIO WHOLE HOME AUDIO SYSTEM AT CEDIA
Explore bathroom project ideas for every room to see how designer switches and outlets can elevate your space.
Explore bedroom project ideas for every room to see how designer switches and outlets can elevate your space.
Get that full battery feeling, faster, with these easy tips for superior mobile device charging.
NEW LEGRAND 42” PLASTIC ENCLOSURE EASILY INTEGRATES WIRELESS DEVICES INTO STRUCTURED WIRING INSTALLATIONS
See how designer switches and outlets can enhance your space with clutter-free wireless charging and dimming capability.
Select the right code version to specify wired or wireless digital lighting management solutions for code compliance within a specific space or room solution.
Visitors to Lightfair 2018 will be able to see a sneak peek of upcoming state-of-the art wireless lighting control solutions, touchscreen interface, and design tool for Wattstopper Digital Lighting Management (DLM), the industry’s most powerful and easy-to-use lighting controls platform from Legrand® North & Central America. These latest DLM solutions and capabilities are on display at LIGHTFAIR International 2018 at booth #1843.
Extended height WattStopper occupancy sensor allows more facilities to benefit from digital lighting control solutions
Legrand’s adorne and radiant with Netatmo solutions leverage leading technology to optimize Smart Lighting for whole home use