5
Browse 1,872 results for
"outlet"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Brand
Choose from one of Legrand's brands.
Product Family
Used to identify and differentiate offerings within a particular product line. Product families are typically treated as adjectives. It is not recommended to use the product line (ex: Wiremold®) and product family names (Evolution™) together. This will introduce a level of unnecessary confusion for the audience.
Product Series
A collection of related products that share a common design, technology, or purpose. Products within the series either maintain a cohesive brand / style identity or work together to serve a particular solution.
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Timer Type
The mechanism by which the timer operates, such as mechanical, digital, or programmable.
Outlet Type
Describes the unique qualities or characteristics of an electrical outlet that make it better suited to different uses. The listed qualities may give the outlet improved safety performance, increased efficiency, or additional functionality.
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
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
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
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
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
Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.
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
Describes the mode of operation for devices that can be turned on, indicating whether they stay on continuously or operate on a timer or sensor.
Lighting Types
Different forms of light a device is able to provide.
Service Capacity
Denotes the number of different services that can be used within a product as a result of separated internal compartments, including electrical, low voltage, water, air, and more.
Throw Type
Describes the method of switch operation, indicating whether it controls one circuit (single-throw) or switches between two circuits (double-throw).
Operating Temperature
The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit
Operating Temperature Max
Indicates the highest possible temperature a device can be safely used without the risk of failure or damage.
Storage Temperature
Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.
Is the Device Prewired?
Denotes whether a product comes prewired for quicker installation.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
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
Indicates whether a device is designed with a raised edge/rim, on or around its receptacle, for superior strength, handling, or attachment to another object.
Line Frequency
The frequency of alternating current (AC) in an electrical power system, measured in Hz. Also commonly referred to as Utility Frequency, Power Line Frequency, or Mains Frequency.
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
Describes the maximum electrical current the conductor or device can carry through its USB ports before sustaining immediate or progressive deterioration.
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
The total Possible Sensing Capability of the Sensor, Beginning After the Deadband, and Extending Out as Far as the Sensor is Able to Reach Effectively
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
A Convention or Standard that Controls or Enables the Connection, Communication, and Data Transfer Between Two Computing Endpoints, the Rules Governing the Syntax, Semantics, and Synchronization of Communication
Single/Multimode
Describes the mode of fiber either utilized or accepted by a device to transmit or receive a fiber optic signal.
Circular Outlet Diameter
Refers to the diameter of the circular opening in a wall plate, which should match the diameter of the outlet it is intended to cover.
Receptacle Spacing
Refers to the distance between power outlets or receptacles on a device, which can be important for planning the layout of plugs and connectors.
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
Refers to the distance from the surface level of a box to the area where internal devices are plugged in, illustrating the available space within to accommodate cords, receptacles, and large devices.
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
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
The Countertop Outlet follows NEC code updates to bring power to countertop settings in homes, bars, restaurants, hotels, lobbies, offices and beyond.
To keep devices charged, Legrand offers an extensive range of USB power outlets for commercial and residential spaces, including outdoor areas.
Elevate any space with the exceptional style and innovative functionality of designer outlets from the adorne and radiant Collections.
GFCI Outlet with USB offers charging ports and ground fault protection for kitchens, bathrooms and laundry rooms to easily see and reset electrical trips.
Looking to replace standard outlets with built-in USB charging ports? Here are our favorite spots to add one.
Upgrading kitchen outlets is a quick DIY project that makes a space easier to use and enjoy. Browse picks for kitchen island outlets, under-cab power and more.
Nightlights built into outlets make for easy children to see in the dark.
Upgraded outlets in the playroom with built-in nightlights perfect for kids.
An easy upgrade, USB Outlets from the adorne® and radiant® Collections install quickly and include a variety of features to perfectly fit your charging needs.
See how designer switches and outlets can provide power wherever you need it.
Read how blogger Leslie used Brushed Brass Wall Plates from the adorne® Collection to enhance her space.
A GFCI outlet is designed to protect individuals from electrical shock in wet or damp areas, such as bathrooms, kitchens, laundry rooms and exterior spaces.
Meet the first-of-its-kind GFCI USB Outlet. Power, safety, charging – put it all within reach, with this revolutionary device.
Meet the first-of-its-kind GFCI USB Outlet. Power, safety, charging – put it all within reach, with this revolutionary device.
Elevate any space with the exceptional style and innovative functionality of designer switches and outlets. Available in two distinct collections.
See how designer switches and outlets give access to three plugs simultaneously, then disappears back into the wall or counter
Unplug from ordinary with the adorne® Pop-Out™ Outlet. This clever solution hides your outlet until you need it. Simply push on the square face to "pop out" the outlets, then push the face back in for a smooth finish.
Complement the décor of your home with designer switches and outlets from the radiant Collection.
Whether for a simple style upgrade or to add modern features like USB charging, replacing outlets in your home is a quick DIY project with these easy steps.
Follow the step-by-step guide to install a USB outlet. From required tools to detailed instructions, you’ll find everything needed for safe installation.
See how adorne outlets can charge your devices while matching the aesthetic of your room.
“How awesome is that?!” Check out the awesome adorne® USB Outlet in this TV spot from 2018.
See how adorne magnesium GFCI outlets provide safety and style to this bathroom.
Watch this short how-to video to see how easy it is to install the adorne Dual USB, Plus Size Combo Outlet.
View white adorne Power Outlets placed on either side of the bed of The Gates Hotel South Beach guest room.
View an example of the adorne GFCI Outlet installed in the Quirk Hotel Richmond’s guest bathroom.
Get inspired for your next project. View our video gallery to see how designer switches and outlets from adorne® and radiant® can elevate any space.
View adorne power, lighting control and USB charging installed directly in the headboard at the Dream Hollywood.
Explore bathroom project ideas for every room to see how designer switches and outlets can elevate your space.
Read up on some common reasons, and resolutions, for electrical hiccups around the house.