5
Browse 2,275 results for
"outlet"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Brand
Choose from one of Legrand's brands.
Product Family
Used to identify and differentiate offerings within a particular product line. Product families are typically treated as adjectives. It is not recommended to use the product line (ex: Wiremold®) and product family names (Evolution™) together. This will introduce a level of unnecessary confusion for the audience.
Product Series
A collection of related products that share a common design, technology, or purpose. Products within the series either maintain a cohesive brand / style identity or work together to serve a particular solution.
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Timer Type
The mechanism by which the timer operates, such as mechanical, digital, or programmable.
Outlet Type
Describes the unique qualities or characteristics of an electrical outlet that make it better suited to different uses. The listed qualities may give the outlet improved safety performance, increased efficiency, or additional functionality.
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
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
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
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
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
Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.
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
Describes the mode of operation for devices that can be turned on, indicating whether they stay on continuously or operate on a timer or sensor.
Lighting Types
Different forms of light a device is able to provide.
Service Capacity
Denotes the number of different services that can be used within a product as a result of separated internal compartments, including electrical, low voltage, water, air, and more.
Throw Type
Describes the method of switch operation, indicating whether it controls one circuit (single-throw) or switches between two circuits (double-throw).
Operating Temperature
The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit
Operating Temperature Max
Indicates the highest possible temperature a device can be safely used without the risk of failure or damage.
Storage Temperature
Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.
Is the Device Prewired?
Denotes whether a product comes prewired for quicker installation.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
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
Indicates whether a device is designed with a raised edge/rim, on or around its receptacle, for superior strength, handling, or attachment to another object.
Line Frequency
The frequency of alternating current (AC) in an electrical power system, measured in Hz. Also commonly referred to as Utility Frequency, Power Line Frequency, or Mains Frequency.
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
Describes the maximum electrical current the conductor or device can carry through its USB ports before sustaining immediate or progressive deterioration.
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
The total Possible Sensing Capability of the Sensor, Beginning After the Deadband, and Extending Out as Far as the Sensor is Able to Reach Effectively
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
A Convention or Standard that Controls or Enables the Connection, Communication, and Data Transfer Between Two Computing Endpoints, the Rules Governing the Syntax, Semantics, and Synchronization of Communication
Single/Multimode
Describes the mode of fiber either utilized or accepted by a device to transmit or receive a fiber optic signal.
Circular Outlet Diameter
Refers to the diameter of the circular opening in a wall plate, which should match the diameter of the outlet it is intended to cover.
Receptacle Spacing
Refers to the distance between power outlets or receptacles on a device, which can be important for planning the layout of plugs and connectors.
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
Refers to the distance from the surface level of a box to the area where internal devices are plugged in, illustrating the available space within to accommodate cords, receptacles, and large devices.
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
Publishing Date Range
Date article, blog, or press release was published.
Filter by Product Category
Filter downloadable resources by the product category they relate or are relevant to.
Brand
Choose from one of Legrand's brands.
Resource Type
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
Read how blogger Ashley introduced unique features and accents to makeover her kitchen.
Read how blogger Carrie simplified charging by adding the radiant® Wireless Charger throughout her home.
Upgrading kitchen outlets is a quick DIY project that makes a space easier to use and enjoy. Browse picks for kitchen island outlets, under-cab power and more.
For students of all ages, here is our roundup of helpful gadgets to study hard and keep charged.
Paint and Plate Pairings to Make Yours Walls a Work of Art.
Check out our tips for upgrading your at-home workspace, featuring ways to maximize efficiency while including your own personal touch.
Looking to reduce your energy consumption in 2024? Upgrade your residential lighting with LED bulbs, monitor consumption and install dimming switches.
Match the latest decorative wall plates from the adorne Collection in Evergreen, Peachy, Rosa, Oatmeal and Mystic with popular interior design trends.
The adorne® Under-Cabinet Lighting and Power System uses an array of modular components that swap out so easily, you can reconfigure whenever the mood strikes.
Easily install the Smart Tru-Universal Dimmer from the radiant Collection.
Summer is almost over. Whether your student will be heading back to class in person or online, here are some tools to help foster success this fall.
Learn the differences between Thread and Wi-Fi when it comes to smart lighting and Matter-enabled devices for the home to determine the best solution.
Legrand’s solutions transform hotel spaces, from lobby to guest room and beyond. Browse options for power and charging, connectivity, smart control and more.
Legrand offers smart lighting solutions to fit every lifestyle, application or project.
GFCI protection is an important part of maintaining electrical safety within our homes. Learn more about how your GFCI outlets are keeping you safe from shock.
Watch this short video to learn how to configure your radiant Collection Smart Lighting in multiple locations.
Vantage Lighting Controls Combine With Stylish Push-Button and Toggle Switches for a Refined Smart Home Experience
View adorne Paddle Switches and Power/USB Outlets in the headboard of the Dream Hollywood’s guest beds.
Find innovation for commercial, residential and industrial electrical wiring. Explore Pass & Seymour switches, receptacles, GFCI outlets, USB chargers and more.
Spruce up the space you’ll be enjoying all summer, with these ideas for fantastic outdoor remodels and makeovers.
Designating a space for working out at home? Here are some tips for an optimal home gym setup.
Discover Legrand’s home builder technology solutions like smart lighting, USB charging outlets, wifi readiness, AV connectivity, home theater connections, etc.
Connect your smart light switches with other smart devices in your home, including Amazon Alexa or Google Home devices.
Bypass the adapter. Check out the convenient USB Outlet from the adorne® Collection.
Don’t skip the gadgets! See our checklist for getting your tech tidy this Spring Cleaning season!
Easily find your switch or dimmer in the dark, with a simple-to-install locator light. Watch to see how.
dash Furniture Power Center adds configurable and convenient access to power directly to furniture. configure power, data, and switching cubes.
A variety of furniture power centers, configurable power solutions, smart switches, and lighting controls for hotel rooms and furniture. Learn More.
An easy upgrade, USB Outlets from the adorne® and radiant® Collections install quickly and include a variety of features to perfectly fit your charging needs.
Get prepped and ready for the season of visitors and overnight guests, with these tips for holiday hosting.