5
Browse 185 results for
"timer switch"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Brand
Choose from one of Legrand's brands.
Frequency Band
A Continuous Group, or Range, of Frequencies with an Upper Limit and a Lower Limit
Sensor Type
The Device that Receives a Signal or Stimulus (As Heat or Pressure or Light or Motion Etc.) and Responds to it in a Distinctive Manner
Amperage
Maximum electrical current the conductor or device can carry before sustaining immediate or progressive deterioration
Installation Location
Where a Device is or is to be Installed
Load
The Maximum Amount of Power Which the item can withstand or Operate without any performance Loss
NEMA Rating
National Electrical Manufacturers Association Ratings are Standards that are Useful in Defining the Types of Environments in Which an Electrical Enclosure can be Used
Contact Rating
The Voltage, Current, and Power Capacities of Relay Contacts Under Specified Environmental Conditions
Availability
Product is available to buy on Legrand.us
Compatibility
Capability of Being Used with or Connected to Different Types of Devices or Components without any Modifications
Product Certifications
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
Number of Gangs
The amount of switches on the plate.
Connection
Between Discrete Points Allows the Flow of Electrons (Electric Current)
Frequency Rating
The Number of Occurrences within a Given Time Period, the Rate at Which Alternating Current Makes a Complete Cycle of Reversals
Indoor/Outdoor
Enviromental Conditions rating on the product. Indoor Only, Outdoor, Both
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Input Voltage
The Difference of Electrical Potential Between Two Points of an Electrical or Electronic Circuit Entering a System
Timing Range
The Time Span for Which the System/Device is in Desired Active/Working Mode
Load Type
Denotes the type(s) of load that can be applied to a dimmer, which determines its compatible light sources.
Mounting Type
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
Number of Buttons
The Number of Keys/Switches in the item Used for Selecting a Particular Function
Sensitivity
The Minimum Input Which the Device can Sense and Produce the Output
Has Battery
A Device for Converting Chemical Energy Into Electrical Energy a Group of Two or More Connected Voltaic Cells
Response Frequency
Frequency response is the quantitative measure of the output spectrum of a system or device in response to a stimulus, and is used to characterize the dynamics of the system. It is a measure of magnitude and phase of the output as a function of frequency, in comparison to the input.
Wire Size
It is the Normal Size of the Conductors for Building Wire
Product Family
Filter to specific families of related products that share common characteristics, designs, or functions.
Load Rating
The maximum load that a device is designed to withstand without breakage or loss of performance.
Wattage
amount of watts used
Connection TypeTooltip Title
Style or Type of Connection Used
Target Size
The Dimensional Specification of the Object Which is Set as a Target for the Sensor
Sensing Range
The total Possible Sensing Capability of the Sensor, Beginning After the Deadband, and Extending Out as Far as the Sensor is Able to Reach Effectively
Number of Switches
Number of electrical switches
Voltage
The Rate at Which Energy is Drawn from a Source that Produces a Flow of Electricity in a Circuit
Operating Temperature
The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit
Included
The Supplementary items Supplied with the Product Which May be Necessary for the Optimum Operation of the Product
Product Has Potential to Contribute to LEED
This product contributes to earning credits in the LEED rating system.
Wire Connection Type
Describes the method used to connect wires to the device, such as screw terminals, push-in connectors, or lead wires.
Preset
Denotes whether a dimmer returns lights to their previously-selected light level when turned on.
Operating Temperature Min
Indicates the lowest possible temperature a device can be safely used without the risk of failure or damage.
On Function
Describes the mode of operation for devices that can be turned on, indicating whether they stay on continuously or operate on a timer or sensor.
Engraving Type
Refers to the available styles to mark or inscribe text, symbols, or patterns on a product.
Seismic Tested
Indicates whether a device has been tested to withstand and/or perform under certain seismic conditions.
Sensor Coverage
Describes the total area, measured in square footage, within which a sensor can detect presence or movement.
Standard
The industrial standard(s) to which a device is manufactured, operated, or tested.
Sensitivity Adjustment
Refers to any customization settings, or range of adjustments for motion detection sensitivity, required to turn lights on.
Storage Temperature
Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.
Device Front Face Size
Describes the general proportions of a product's front face relative to the overall device.
Indicator
Describes the type/specification of signaling a device uses to indicate abnormal and/or operating conditions.
Timer Type
The mechanism by which the timer operates, such as mechanical, digital, or programmable.
Dimming Compatibility
Describes the method(s) used by a device or system to adjust the brightness of a lighting load.
Application Sector
Refers to the expected environment(s) or intended usage(s) for a product (e.g. Residential, Commercial, Industrial, etc.).
Trim/Adjustment Level
A control feature that allows the adjustment of the minimum and maximum light levels to prevent issues such as flickering at lower brightness levels, ensuring smooth and stable dimming performance.
Topology
The arrangement in which the Nodes of a LAN are connected to each other.
Wall Plate Included
Indicates if the device comes with a cover plate for aesthetic integration with the wall.
Works With
Need to ensure your choice works with your device, system, or software? Select your needs using this filter to confirm compatibility.
Sensor Coverage Pattern
Describes the shape of the area that a sensor is able to detect presence or movement within, measured in degrees.
Horsepower Rating
Refers to the power capacity of a device under normal load conditions, measured in horsepower (HP).
Current Draw
The amount of electrical current the device uses during operation, measured in amperes (or amps).
Requires Neutral Wire
Indicates whether a device requires a neutral wire to function properly.
Operating Humidity
Describes the range of humidity at which a device can be utilized safely without the risk of failure or damage.
Connection Location
Specifies where on the device the electrical connections are made, which can affect installation.
Product Series
A collection of related products that share a common design, technology, or purpose. Products within the series either maintain a cohesive brand / style identity or work together to serve a particular solution.
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Throw Type
Describes the method of switch operation, indicating whether it controls one circuit (single-throw) or switches between two circuits (double-throw).
Line Frequency
The frequency of alternating current (AC) in an electrical power system, measured in Hz. Also commonly referred to as Utility Frequency, Power Line Frequency, or Mains Frequency.
Maximum Humidity
The highest level of atmospheric moisture a device can withstand without compromising functionality or safety.
Features
Unique characteristics and functionality that set the product apart from others in its field.
Sensor Technology
The technology used by a device to sense a change in signal or stimulus.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
Operating Temperature Max
Indicates the highest possible temperature a device can be safely used without the risk of failure or damage.
Warranty Type
The product warranty that accompanies the specific product.
Terminal Accommodation
Describes the type and size of wire that the receptacle's terminals can securely hold (typically provided as a range in gauge size).
Electrical Rating
The maximum load or capacity of electrical power a dimmer switch is rated to manage when linked to a specific type of light bulb.
Environmental Conditions
Describes the relative range of climatic standards a device can safely operate within.
Finish
Describes the specific surface treatment applied to the outer product for either aesthetics and/or durability.
Product Length
The overall length of a product.
Ultrasonic Frequency
Describes the specific frequency at which a sensor emits and detects sound waves in order to measure distances, detect objects, or perform other functions.
Bulb Compatibility
Indicates the type(s) of lighting a dimmer or controller is designed to work with, ensuring proper functionality and performance.
Light Level Adjustment
Captures the range over which a device can adjust the intensity of light in order to maintain the desired ambient light setpoint, enhancing comfort and energy savings.
Device Backbody Size
Describes the general proportions of a product's backbody relative to the overall device.
Number of Rockers
The total number of rocker-type electrical switches included on a device. Typically used to switch between two or more functions.
Sensor Mounting Height
Describes the optimal vertical distance at which a sensor should be installed to ensure reliable detection of motion or other target conditions.
Location Rating
Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.
Material
Indicates the primary material(s) used to construct a product.
Filter to Specific Product Groups
Filter by named groups of related products, including product families, series, systems, and solutions. Groupings may indicate similar styles of products, or signify how they're designed to operate together as a complete solution.
Stock Level
Filter your results to only in-stock products sold directly on legrand.us.
Brand
Choose from one of Legrand's brands.
Category
Our brands, products, resources, and pages are group into divisions. Filter and find a product, resource, or page you are looking for based on a Legrand category.
Filter by Product Category
Filter downloadable resources by the product category they relate or are relevant to.
Brand
Choose from one of Legrand's brands.
Resource Type
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
Light switch timers and occupancy/vacancy sensors offer automated control for convenience and energy savings in the home while allowing for precise lighting control.
radiant switch and timer switch for automatic and manual lighting control.
Less waste, less worry, with timed lighting control from the radiant® Collection. Never accidentally leave the lights again.
Elevate any space with the innovative functionality of hands-free touchless light switches and dimmers from the adorne and radiant Collections.
View wallbox devices that are compatible with your commercial lighting controls system. Wattstopper offers dimmers, timers, switches, and more.
View wallbox devices that are compatible with your commercial lighting controls system. Wattstopper offers dimmers, timers, switches, and more.
Are you familiar with the different types of light switches for the home? Read our guide on the types and best use cases for your lighting control.
Wattstopper offers simple, scalable and flexible, energy-efficient networked lighting controls and solutions for commercial applications. Browse lighting control products and solutions for spaces where occupants learn, work, and heal.
Leagrand puts stylish design and modern conveniences at homeowners’ fingertips with affordable switches, outlets and home automation controls.
Elevate any space with the exceptional style and innovative functionality of designer switches from the adorne and radiant Collections.
Dive deeper into Legrand's switches and dimmers. Learn about functionality, dimmer & switch types, installation guidance, safety, colors, designs and more!
Explore bedroom project ideas for every room to see how designer switches and outlets can elevate your space.
From standard LED dimming to stylish smart lighting, Legrand offers a full spectrum of residential lighting and fan controls to meet any home’s needs.
Perfect for any kitchen and bathroom upgrade, touchless options for lighting control, sink faucets and more can add convenience while reducing mess.
See how designer switches and outlets can elevate bedrooms and master suites, with our photo gallery.
Get inspired for your next project. See how designer switches and outlets can elevate any space, with our photo gallery.
The easy-to-install smart lighting system is here. In just a few simple steps, replace existing switches with smart switches and dimmers.
Check out our tips for upgrading your at-home workspace, featuring ways to maximize efficiency while including your own personal touch.
Designating a space for working out at home? Here are some tips for an optimal home gym setup.
Enhance resilient design through access to backup power and reduce light pollution.
Wattstopper lighting control products are designed to meet code, ensure ease of installation, and enable the control of light. Learn more.
Pennsylvania is adopting a new energy conservation code effective Oct. 1, 2018 through an update of the Pennsylvania Uniform Construction Code (UCC). The 2015 IECC will be the new building efficiency standard statewide except for in the city of Philadelphia, which is adopting the newer 2018 IECC standard.
Legrand announces that three of its Wattstopper products have been accepted into the 2017 IES (Illuminating Engineering Society) Progress report which seeks to highlight developments in the art and science of lighting throughout the world.
In the midst of the pandemic, commercial spaces, offices in particular, have been greatly impacted by social distancing requirements. As we look to our future return to the workplace, adjusting to new health and safety restrictions will require innovative solutions to keep employees safe.
LFI 2016: Legrand Showcases Code Compliant Control Solutions for Indoor and Outdoor LED Luminaires
What color options are available? Charging stations are available in black, bronze and silver, as well as custom colors. We can also add custom logos to the pedestal if desired. Can the station be used indoors or only outdoors? Technically, you could use the charging station indoors assuming you sink the L bolts into concrete. However, it is designed to offer maximum durability and to align with the UL requirements for outdoor use.
With good planning and the use of energy monitoring and home automation technologies, we can all do our part to reduce the flow of energy consumption.
Visitors to Lightfair 2018 will be able to see a sneak peek of upcoming state-of-the art wireless lighting control solutions, touchscreen interface, and design tool for Wattstopper Digital Lighting Management (DLM), the industry’s most powerful and easy-to-use lighting controls platform from Legrand® North & Central America. These latest DLM solutions and capabilities are on display at LIGHTFAIR International 2018 at booth #1843.