5
Browse 1,878 results for
"outlet"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Brand
Choose from one of Legrand's brands.
Product Family
Used to identify and differentiate offerings within a particular product line. Product families are typically treated as adjectives. It is not recommended to use the product line (ex: Wiremold®) and product family names (Evolution™) together. This will introduce a level of unnecessary confusion for the audience.
Product Series
A collection of related products that share a common design, technology, or purpose. Products within the series either maintain a cohesive brand / style identity or work together to serve a particular solution.
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Timer Type
The mechanism by which the timer operates, such as mechanical, digital, or programmable.
Outlet Type
Describes the unique qualities or characteristics of an electrical outlet that make it better suited to different uses. The listed qualities may give the outlet improved safety performance, increased efficiency, or additional functionality.
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
Floor Type
Floor construction product is designed to work in
Wall Plate Type
Refers to the style or intended usage of a wall plate.
Connector Style
The design or type of the connector used to join electrical circuits together.
Connector Type
The Type of Connectors / Terminals that Tool can Crimp to Wire or Cable
Product Certifications
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
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
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
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
Sensor Technology
The technology used by a device to sense a change in signal or stimulus.
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
Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.
Compatibility
Capability of Being Used with or Connected to Different Types of Devices or Components without any Modifications
Works With
Need to ensure your choice works with your device, system, or software? Select your needs using this filter to confirm compatibility.
Bulb Compatibility
Indicates the type(s) of lighting a dimmer or controller is designed to work with, ensuring proper functionality and performance.
On Function
Describes the mode of operation for devices that can be turned on, indicating whether they stay on continuously or operate on a timer or sensor.
Lighting Types
Different forms of light a device is able to provide.
Service Capacity
Denotes the number of different services that can be used within a product as a result of separated internal compartments, including electrical, low voltage, water, air, and more.
Throw Type
Describes the method of switch operation, indicating whether it controls one circuit (single-throw) or switches between two circuits (double-throw).
Operating Temperature
The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit
Operating Temperature Max
Indicates the highest possible temperature a device can be safely used without the risk of failure or damage.
Storage Temperature
Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.
Is the Device Prewired?
Denotes whether a product comes prewired for quicker installation.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
Number of Wires
The Number of Pliable Metallic Strand or Rod Made in Many Lengths and Diameters and are Electrically Insulated, Used Conduct Electricity
Wire Connection Type
Describes the method used to connect wires to the device, such as screw terminals, push-in connectors, or lead wires.
Timing Range
The Time Span for Which the System/Device is in Desired Active/Working Mode
Connection TypeTooltip Title
Style or Type of Connection Used
Flanged
Indicates whether a device is designed with a raised edge/rim, on or around its receptacle, for superior strength, handling, or attachment to another object.
Line Frequency
The frequency of alternating current (AC) in an electrical power system, measured in Hz. Also commonly referred to as Utility Frequency, Power Line Frequency, or Mains Frequency.
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
Describes the maximum electrical current the conductor or device can carry through its USB ports before sustaining immediate or progressive deterioration.
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
Number of Channels
The Number of Media Used to Convey Information
Number of Conductors
The Number of Materials/Strands/Pairs Which Contain Movable Electric Charges
Contact Configuration
Different Switching Functions of the Relay Contacts
Contact Rating
The Voltage, Current, and Power Capacities of Relay Contacts Under Specified Environmental Conditions
Sensing Range
The total Possible Sensing Capability of the Sensor, Beginning After the Deadband, and Extending Out as Far as the Sensor is Able to Reach Effectively
Sensor Coverage
Describes the total area, measured in square footage, within which a sensor can detect presence or movement.
Sensor Coverage Pattern
Describes the shape of the area that a sensor is able to detect presence or movement within, measured in degrees.
Wireless Range
Describes the maximum distance wireless devices can be separated while preserving signal quality and reliability.
Protocol
A Convention or Standard that Controls or Enables the Connection, Communication, and Data Transfer Between Two Computing Endpoints, the Rules Governing the Syntax, Semantics, and Synchronization of Communication
Single/Multimode
Describes the mode of fiber either utilized or accepted by a device to transmit or receive a fiber optic signal.
Circular Outlet Diameter
Refers to the diameter of the circular opening in a wall plate, which should match the diameter of the outlet it is intended to cover.
Receptacle Spacing
Refers to the distance between power outlets or receptacles on a device, which can be important for planning the layout of plugs and connectors.
Box Depth
The measurement from the front opening to the back of an electrical box, indicating the volume of wiring it can contain.
Knockout Size
Physical dimension of the knock-out size, could be diameter or a range
Core Hole Size
Physical Dimensions of the hole
Internal Depth
Refers to the distance from the surface level of a box to the area where internal devices are plugged in, illustrating the available space within to accommodate cords, receptacles, and large devices.
Thickness
The Dimension Through an Object as Opposed to its Length or Width
Wall Plate Size
The general size of the the included wall plate. The size may determine whether it suits your personal application!
Cable Length
The Longest Dimension of Insulated Conductors
Cord Length
The Linear Extent of Cord in Space from one End to the Other
Wire Gauge
Measuring and Indicating a Quantity of Wire
Number of Gangs
The amount of switches on the plate.
Number of Buttons
The Number of Keys/Switches in the item Used for Selecting a Particular Function
Number of Switches
Number of electrical switches
Number of Outlets
The Different Types of Receptacles Providing a Place in a Wiring System Where Current can be Taken to Supply Electrical Devices
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
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
The Countertop Outlet follows NEC code updates to bring power to countertop settings in homes, bars, restaurants, hotels, lobbies, offices and beyond.
To keep devices charged, Legrand offers an extensive range of USB power outlets for commercial and residential spaces, including outdoor areas.
Elevate any space with the exceptional style and innovative functionality of designer outlets from the adorne and radiant Collections.
GFCI Outlet with USB offers charging ports and ground fault protection for kitchens, bathrooms and laundry rooms to easily see and reset electrical trips.
Looking to replace standard outlets with built-in USB charging ports? Here are our favorite spots to add one.
Upgrading kitchen outlets is a quick DIY project that makes a space easier to use and enjoy. Browse picks for kitchen island outlets, under-cab power and more.
Upgraded outlets in the playroom with built-in nightlights perfect for kids.
See how designer switches and outlets can provide power wherever you need it.
A GFCI outlet is designed to protect individuals from electrical shock in wet or damp areas, such as bathrooms, kitchens, laundry rooms and exterior spaces.
Meet the first-of-its-kind GFCI USB Outlet. Power, safety, charging – put it all within reach, with this revolutionary device.
Elevate any space with the exceptional style and innovative functionality of designer switches and outlets. Available in two distinct collections.
Nightlights built into outlets make for easy children to see in the dark.
An easy upgrade, USB Outlets from the adorne® and radiant® Collections install quickly and include a variety of features to perfectly fit your charging needs.
Read how blogger Leslie used Brushed Brass Wall Plates from the adorne® Collection to enhance her space.
Meet the first-of-its-kind GFCI USB Outlet. Power, safety, charging – put it all within reach, with this revolutionary device.
Whether for a simple style upgrade or to add modern features like USB charging, replacing outlets in your home is a quick DIY project with these easy steps.
Unplug from ordinary with the adorne® Pop-Out™ Outlet. This clever solution hides your outlet until you need it. Simply push on the square face to "pop out" the outlets, then push the face back in for a smooth finish.
Complement the décor of your home with designer switches and outlets from the radiant Collection.
Follow the step-by-step guide to install a USB outlet. From required tools to detailed instructions, you’ll find everything needed for safe installation.
“How awesome is that?!” Check out the awesome adorne® USB Outlet in this TV spot from 2018.
See how designer switches and outlets give access to three plugs simultaneously, then disappears back into the wall or counter
See how adorne magnesium GFCI outlets provide safety and style to this bathroom.
See how adorne outlets can charge your devices while matching the aesthetic of your room.
Explore bathroom project ideas for every room to see how designer switches and outlets can elevate your space.
Read up on some common reasons, and resolutions, for electrical hiccups around the house.
Meet the solution for those hard-to-reach outlets behind your furniture. With a few household tools & 30 minutes, this DIY kit lets you move your power access.
Explore bedroom project ideas for every room to see how designer switches and outlets can elevate your space.
Designer switches and outlets are the perfect finishing touch. Explore options for elevating your property and enhancing the guest experience.
View an example of the adorne GFCI Outlet installed in the Quirk Hotel Richmond’s guest bathroom.
GFCI protection is an important part of maintaining electrical safety within our homes. Learn more about how your GFCI outlets are keeping you safe from shock.