5
Browse 218 results for
"Wattstopper PLUS"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Brand
Choose from one of Legrand's brands.
Product Type
Select a Product Type to find products that share the same basic form and function, such as switches, cables, panels, or electrical boxes.
Number of Receptacles
The Number of Electrical Wall Outlets Designed for Use with a Plug
Frequency Band
A Continuous Group, or Range, of Frequencies with an Upper Limit and a Lower Limit
Sensor Type
The Device that Receives a Signal or Stimulus (As Heat or Pressure or Light or Motion Etc.) and Responds to it in a Distinctive Manner
Amperage
Maximum electrical current the conductor or device can carry before sustaining immediate or progressive deterioration
Installation Location
Where a Device is or is to be Installed
Connector Type
The Type of Connectors / Terminals that Tool can Crimp to Wire or Cable
Contact Rating
The Voltage, Current, and Power Capacities of Relay Contacts Under Specified Environmental Conditions
Compatibility
Capability of Being Used with or Connected to Different Types of Devices or Components without any Modifications
Product Certifications
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
Is Tamper-Resistant
Tamper resistance is resistance to tampering (intentional malfunction or sabotage) by either the normal users of a product, package, or system or others with physical access to it.
Number of Gangs
The amount of switches on the plate.
Connector
Refers to the specific types of connections a device uses to join electrical conductors and create an electrical circuit. When you select the first desired connector, a second filter will appear listing any connectors on the opposite end of your selected connector on a device.
Antenna
A Conductor or Set of Conductors Used to Radiate RF Energy Into Space or to Collect RF Energy from Space or to Do Both
Is Weather Resistant
Is this product listed as Weather Resistant ?
Contact Configuration
Different Switching Functions of the Relay Contacts
Indoor/Outdoor
Enviromental Conditions rating on the product. Indoor Only, Outdoor, Both
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Timer Duration
Amount of Time a Timer can Last
Input Voltage
The Difference of Electrical Potential Between Two Points of an Electrical or Electronic Circuit Entering a System
Load Type
Denotes the type(s) of load that can be applied to a dimmer, which determines its compatible light sources.
Output Voltage
The Voltage Measured at the Output Terminals of a Power Supply
Mounting Type
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
Number of Buttons
The Number of Keys/Switches in the item Used for Selecting a Particular Function
Number of USBs
Number of USB ports
Lens Type
The type of lens that the adapter is fixing to.
Has Battery
A Device for Converting Chemical Energy Into Electrical Energy a Group of Two or More Connected Voltaic Cells
Data Transfer Rate
The Speed at Which Data is Transferred from one Location to Another with in the Time Frame
Shielded/Unshielded
Denotes whether a cable is designed with an extra layer of metal foil or braid surrounding the inner conductor to protect against electromagnetic interference (EMI).
Power Supply
The Specification of the Electrical Power or the Description of This Electrical Power Which is Required for the Proper Functioning of the item
Wire Gauge
Measuring and Indicating a Quantity of Wire
Load Rating
The maximum load that a device is designed to withstand without breakage or loss of performance.
Battery
A Device for Converting Chemical Energy Into Electrical Energy a Group of Two or More Connected Voltaic Cells
Encryption
The Activity of Converting Data or Information Into Code
Cable Length
The Longest Dimension of Insulated Conductors
Color
The color of the product itself
Sensing Range
The total Possible Sensing Capability of the Sensor, Beginning After the Deadband, and Extending Out as Far as the Sensor is Able to Reach Effectively
Power Consumption
Number of Switches
Number of electrical switches
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
Wire Connection Type
Describes the method used to connect wires to the device, such as screw terminals, push-in connectors, or lead wires.
Operating Temperature Min
Indicates the lowest possible temperature a device can be safely used without the risk of failure or damage.
Battery Life
Describes the approximate amount of time a battery can power a device before it needs to be recharged or replaced.
Security Method
Describes the functions or methods used by a device or software to protect against unauthorized access to a device or software platform.
On Function
Describes the mode of operation for devices that can be turned on, indicating whether they stay on continuously or operate on a timer or sensor.
Number of Connections
The number of connections a product is able to make to other devices.
Battery Capacity
Describes the maximum amount of electrical charge that a battery can store and deliver.
Engraving Type
Refers to the available styles to mark or inscribe text, symbols, or patterns on a product.
Connector Hood Material
The material used for the protective covering or outer casing of a connector.
Sensor Coverage
Describes the total area, measured in square footage, within which a sensor can detect presence or movement.
Antenna Pattern
Captures the directional representation of how radio waves are sent and received by the antenna.
Standard
The industrial standard(s) to which a device is manufactured, operated, or tested.
Sensitivity Adjustment
Refers to any customization settings, or range of adjustments for motion detection sensitivity, required to turn lights on.
Storage Temperature
Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.
Indicator
Describes the type/specification of signaling a device uses to indicate abnormal and/or operating conditions.
Antenna Gain
A calculated measure of how effectively an antenna sends or receives radio signals in a particular direction, measured in dBi (Decibals relative to isotropic).
Termination Style
The style of connection used for electrical termination between two devices.
Timer Type
The mechanism by which the timer operates, such as mechanical, digital, or programmable.
Antenna Type
Refers to the design or style of antenna used within a device, which can impact signal direction, range, and performance in wireless communication.
Dimming Compatibility
Describes the method(s) used by a device or system to adjust the brightness of a lighting load.
Bus Power Supply
Refers to the electrical power provided to a device through a common communication bus.
Max Distance Support
Refers to the maximum range a signal can be effectively supported to by a device.
Application Sector
Refers to the expected environment(s) or intended usage(s) for a product (e.g. Residential, Commercial, Industrial, etc.).
Product Depth
The overall depth of a product.
Topology
The arrangement in which the Nodes of a LAN are connected to each other.
Wall Plate Included
Indicates if the device comes with a cover plate for aesthetic integration with the wall.
Sensor Coverage Pattern
Describes the shape of the area that a sensor is able to detect presence or movement within, measured in degrees.
Horsepower Rating
Refers to the power capacity of a device under normal load conditions, measured in horsepower (HP).
Current Draw
The amount of electrical current the device uses during operation, measured in amperes (or amps).
Operating Humidity
Describes the range of humidity at which a device can be utilized safely without the risk of failure or damage.
Connection Location
Specifies where on the device the electrical connections are made, which can affect installation.
Jacket Application
Describes the specific application(s) a cable's jacket is designed to be used in, such as in-wall, plenum, or riser.
Jacket Color
Describes the color used on the outer covering of a cord or cable; often used as a way to easily identify different cables or signal types in networking setups.
Product Height
The overall height of a product.
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Wireless Range
Describes the maximum distance wireless devices can be separated while preserving signal quality and reliability.
Throw Type
Describes the method of switch operation, indicating whether it controls one circuit (single-throw) or switches between two circuits (double-throw).
Line Frequency
The frequency of alternating current (AC) in an electrical power system, measured in Hz. Also commonly referred to as Utility Frequency, Power Line Frequency, or Mains Frequency.
Conductor
Describes the number and configuration of electrical wires used within a cable to transmit signals.
Features
Unique characteristics and functionality that set the product apart from others in its field.
Bend Radius
The minimum radius a cable, cord, or wire can bend without kinking it, damaging it, or shortening its life.
Sensor Technology
The technology used by a device to sense a change in signal or stimulus.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
Operating Temperature Max
Indicates the highest possible temperature a device can be safely used without the risk of failure or damage.
Warranty Type
The product warranty that accompanies the specific product.
Device Interface
Refers to the type and/or specification of connectors used by a device to establish a connection with other devices or systems for data transfer.
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
Light Level Adjustment
Captures the range over which a device can adjust the intensity of light in order to maintain the desired ambient light setpoint, enhancing comfort and energy savings.
Jacket Rating
Denotes the NEC (National Electric Code) standards the outer casing/jacket surrounding a cable or cord's internal wiring and insulation is rated to.
Outlet Type
Describes the unique qualities or characteristics of an electrical outlet that make it better suited to different uses. The listed qualities may give the outlet improved safety performance, increased efficiency, or additional functionality.
Number of Rockers
The total number of rocker-type electrical switches included on a device. Typically used to switch between two or more functions.
Sensor Mounting Height
Describes the optimal vertical distance at which a sensor should be installed to ensure reliable detection of motion or other target conditions.
Location Rating
Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.
Number of Relays
Denotes the number of controlled loads a device can support.
Material
Indicates the primary material(s) used to construct a product.
Cable Diameter
The typical outer diameter of a cable.
Filter to Specific Product Groups
Filter by named groups of related products, including product families, series, systems, and solutions. Groupings may indicate similar styles of products, or signify how they're designed to operate together as a complete solution.
Stock Level
Filter your results to only in-stock products sold directly on legrand.us.
Publishing Date Range
Date article, blog, or press release was published.
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
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
Learn about how to submit a Wattstopper RMA. Our process has improved thanks to customer feedback!
Legrand, a global leader in electrical and digital building infrastructures, is announcing the rebranding of Encelium technology to Wattstopper PLUS.
Legrand®, a global leader in electrical and digital building infrastructures has announced a new integration between its Wattstopper® lighting control systems and Mecho® motorized and automated shades. This collaboration creates a streamlined approach for building owners, designers, and integrators to combine advanced lighting and shading solutions, driving greater energy efficiency, comfort, and occupant control.
Legrand®, a global leader in electrical and digital building infrastructures has announced a new integration between its Wattstopper® lighting control systems and Mecho® motorized and automated shades. This collaboration creates a streamlined approach for building owners, designers, and integrators to combine advanced lighting and shading solutions, driving greater energy efficiency, comfort, and occupant control.
Legrand’s i3 Platform integrates with Wattstopper PLUS, and DLM to helps users monitor, analyze, and manage smart building data in real-time.
Find comprehensive Wattstopper lighting resources and support here. Explore user guides, installation instructions, CAD Drawings, and more to optimize your Wattstopper lighting controls.
Innovative WattStopper hi/low sensor for outdoor LED fixtures wins top honors in Consulting-Specifying Engineer reader survey
Access all the specification tools and resources you need for your next project.
Easily manage, adjust, and optimize your lighting control system with Wattstopper’s Lighting Control System Services broad portfolio of support. Learn more now.
Simplify the complex functionality of lighting control systems with Wattstopper scalable and flexible energy efficient lighting controls. Explore now.
Legrand, North & Central America announced the launch of Wattstopper Technology-Enabled Service Contracts, a new offering that brings added convenience and protection to lighting control system investments.
Legrand unveils Wattstopper i3, a groundbreaking smart building management platform powered by KODE Labs. Discover seamless control, intelligent automation, and future-ready integration.
Wattstopper® in-fixture lighting controls integrate occupancy sensing, daylight-responsive control and lighting control functionality directly into compatible commercial luminaires.
Wattstopper partners with Genlyte Solutions to deliver integrated outdoor lighting controls using the FSP‑600 Fixture Sensor Photocell and Gardco luminaires.
Wattstopper FSP-600 Series, a next-generation wireless in-fixture lighting control solution. Featuring 0–10V dimming with integrated motion sensing, daylight harvesting, and wireless networking, the FSP-600 delivers flexible, scalable control for a wide range of applications.
Legrand’s products and systems touch nearly every part of the building environment. Find your business solution from Legrand today!
Discover our solutions designed to help you meet the diverse needs of everyone in your healthcare facility.
Features Simplified Setup and Diagnostics Via Touch Screen Display and Delivers Highest Quality Audio to Three Zones Simultaneously with 110-Watts of Power
AT ISE, LEGRAND FEATURES NUVO P4300, NEW MULTI-ZONE, RACK-MOUNT PLAYER FOR PLAYER PORTFOLIO MUSIC SYSTEM
Have a question? Want to get in contact with a Legrand customer service representative? Email or contact our customer support desk. Contact us today!