5
Browse 215 results for
"Wattstopper PLUS"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Brand
Choose from one of Legrand's brands.
Product Family
Used to identify and differentiate offerings within a particular product line. Product families are typically treated as adjectives. It is not recommended to use the product line (ex: Wiremold®) and product family names (Evolution™) together. This will introduce a level of unnecessary confusion for the audience.
Product Series
A collection of related products that share a common design, technology, or purpose. Products within the series either maintain a cohesive brand / style identity or work together to serve a particular solution.
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Timer Type
The mechanism by which the timer operates, such as mechanical, digital, or programmable.
Outlet Type
Describes the unique qualities or characteristics of an electrical outlet that make it better suited to different uses. The listed qualities may give the outlet improved safety performance, increased efficiency, or additional functionality.
Sensor Type
The Device that Receives a Signal or Stimulus (As Heat or Pressure or Light or Motion Etc.) and Responds to it in a Distinctive Manner
Lens Type
The type of lens that the adapter is fixing to.
Connector
Refers to the specific types of connections a device uses to join electrical conductors and create an electrical circuit. When you select the first desired connector, a second filter will appear listing any connectors on the opposite end of your selected connector on a device.
Connector Type
The Type of Connectors / Terminals that Tool can Crimp to Wire or Cable
Product Certifications
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
Features
Unique characteristics and functionality that set the product apart from others in its field.
Material
Indicates the primary material(s) used to construct a product.
Mounting Type
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
Standard
The industrial standard(s) to which a device is manufactured, operated, or tested.
Load Rating
The maximum load that a device is designed to withstand without breakage or loss of performance.
Load Type
Denotes the type(s) of load that can be applied to a dimmer, which determines its compatible light sources.
Amperage
Maximum electrical current the conductor or device can carry before sustaining immediate or progressive deterioration
Input Voltage
The Difference of Electrical Potential Between Two Points of an Electrical or Electronic Circuit Entering a System
Voltage
The Rate at Which Energy is Drawn from a Source that Produces a Flow of Electricity in a Circuit
Sensor Technology
The technology used by a device to sense a change in signal or stimulus.
Application Sector
Refers to the expected environment(s) or intended usage(s) for a product (e.g. Residential, Commercial, Industrial, etc.).
Indoor/Outdoor
Enviromental Conditions rating on the product. Indoor Only, Outdoor, Both
Installation Location
Where a Device is or is to be Installed
Location Rating
Denotes the classification used to assess the suitability or performance of a device based on the specific environmental location in which it operates.
Jacket Application
Describes the specific application(s) a cable's jacket is designed to be used in, such as in-wall, plenum, or riser.
Compatibility
Capability of Being Used with or Connected to Different Types of Devices or Components without any Modifications
On Function
Describes the mode of operation for devices that can be turned on, indicating whether they stay on continuously or operate on a timer or sensor.
Throw Type
Describes the method of switch operation, indicating whether it controls one circuit (single-throw) or switches between two circuits (double-throw).
Operating Temperature
The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit
Operating Temperature Max
Indicates the highest possible temperature a device can be safely used without the risk of failure or damage.
Storage Temperature
Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
Wire Connection Type
Describes the method used to connect wires to the device, such as screw terminals, push-in connectors, or lead wires.
Line Frequency
The frequency of alternating current (AC) in an electrical power system, measured in Hz. Also commonly referred to as Utility Frequency, Power Line Frequency, or Mains Frequency.
Output Voltage
The Voltage Measured at the Output Terminals of a Power Supply
Contact Configuration
Different Switching Functions of the Relay Contacts
Contact Rating
The Voltage, Current, and Power Capacities of Relay Contacts Under Specified Environmental Conditions
Sensing Range
The total Possible Sensing Capability of the Sensor, Beginning After the Deadband, and Extending Out as Far as the Sensor is Able to Reach Effectively
Sensor Coverage
Describes the total area, measured in square footage, within which a sensor can detect presence or movement.
Sensor Coverage Pattern
Describes the shape of the area that a sensor is able to detect presence or movement within, measured in degrees.
Wireless Range
Describes the maximum distance wireless devices can be separated while preserving signal quality and reliability.
Data Transfer Rate
The Speed at Which Data is Transferred from one Location to Another with in the Time Frame
Termination Style
The style of connection used for electrical termination between two devices.
Conductor
Describes the number and configuration of electrical wires used within a cable to transmit signals.
Shielded/Unshielded
Denotes whether a cable is designed with an extra layer of metal foil or braid surrounding the inner conductor to protect against electromagnetic interference (EMI).
Max Distance Support
Refers to the maximum range a signal can be effectively supported to by a device.
Cable Diameter
The typical outer diameter of a cable.
Cable Length
The Longest Dimension of Insulated Conductors
Wire Gauge
Measuring and Indicating a Quantity of Wire
Number of Gangs
The amount of switches on the plate.
Number of Buttons
The Number of Keys/Switches in the item Used for Selecting a Particular Function
Number of Switches
Number of electrical switches
Number of Receptacles
The Number of Electrical Wall Outlets Designed for Use with a Plug
Number of USBs
Number of USB ports
Publishing Date Range
Date article, blog, or press release was published.
Brand
Choose from one of Legrand's brands.
Filter by Product Category
Filter downloadable resources by the product category they relate or are relevant to.
Brand
Choose from one of Legrand's brands.
Resource Type
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
Learn about how to submit a Wattstopper RMA. Our process has improved thanks to customer feedback!
Legrand, a global leader in electrical and digital building infrastructures, is announcing the rebranding of Encelium technology to Wattstopper PLUS.
Legrand®, a global leader in electrical and digital building infrastructures has announced a new integration between its Wattstopper® lighting control systems and Mecho® motorized and automated shades. This collaboration creates a streamlined approach for building owners, designers, and integrators to combine advanced lighting and shading solutions, driving greater energy efficiency, comfort, and occupant control.
Legrand®, a global leader in electrical and digital building infrastructures has announced a new integration between its Wattstopper® lighting control systems and Mecho® motorized and automated shades. This collaboration creates a streamlined approach for building owners, designers, and integrators to combine advanced lighting and shading solutions, driving greater energy efficiency, comfort, and occupant control.
Legrand’s i3 Platform integrates with Wattstopper PLUS, and DLM to helps users monitor, analyze, and manage smart building data in real-time.
Find comprehensive Wattstopper resources and support here. Explore user guides, installation instructions, CAD Drawings, and more to optimize your Wattstopper lighting controls.
Innovative WattStopper hi/low sensor for outdoor LED fixtures wins top honors in Consulting-Specifying Engineer reader survey
Access all the specification tools and resources you need for your next project.
Wattstopper offers simple, scalable and flexible, energy-efficient networked lighting controls and solutions for commercial applications. Browse lighting control products and solutions for spaces where occupants learn, work, and heal.
Easily manage, adjust, and optimize your lighting control system with Wattstopper’s Lighting Control System Services broad portfolio of support. Learn more now.
Legrand, North & Central America announced the launch of Wattstopper Technology-Enabled Service Contracts, a new offering that brings added convenience and protection to lighting control system investments.
Legrand unveils Wattstopper i3, a groundbreaking smart building management platform powered by KODE Labs. Discover seamless control, intelligent automation, and future-ready integration.
Wattstopper partners with Genlyte Solutions to deliver integrated outdoor lighting controls using the FSP‑600 Fixture Sensor Photocell and Gardco luminaires.
Wattstopper FSP-600 Series, a next-generation wireless in-fixture lighting control solution. Featuring 0–10V dimming with integrated motion sensing, daylight harvesting, and wireless networking, the FSP-600 delivers flexible, scalable control for a wide range of applications.
Legrand’s products and systems touch nearly every part of the building environment. Find your business solution from Legrand today!
Discover our solutions designed to help you meet the diverse needs of everyone in your healthcare facility.
Features Simplified Setup and Diagnostics Via Touch Screen Display and Delivers Highest Quality Audio to Three Zones Simultaneously with 110-Watts of Power
AT ISE, LEGRAND FEATURES NUVO P4300, NEW MULTI-ZONE, RACK-MOUNT PLAYER FOR PLAYER PORTFOLIO MUSIC SYSTEM
Have a question? Want to get in contact with a Legrand customer service representative? Email or contact our customer support desk. Contact us today!