5
Browse 43 results for
"Matter-Enabled"
Filter by Category
Our products, brands, and resources fall under many unique categories based on the product's type or function. Filter and find a product you are looking for based on a Legrand product category.
Brand
Choose from one of Legrand's brands.
Product Type
Select a Product Type to find products that share the same basic form and function, such as switches, cables, panels, or electrical boxes.
Number of Receptacles
The Number of Electrical Wall Outlets Designed for Use with a Plug
Amperage
Maximum electrical current the conductor or device can carry before sustaining immediate or progressive deterioration
Availability
Product is available to buy on Legrand.us
Product Certifications
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
Number of Gangs
The amount of switches on the plate.
Frequency Rating
The Number of Occurrences within a Given Time Period, the Rate at Which Alternating Current Makes a Complete Cycle of Reversals
Indoor/Outdoor
Enviromental Conditions rating on the product. Indoor Only, Outdoor, Both
Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Mounting Type
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
NEMA Configuration Code
Alpha-Numeric Code Applied to Connectors to Guarantee Consistency and Interchageability Between Manufacturers
Load Rating
The maximum load that a device is designed to withstand without breakage or loss of performance.
Wattage
amount of watts used
Receptacle Type
The physical character of a Receptacle. The Type/Specification of a Contact Device Installed at the Outlet for the Connection of an Attachment Plug a Single Receptacle is a Single Contact Device with No Other Contact Device on the Same Yoke a Multiple Receptacle is Two or More Contact Devices.
Color
The color of the product itself
Number of Switches
Number of electrical switches
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
Wire Connection Type
Describes the method used to connect wires to the device, such as screw terminals, push-in connectors, or lead wires.
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
Wall Plate Included
Indicates if the device comes with a cover plate for aesthetic integration with the wall.
Works With
Need to ensure your choice works with your device, system, or software? Select your needs using this filter to confirm compatibility.
Dimming Phase
Refers to the point in the AC power cycle at which the dimmer begins to reduce voltage to the light. "Leading Edge" dimmers cut the initial phase and are typically used for incandescent bulbs, while "Trailing Edge" dimmers cut the end phase, which is more suitable for LEDs.
Requires Neutral Wire
Indicates whether a device requires a neutral wire to function properly.
Operating Humidity
Describes the range of humidity at which a device can be utilized safely without the risk of failure or damage.
Connection Location
Specifies where on the device the electrical connections are made, which can affect installation.
Product Height
The overall height of a product.
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Throw Type
Describes the method of switch operation, indicating whether it controls one circuit (single-throw) or switches between two circuits (double-throw).
Features
Unique characteristics and functionality that set the product apart from others in its field.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
Warranty Type
The product warranty that accompanies the specific product.
Terminal Accommodation
Describes the type and size of wire that the receptacle's terminals can securely hold (typically provided as a range in gauge size).
Finish
Describes the specific surface treatment applied to the outer product for either aesthetics and/or durability.
Product Length
The overall length of a product.
Bulb Compatibility
Indicates the type(s) of lighting a dimmer or controller is designed to work with, ensuring proper functionality and performance.
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
Our brands, products, resources, and pages are group into divisions. Filter and find a product, resource, or page you are looking for based on a Legrand category.
Filter by Product Category
Filter downloadable resources by the product category they relate or are relevant to.
Brand
Choose from one of Legrand's brands.
Resource Type
Filter for different types of resources like CAD drawings, BIM objects, guide form specs, online configurators, white papers, brochures, or product cut sheets.
File Size
Filter downloadable resources by their approximate file size.
Setup Matter smart lights, dimmers and outlets in Amazon Alexa to control your home’s lighting with this step-by-step guide.
Matter-enabled devices offer a convenient way to integrate multiple types of devices into a smart home system so they all communicate with each other.
Learn the differences between Thread and Wi-Fi when it comes to smart lighting and Matter-enabled devices for the home to determine the best solution.
Smart Wi-Fi Light switches and dimmers from Legrand allow users to easily control light and power from a smart home lighting system or Matter hub.
New Matter-enabled devices from the radiant® Collection, developed using Amazon’s Alexa Connect Kit for Matter, are on preview at the 2024 Consumer Electronics Show.
Discover Legrand's latest innovations in lighting control solutions. Explore cutting-edge innovations for seamless LED dimming and advanced lighting control experiences.
Find answers to the most frequently asked questions about Smart Lighting from the radiant Collection.
Legrand offers smart lighting solutions to fit every lifestyle, application or project.
Easily adjust the maximum and minimum brightness of your smart dimmer switch in the Legrand Home + Control App. Settings also eliminate flickering and other issues.
Step-by-step instructions to create custom settings for Netatmo smart lights using Amazon’s Alexa voice commands.
Learn to set up a smart lighting gateway for Legrand’s Smart Lighting with Netatmo light switches, dimmers and outlets to complete a whole home solution.
Control your Legrand smart light switches in Google Home with voice commands using these step-by-step instructions.
Discover how Legrand products and solutions are used by our customers to improve healthcare facilities.
Light switch timers and occupancy/vacancy sensors offer automated control for convenience and energy savings in the home while allowing for precise lighting control.
Discover our solutions designed to help you meet the diverse needs of everyone in your healthcare facility.
Smart lighting schedules help automate lighting for convenience, energy efficiency and safety, all accessible through the Legrand Home + Control app.
Alliance Pairs Vantage’s Customizable Lighting Controls With Soraa LED Lamps to Deliver a Dynamic, End-to-End Lighting Solution
Overhead power distribution using track busway systems is rapidly becoming the solution of choice in data centers, industrial and manufacturing plants, and other facilities that require continuous uptime and faster adaptability.
Data center equipment density is higher than ever, a trend sure to continue as demand for artificial intelligence (AI) and high-performance computing (HPC) soars. This trend is forcing data center operators to rethink their infrastructure and cooling systems at a time when energy optimization and meeting sustainability goals are top priorities.
Want to control your lights from anywhere? With the Netatmo Solutions and Legrand Home + Control app, you can manage and monitor lights from anywhere.
Designating a space for working out at home? Here are some tips for an optimal home gym setup.
Read for tips to get organized with a stylish DIY charging station that will meet your family’s mobile device needs.
Legrand solutions have supported the Cisco Live NOC for several years, with 2025 marking the fourth consecutive year that Legrand's acclAIM high-density fiber system has played a key role.
Wiremold offers a standard 1-year limited warranty from date of installation or two years from the date of purchase, whichever is sooner.
IECC light control guidelines suggest adding dimmers, timers and sensors to the home for energy efficiency. Read our guide to the standards and why they’re important.
Learn how to gain the convenience of multi-location control with elevated style. Just follow these simple steps for wiring adorne® or radiant® 3-way switches.
USB wall outlet installation is an easy upgrade to improve functionality in the home. Follow our tips and steps to choosing the right option.
Leverage evolving technology and real-time data analytics to overcome facility manager challenges associated with post-COVID workplaces. Read the article to learn more.
For anyone making the switch to an electric vehicle (EV), it’s beneficial to understand what to look for in a home EV charger. Here are factors to consider.